User Interface.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | MOUSE_MOVE_RANGE 3 |
Functions | |
ISR (PORTB_INT0_vect) | |
Interrupt on "pin change" from switch to do wakeup on USB Callback running when USB Host enable mouse interface. More... | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
#define MOUSE_MOVE_RANGE 3 |
Referenced by ui_process().
ISR | ( | PORTB_INT0_vect | ) |
Interrupt on "pin change" from switch to do wakeup on USB Callback running when USB Host enable mouse interface.
Note: This interrupt is enable when the USB host enable remotewakeup feature This interrupt wakeup the CPU if this one is in idle mode
References GPIO_PUSH_BUTTON_0, ioport_pin_to_port(), and udc_remotewakeup().
void ui_init | ( | void | ) |
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED0_GPIO, LED1_GPIO, and LED_Off.
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References gpio_pin_is_low, GPIO_PUSH_BUTTON_0, GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, GPIO_PUSH_BUTTON_3, LED1_GPIO, LED_Off, LED_On, MOUSE_MOVE_RANGE, udi_hid_mouse_moveX(), and udi_hid_mouse_moveY().
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0_GPIO, and LED_On.
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References GPIO_PUSH_BUTTON_0, and ioport_pin_to_port().
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References GPIO_PUSH_BUTTON_0, GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, GPIO_PUSH_BUTTON_3, ioport_configure_pin(), IOPORT_DIR_INPUT, ioport_pin_to_port(), and IOPORT_PULL_UP.
Referenced by main_remotewakeup_enable().