Main functions for Mouse unit test.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdio.h>
#include <asf.h>
#include <unit_test/suite.h>
#include <stdio_serial.h>
#include <conf_test.h>
Functions | |
int | main (void) |
Run usb device mouse unit tests. More... | |
void | main_mouse_disable (void) |
Called by HID interface Callback running when USB Host disable mouse interface. More... | |
bool | main_mouse_enable (void) |
Called by HID interface Callback running when USB Host enable mouse interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vbus_action (bool b_high) |
Called when Vbus line state change. More... | |
static void | run_usb_mouse_test (const struct test_case *test) |
static void | run_usb_resume_test (const struct test_case *test) |
static void | run_usb_sof_test (const struct test_case *test) |
static void | run_usb_suspend_test (const struct test_case *test) |
static void | run_usb_vbus_test (const struct test_case *test) |
Variables | |
static bool | main_b_mouse_enumerated = false |
static bool | main_b_resume_event = false |
static bool | main_b_sof_event = false |
static bool | main_b_suspend_event = false |
static bool | main_b_vbus_event = false |
int main | ( | void | ) |
Run usb device mouse unit tests.
Initializes the clock system, board and serial output, then sets up the usb unit test suite and runs it.
References usart_options_t::baudrate, board_init(), CONF_TEST_BAUDRATE, CONF_TEST_CHARLENGTH, CONF_TEST_PARITY, CONF_TEST_STOPBITS, CONF_TEST_USART, cpu_irq_enable, DEFINE_TEST_ARRAY, DEFINE_TEST_CASE, DEFINE_TEST_SUITE, irq_initialize_vectors, run_usb_mouse_test(), run_usb_resume_test(), run_usb_sof_test(), run_usb_suspend_test(), run_usb_vbus_test(), SLEEPMGR_ACTIVE, SLEEPMGR_IDLE, sleepmgr_init(), sleepmgr_lock_mode(), stdio_serial_init(), sysclk_init(), and test_suite_run().
void main_mouse_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable mouse interface.
bool main_mouse_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable mouse interface.
true | if mouse startup is ok |
References main_b_mouse_enumerated.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References main_b_suspend_event.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_sof_event.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References main_b_resume_event.
void main_vbus_action | ( | bool | b_high | ) |
Called when Vbus line state change.
References main_b_vbus_event.
Referenced by run_usb_mouse_test().
|
static |
References main_b_mouse_enumerated, main_vbus_action(), sleepmgr_enter_sleep(), udc_include_vbus_monitoring(), udc_start(), udc_stop(), and UNUSED.
Referenced by main().
|
static |
References main_b_resume_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_sof_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_suspend_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_vbus_event, and test_assert_true.
Referenced by main().
Referenced by main_mouse_enable(), and run_usb_mouse_test().
Referenced by main_suspend_action(), and run_usb_resume_test().
Referenced by main_sof_action(), and run_usb_sof_test().
Referenced by main_resume_action(), and run_usb_suspend_test().
Referenced by main_vbus_action(), and run_usb_vbus_test().