License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick Start Guide for the System Clock Management | Service (SAM4E) |
Advanced use case - Peripheral Bus Clock | Management (SAM4E) |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick start guide for USB device mouse module (UDI mouse) | This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID mouse in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
"SAM4E-EK - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM4E-EK - Board informations" | This page lists several definition related to the board description |
"SAM4E-EK - USB device" | |
"SAM4E-EK - External components" | This page lists the definitions related to external on-board components located in the board.h file for the SAM4E-EK |
"SAM4E-EK - Memories" | This page lists definitions related to internal & external on-board memories |
"SAM4E-EK - CAN" | This page lists definitions related to CAN0 and CAN1 |
Todo List | |