Declaration of main function used by HID multi-touch example.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_multitouch_disable (void) |
Called by HID interface Callback running when USB Host disable multi-touch interface. More... | |
bool | main_multitouch_enable (void) |
Called by HID interface Callback running when USB Host enable multi-touch interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void main_multitouch_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable multi-touch interface.
References main_b_mtouch_enable.
bool main_multitouch_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable multi-touch interface.
true | if multi-touch startup is ok |
References main_b_mtouch_enable.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
References ui_wakeup_enable().
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_mtouch_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References ui_powerdown().