Software Driver for the Accelerometer LIS3L06AL.
This driver relies on the ADC hardware module. It provides functions to initialize the module, to read (x,y,z) coordinates and to get acceleration/orientation/angle information.
Data Structures | |
struct | avr32_acc_t |
Set of computed data. More... | |
struct | xyz_t |
All 3-axis values from ADC conversion. More... | |
Macros | |
#define | ACC_SHIFT 2 |
Functions | |
unsigned long | acc_get_m_x (void) |
Return measured value of X sensor. More... | |
unsigned long | acc_get_m_y (void) |
Return measured value of Y sensor. More... | |
unsigned long | acc_get_m_z (void) |
Return measured value of Z sensor. More... | |
void | acc_init (void) |
Initialize Accelerometer driver. Mandatory to call. More... | |
void | acc_update (void) |
Get accelerometer measure (3x) and process results. More... | |
signed long | is_acc_abs_angle_x (unsigned long abs_ang) |
Test if absolute value of X angle has reached the specified limit. More... | |
signed long | is_acc_abs_angle_y (unsigned long abs_ang) |
Test if absolute value of Y angle has reached the specified limit. More... | |
bool | is_acc_down (void) |
Test if sensor have detected 'down' orientation. More... | |
bool | is_acc_left (void) |
Test if sensor have detected 'left' orientation. More... | |
bool | is_acc_meuh (char stop) |
Detect a topdown to up transition. More... | |
bool | is_acc_right (void) |
Test if sensor have detected 'right' orientation. More... | |
bool | is_acc_slow (void) |
Test acceleration about 1g +-10%. More... | |
bool | is_acc_topdown (void) |
Test if sensor have detected 'topdown' orientation. More... | |
bool | is_acc_up (void) |
Test if sensor have detected 'up' orientation. More... | |
Nominal values out of lis3l06al accelerometer spec | |
#define | ACC_ZERO (512 >> ACC_SHIFT) |
#define | ACC_1G (205 >> ACC_SHIFT) |
#define | ACC_MIN ( ACC_ZERO - ACC_1G ) |
#define | ACC_MAX ( ACC_ZERO + ACC_1G ) |
Sinus table | |
#define | SIN0 0 |
#define | SIN15 0.26 |
#define | SIN30 0.5 |
#define | SIN45 0.71 |
#define | SIN60 0.87 |
#define | SIN75 0.97 |
#define | SIN90 1 |
Axis calibration correction | |
#define | ACC_CALIB_X 0 |
#define | ACC_CALIB_Y 0 |
#define | ACC_CALIB_Z 0 |
Axis zero point. | |
#define | ACC_ZERO_X ( ACC_ZERO + ACC_CALIB_X ) |
#define | ACC_ZERO_Y ( ACC_ZERO + ACC_CALIB_Y ) |
#define | ACC_ZERO_Z ( ACC_ZERO + ACC_CALIB_Z ) |
Axis reference values for a set of predefined angles. | |
#define | ACC_TRIG_X0 (int) ( ACC_ZERO_X - SIN15 * ACC_1G ) |
#define | ACC_TRIG_X1 (int) ( ACC_ZERO_X + SIN15 * ACC_1G ) |
#define | ACC_TRIG_Y0 (int) ( ACC_ZERO_Y - SIN15 * ACC_1G ) |
#define | ACC_TRIG_Y1 (int) ( ACC_ZERO_Y + SIN15 * ACC_1G ) |
#define | ACC_TRIG_Z_TOP (int) ( ACC_ZERO_Z - SIN75 * ACC_1G ) |
#define | ACC_TRIG_Z_BOT (int) ( ACC_ZERO_Z + SIN60 * ACC_1G ) |
Sudden acceleration thresholds | |
#define | ACC_QUIET_LO (int) ( 0.6 * ACC_1G * ACC_1G ) |
#define | ACC_QUIET_HI (int) ( 1.4 * ACC_1G * ACC_1G ) |
Accelerometer ADC channel mapping | |
#define | ADC_CHANNEL_X ADC_ACC_X_CHANNEL |
#define | ADC_CHANNEL_Y ADC_ACC_Y_CHANNEL |
#define | ADC_CHANNEL_Z ADC_ACC_Z_CHANNEL |
#define ACC_1G (205 >> ACC_SHIFT) |
Referenced by is_acc_abs_angle_x(), and is_acc_abs_angle_y().
#define ACC_CALIB_X 0 |
#define ACC_CALIB_Y 0 |
#define ACC_CALIB_Z 0 |
Referenced by is_acc_slow().
Referenced by is_acc_slow().
#define ACC_SHIFT 2 |
Referenced by acc_get_value().
#define ACC_TRIG_X0 (int) ( ACC_ZERO_X - SIN15 * ACC_1G ) |
Referenced by is_acc_right().
#define ACC_TRIG_X1 (int) ( ACC_ZERO_X + SIN15 * ACC_1G ) |
Referenced by is_acc_left().
#define ACC_TRIG_Y0 (int) ( ACC_ZERO_Y - SIN15 * ACC_1G ) |
Referenced by is_acc_up().
#define ACC_TRIG_Y1 (int) ( ACC_ZERO_Y + SIN15 * ACC_1G ) |
Referenced by is_acc_down().
#define ACC_TRIG_Z_BOT (int) ( ACC_ZERO_Z + SIN60 * ACC_1G ) |
Referenced by is_acc_meuh(), and is_acc_topdown().
#define ACC_TRIG_Z_TOP (int) ( ACC_ZERO_Z - SIN75 * ACC_1G ) |
Referenced by is_acc_meuh().
#define ACC_ZERO (512 >> ACC_SHIFT) |
#define ACC_ZERO_X ( ACC_ZERO + ACC_CALIB_X ) |
#define ACC_ZERO_Y ( ACC_ZERO + ACC_CALIB_Y ) |
#define ACC_ZERO_Z ( ACC_ZERO + ACC_CALIB_Z ) |
#define ADC_CHANNEL_X ADC_ACC_X_CHANNEL |
Referenced by acc_get_value().
#define ADC_CHANNEL_Y ADC_ACC_Y_CHANNEL |
Referenced by acc_get_value().
#define ADC_CHANNEL_Z ADC_ACC_Z_CHANNEL |
Referenced by acc_get_value().
#define SIN0 0 |
#define SIN15 0.26 |
#define SIN30 0.5 |
#define SIN45 0.71 |
#define SIN60 0.87 |
#define SIN75 0.97 |
#define SIN90 1 |
unsigned long acc_get_m_x | ( | void | ) |
Return measured value of X sensor.
References avr32_acc_t::m, and xyz_t::x.
unsigned long acc_get_m_y | ( | void | ) |
Return measured value of Y sensor.
References avr32_acc_t::m, and xyz_t::y.
unsigned long acc_get_m_z | ( | void | ) |
Return measured value of Z sensor.
References avr32_acc_t::m, and xyz_t::z.
void acc_init | ( | void | ) |
Initialize Accelerometer driver. Mandatory to call.
References adc_configure(), and gpio_enable_module().
Referenced by ui_init().
void acc_update | ( | void | ) |
Get accelerometer measure (3x) and process results.
References acc_get_value(), avr32_acc_t::ag, avr32_acc_t::ak, avr32_acc_t::ak2, avr32_acc_t::g, is_acc_slow(), avr32_acc_t::k, avr32_acc_t::m, avr32_acc_t::s, xyz_t::x, xyz_add(), xyz_diff(), xyz_round0(), xyz_sumsq(), xyz_t::y, and xyz_t::z.
Referenced by ui_device_sof_action().
signed long is_acc_abs_angle_x | ( | unsigned long | abs_ang | ) |
Test if absolute value of X angle has reached the specified limit.
References abs, ACC_1G, avr32_acc_t::ak, DEG_2_RAD, and xyz_t::x.
Referenced by ui_device_sof_action().
signed long is_acc_abs_angle_y | ( | unsigned long | abs_ang | ) |
Test if absolute value of Y angle has reached the specified limit.
References abs, ACC_1G, avr32_acc_t::ak, DEG_2_RAD, and xyz_t::y.
Referenced by ui_device_sof_action().
bool is_acc_down | ( | void | ) |
Test if sensor have detected 'down' orientation.
This function uses an software hysteresis.
References ACC_TRIG_Y1, avr32_acc_t::down, avr32_acc_t::m, avr32_acc_t::pos, and xyz_t::y.
bool is_acc_left | ( | void | ) |
Test if sensor have detected 'left' orientation.
This function uses an software hysteresis.
References ACC_TRIG_X1, avr32_acc_t::left, avr32_acc_t::m, avr32_acc_t::pos, and xyz_t::x.
bool is_acc_meuh | ( | char | stop | ) |
Detect a topdown to up transition.
This function uses an software hysteresis.
References ACC_TRIG_Z_BOT, ACC_TRIG_Z_TOP, avr32_acc_t::m, and xyz_t::z.
bool is_acc_right | ( | void | ) |
Test if sensor have detected 'right' orientation.
This function uses an software hysteresis.
References ACC_TRIG_X0, avr32_acc_t::m, avr32_acc_t::pos, avr32_acc_t::right, and xyz_t::x.
bool is_acc_slow | ( | void | ) |
Test acceleration about 1g +-10%.
Gravity is always present! This is used to decide slow / fast behavior
References ACC_QUIET_HI, ACC_QUIET_LO, and avr32_acc_t::ak2.
Referenced by acc_update().
bool is_acc_topdown | ( | void | ) |
Test if sensor have detected 'topdown' orientation.
This function uses an software hysteresis.
References ACC_TRIG_Z_BOT, avr32_acc_t::m, avr32_acc_t::pos, avr32_acc_t::topdown, and xyz_t::z.
bool is_acc_up | ( | void | ) |
Test if sensor have detected 'up' orientation.
This function uses an software hysteresis.
References ACC_TRIG_Y0, avr32_acc_t::m, avr32_acc_t::pos, avr32_acc_t::up, and xyz_t::y.