User Interface.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
Internal routines to manage asynchronous interrupt pin change | |
This interrupt is connected to a switch and allows to wakeup CPU in low sleep mode. This wakeup the USB devices connected via a downstream resume. | |
static void | ui_enable_asynchronous_interrupt (void) |
Initializes and enables interrupt pin change. More... | |
static void | ui_disable_asynchronous_interrupt (void) |
Disables interrupt pin change. More... | |
ISR (ui_wakeup_isr, AVR32_GPIO_IRQ_GROUP, 0) | |
Interrupt handler for interrupt pin change. More... | |
Main user interface functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_usb_mode_change (bool b_host_mode) |
Notify that the USB mode are switched automatically. This is possible only when ID pin is available. More... | |
Host mode user interface functions | |
static uhc_enum_status_t | ui_enum_status =UHC_ENUM_DISCONNECT |
Status of device enumeration. More... | |
static uint16_t | ui_device_speed_blink |
Blink frequency depending on device speed. More... | |
static int8_t | ui_x |
Manages device mouse moving. More... | |
static int8_t | ui_y |
static int8_t | ui_scroll |
void | ui_usb_vbus_change (bool b_vbus_present) |
Notify that a Vbus are changed Available only in USB hardware with Vbus monitoring. More... | |
void | ui_usb_vbus_error (void) |
Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring. More... | |
void | ui_usb_connection_event (uhc_device_t *dev, bool b_present) |
Notify that a USB device has been connected or disconnected. More... | |
void | ui_usb_enum_event (uhc_device_t *dev, uhc_enum_status_t status) |
Notify the end of a USB device enumeration. More... | |
void | ui_usb_wakeup_event (void) |
Notify that a USB device or the host has wake up the USB line. More... | |
void | ui_usb_sof_event (void) |
Notify that a SOF has been sent (each 1 ms) More... | |
static void | ui_uhi_hid_mouse_btn (bool b_state) |
void | ui_uhi_hid_mouse_btn_left (bool b_state) |
void | ui_uhi_hid_mouse_btn_right (bool b_state) |
void | ui_uhi_hid_mouse_btn_middle (bool b_state) |
void | ui_uhi_hid_mouse_move (int8_t x, int8_t y, int8_t scroll) |
ISR | ( | ui_wakeup_isr | , |
AVR32_GPIO_IRQ_GROUP | , | ||
0 | |||
) |
Interrupt handler for interrupt pin change.
References eic_clear_interrupt_line(), EXT_NMI, gpio_clear_pin_interrupt_flag(), uhc_is_suspend(), uhc_resume(), and ui_disable_asynchronous_interrupt().
|
static |
Disables interrupt pin change.
References eic_disable_line(), EXT_NMI, and gpio_disable_pin_interrupt().
Referenced by ISR(), and ui_usb_wakeup_event().
|
static |
Initializes and enables interrupt pin change.
Structure holding the configuration parameters of the EIC low level driver.
References cpu_irq_restore(), cpu_irq_save(), EIC_ASYNCH_MODE, eic_enable_line(), EIC_FILTER_ENABLED, eic_init(), EIC_LEVEL_LOW_LEVEL, eic_options_t::eic_line, EIC_MODE_LEVEL_TRIGGERED, EXT_NMI, gpio_enable_module_pin(), gpio_enable_pin_interrupt(), gpio_enable_pin_pull_up(), GPIO_PIN_CHANGE, and irq_register_handler.
Referenced by ui_usb_sof_event().
void ui_init | ( | void | ) |
|
static |
References LED3, LED_Off(), and LED_On().
Referenced by ui_uhi_hid_mouse_btn_left(), ui_uhi_hid_mouse_btn_middle(), and ui_uhi_hid_mouse_btn_right().
void ui_uhi_hid_mouse_btn_left | ( | bool | b_state | ) |
References ui_uhi_hid_mouse_btn().
void ui_uhi_hid_mouse_btn_middle | ( | bool | b_state | ) |
References ui_uhi_hid_mouse_btn().
void ui_uhi_hid_mouse_btn_right | ( | bool | b_state | ) |
References ui_uhi_hid_mouse_btn().
void ui_uhi_hid_mouse_move | ( | int8_t | x, |
int8_t | y, | ||
int8_t | scroll | ||
) |
void ui_usb_connection_event | ( | uhc_device_t * | dev, |
bool | b_present | ||
) |
void ui_usb_enum_event | ( | uhc_device_t * | dev, |
uhc_enum_status_t | status | ||
) |
Notify the end of a USB device enumeration.
dev | Pointer on USB device information |
status | Status of the USB enumeration |
References UHD_SPEED_FULL, UHD_SPEED_HIGH, UHD_SPEED_LOW, ui_device_speed_blink, ui_enum_status, ui_scroll, ui_x, and ui_y.
void ui_usb_mode_change | ( | bool | b_host_mode | ) |
Notify that the USB mode are switched automatically. This is possible only when ID pin is available.
b_host_mode | true, if the host mode has been selected |
References ui_init().
void ui_usb_sof_event | ( | void | ) |
Notify that a SOF has been sent (each 1 ms)
References gpio_get_pin_value(), GPIO_PUSH_BUTTON_SW2, LED1, LED2, LED3, LED_Off(), LED_On(), LED_Toggle(), uhc_suspend(), ui_device_speed_blink, ui_enable_asynchronous_interrupt(), ui_enum_status, ui_scroll, ui_x, and ui_y.
void ui_usb_vbus_change | ( | bool | b_vbus_present | ) |
void ui_usb_vbus_error | ( | void | ) |
Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring.
void ui_usb_wakeup_event | ( | void | ) |
Notify that a USB device or the host has wake up the USB line.
References ui_disable_asynchronous_interrupt().
|
static |
Blink frequency depending on device speed.
Referenced by ui_usb_enum_event(), and ui_usb_sof_event().
|
static |
Status of device enumeration.
Referenced by ui_usb_connection_event(), ui_usb_enum_event(), and ui_usb_sof_event().
|
static |
Referenced by ui_uhi_hid_mouse_move(), ui_usb_enum_event(), and ui_usb_sof_event().
|
static |
Manages device mouse moving.
Referenced by ui_uhi_hid_mouse_move(), ui_usb_enum_event(), and ui_usb_sof_event().
|
static |
Referenced by ui_uhi_hid_mouse_move(), ui_usb_enum_event(), and ui_usb_sof_event().