Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "ui.h"

Functions

void ui_init (void)
 
void ui_powerdown (void)
 
void ui_process (uint16_t framenumber)
 This process is called called each 1ms It is called only if MSC interface is enable. More...
 
void ui_start_read (void)
 
void ui_start_write (void)
 
void ui_stop_read (void)
 
void ui_stop_write (void)
 
void ui_wakeup (void)
 

void ui_init ( void  )

References LED0_GPIO, LED1_GPIO, LED2_GPIO, LED_Off(), and LED_On().

Referenced by main().

void ui_powerdown ( void  )

References LED0_GPIO, LED1_GPIO, LED2_GPIO, and LED_Off().

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called called each 1ms It is called only if MSC interface is enable.

It is called by SOF interrupt.

References LED0_GPIO, LED_Off(), and LED_On().

Referenced by main_sof_action().

void ui_start_read ( void  )

References LED1_GPIO, and LED_On().

void ui_start_write ( void  )

References LED2_GPIO, and LED_On().

void ui_stop_read ( void  )

References LED1_GPIO, and LED_Off().

void ui_stop_write ( void  )

References LED2_GPIO, and LED_Off().

void ui_wakeup ( void  )

References LED0_GPIO, and LED_On().

Referenced by main_resume_action().