Microchip® Advanced Software Framework

main.h File Reference

Declaration of main function used by MSC example.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void main_msc_disable (void)
 Called by MSC interface Callback running when USB Host disable MSC interface. More...
 
bool main_msc_enable (void)
 Called by MSC interface Callback running when USB Host enable MSC interface. More...
 
void main_msc_notify_trans (void)
 Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state. More...
 
void memories_initialization (void)
 Initialize the memories used by examples. More...
 

void main_msc_disable ( void  )

Called by MSC interface Callback running when USB Host disable MSC interface.

References main_b_msc_enable.

bool main_msc_enable ( void  )

Called by MSC interface Callback running when USB Host enable MSC interface.

Return values
trueif MSC startup is ok

References main_b_msc_enable.

void main_msc_notify_trans ( void  )

Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called.

References pdFALSE, and xSemaphoreGiveFromISR.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

References ui_wakeup().

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

References main_b_msc_enable, udd_get_frame_number(), and ui_process().

void main_suspend_action ( void  )

Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.

References ui_powerdown().

void memories_initialization ( void  )

Initialize the memories used by examples.

References at45dbx_init(), sd_mmc_init(), sysclk_enable_pbb_module(), and SYSCLK_HMATRIX.

Referenced by main().