SCSI Mode Parameter Header used by MODE SELECT(10) and MODE SENSE(10)
#include <spc_protocol.h>
Data Fields | |
be16_t | block_descriptor_length |
Length of block descriptors. More... | |
uint8_t | device_specific_parameter |
Defined by command set. More... | |
uint8_t | flags4 |
LONGLBA in bit 0. More... | |
uint8_t | medium_type |
Medium Type. More... | |
be16_t | mode_data_length |
Number of bytes after this. More... | |
uint8_t | reserved |
be16_t scsi_mode_param_header10::block_descriptor_length |
Length of block descriptors.
uint8_t scsi_mode_param_header10::device_specific_parameter |
Defined by command set.
uint8_t scsi_mode_param_header10::flags4 |
LONGLBA in bit 0.
uint8_t scsi_mode_param_header10::medium_type |
Medium Type.
be16_t scsi_mode_param_header10::mode_data_length |
Number of bytes after this.
uint8_t scsi_mode_param_header10::reserved |