Microchip® Advanced Software Framework

ui.h File Reference

Common User Interface for MSC application.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void ui_init (void)
 
void ui_powerdown (void)
 
void ui_process (uint16_t framenumber)
 This process is called called each 1ms It is called only if MSC interface is enable. More...
 
void ui_start_read (void)
 
void ui_start_write (void)
 
void ui_stop_read (void)
 
void ui_stop_write (void)
 
void ui_wakeup (void)
 

void ui_init ( void  )

References LED_On.

Referenced by main().

void ui_powerdown ( void  )

References LED_Off.

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called called each 1ms It is called only if MSC interface is enable.

It is called by SOF interrupt.

References LED_Off, and LED_On.

Referenced by main_sof_action().

void ui_start_read ( void  )
void ui_start_write ( void  )
void ui_stop_read ( void  )
void ui_stop_write ( void  )
void ui_wakeup ( void  )

References LED_On.

Referenced by main_resume_action().