User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_start_read (void) |
void | ui_start_write (void) |
void | ui_stop_read (void) |
void | ui_stop_write (void) |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void ui_init | ( | void | ) |
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References LED0, LED_Off, and LED_On.
Referenced by main_sof_action().
void ui_start_read | ( | void | ) |
void ui_start_write | ( | void | ) |
void ui_stop_read | ( | void | ) |
void ui_stop_write | ( | void | ) |
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
Referenced by main_resume_action().