Declaration of main function used by MSC example.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | memories_initialization (void) |
Initialize the memories used by examples. More... | |
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
References main_b_msc_enable.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
References main_b_msc_enable.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_msc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References ui_powerdown().
void memories_initialization | ( | void | ) |
Initialize the memories used by examples.
References nand_init(), and sd_mmc_init().
Referenced by main().