Standard USB device qualifier descriptor structure.
This descriptor contains information about the device when running at the "other" speed (i.e. if the device is currently operating at high speed, this descriptor can be used to determine what would change if the device was operating at full speed.)
#include <usb_protocol.h>
Data Fields | |
le16_t | bcdUSB |
uint8_t | bDescriptorType |
uint8_t | bDeviceClass |
uint8_t | bDeviceProtocol |
uint8_t | bDeviceSubClass |
uint8_t | bLength |
uint8_t | bMaxPacketSize0 |
uint8_t | bNumConfigurations |
uint8_t | bReserved |
le16_t usb_dev_qual_desc_t::bcdUSB |
uint8_t usb_dev_qual_desc_t::bDescriptorType |
uint8_t usb_dev_qual_desc_t::bDeviceClass |
uint8_t usb_dev_qual_desc_t::bDeviceProtocol |
uint8_t usb_dev_qual_desc_t::bDeviceSubClass |
uint8_t usb_dev_qual_desc_t::bLength |
Referenced by udc_req_std_dev_get_descriptor().
uint8_t usb_dev_qual_desc_t::bMaxPacketSize0 |
uint8_t usb_dev_qual_desc_t::bNumConfigurations |
uint8_t usb_dev_qual_desc_t::bReserved |