User Interface | Human interface on SAM L21 Xplained Pro |
Virtual Memory in RAM | The component manages a disk on a volatile memory (internal RAM) |
USB device descriptors for a single interface | The following structures provide the USB device descriptors required for USB Device with a single interface MSC |
Memory Control Access | Common abstraction layer for memory interfaces |
Sleep manager | The sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time |
SAM System (SYSTEM) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
SAM System Clock Management (SYSTEM CLOCK) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
SAM System Interrupt (SYSTEM INTERRUPT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
Compiler abstraction layer and code utilities | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
Status Codes | |
Preprocessor - Macro Recursion | |
Preprocessor - Macro Repeat | |
Preprocessor - Stringize | |
Preprocessor - Token Paste | |
Global interrupt management | This is a driver for global enabling and disabling of interrupts |
Deprecated interrupt definitions | |
Atmel part identification macros | This collection of macros identify which series and families that the various Atmel parts belong to |
AVR UC3 parts | |
AVR XMEGA parts | |
megaAVR parts | |
SAM parts | |
SAM System Pin Multiplexer (SYSTEM PINMUX) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
SAM Universal Serial Bus (USB) | The Universal Serial Bus (USB) module complies with the USB 2.1 specification |
SAM External Interrupt (EXTINT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of external interrupts generated by the physical device pins, including edge detection |
SAM Port (PORT) Driver | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
USB Stack | This stack includes the USB Device Stack, USB Host Stack and common definitions |
USB Stack Device | This module includes USB Stack Device implementation |
USB Device Driver Implement (UDD) | USB low-level driver for USB device mode |
USB Device Controller (UDC) | The UDC provides a high-level abstraction of the usb device |
Implementation of UDC | Internal implementation |
USB Device Controller (UDC) - Prerequisites | Common prerequisites for all USB devices |
USB Device Controller (UDC) - Example code | Common example code for all USB devices |
USB Device Controller (UDC) - Workflow | Common workflow for all USB devices |
USB Device Descriptor | |
USB Device Driver (UDD) | The UDD driver provides a low-level abstraction of the device controller hardware |
USB Device Interface (UDI) | The UDI provides a common API for all classes, and this is used by UDC for the main control of USB Device interface |
USB interface descriptors | The following structures provide predefined USB interface descriptors |
Interface with USB Device Core (UDC) | Structures and functions required by UDC |
Implementation of UDI MSC | Class internal implementation |
USB dual role driver | USB low-level driver for dual role features |
Atmel USB Identifiers | This module defines Atmel PID and VIDs constants |
USB Protocol Definitions | This module defines constants and data structures provided by the USB 2.0 specification |
USB Mass Storage Class (MSC) protocol definitions | |
SCSI Block Commands protocol definitions | |
SCSI Primary Commands protocol definitions | |
Generic board support | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
SAM L21 Xplained Pro board | |
Features | Symbols that describe features and capabilities of the board |