See Quick Start Guide for the System Clock Management service (XMEGA).
The sysclk API covers the system clock and all clocks derived from it. The system clock is a chip-internal clock on which all synchronous clocks, i.e. CPU and bus/peripheral clocks, are based. The system clock is typically generated from one of a variety of sources, which may include crystal and RC oscillators as well as PLLs. The clocks derived from the system clock are sometimes also known as synchronous clocks, since they always run synchronously with respect to each other, as opposed to generic clocks which may run from different oscillators or PLLs.
Most applications should simply call sysclk_init() to initialize everything related to the system clock and its source (oscillator, PLL or DFLL), and leave it at that. More advanced applications, and platform-specific drivers, may require additional services from the clock system, some of which may be platform-specific.
The sysclk API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.
The following functions are available on all platforms with the same parameters and functionality. These functions may be called freely by portable applications, drivers and services:
The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behavior. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:
All other functions should be considered platform-specific. Enabling/disabling clocks to specific peripherals as well as determining the speed of these clocks should be done by calling functions provided by the driver for that peripheral.
The following configuration symbols may be used to specify the initial system clock configuration. If any of the symbols are not set, reasonable defaults will be provided.
System Clock Sources | |
#define | SYSCLK_SRC_RC2MHZ CLK_SCLKSEL_RC2M_gc |
Internal 2 MHz RC oscillator. More... | |
#define | SYSCLK_SRC_RC32MHZ CLK_SCLKSEL_RC32M_gc |
Internal 32 MHz RC oscillator. More... | |
#define | SYSCLK_SRC_RC32KHZ CLK_SCLKSEL_RC32K_gc |
Internal 32 KHz RC oscillator. More... | |
#define | SYSCLK_SRC_XOSC CLK_SCLKSEL_XOSC_gc |
External oscillator. More... | |
#define | SYSCLK_SRC_PLL CLK_SCLKSEL_PLL_gc |
Phase-Locked Loop. More... | |
Prescaler A Setting (relative to CLKsys) | |
#define | SYSCLK_PSADIV_1 CLK_PSADIV_1_gc |
Do not prescale. More... | |
#define | SYSCLK_PSADIV_2 CLK_PSADIV_2_gc |
Prescale CLKper4 by 2. More... | |
#define | SYSCLK_PSADIV_4 CLK_PSADIV_4_gc |
Prescale CLKper4 by 4. More... | |
#define | SYSCLK_PSADIV_8 CLK_PSADIV_8_gc |
Prescale CLKper4 by 8. More... | |
#define | SYSCLK_PSADIV_16 CLK_PSADIV_16_gc |
Prescale CLKper4 by 16. More... | |
#define | SYSCLK_PSADIV_32 CLK_PSADIV_32_gc |
Prescale CLKper4 by 32. More... | |
#define | SYSCLK_PSADIV_64 CLK_PSADIV_64_gc |
Prescale CLKper4 by 64. More... | |
#define | SYSCLK_PSADIV_128 CLK_PSADIV_128_gc |
Prescale CLKper4 by 128. More... | |
#define | SYSCLK_PSADIV_256 CLK_PSADIV_256_gc |
Prescale CLKper4 by 256. More... | |
#define | SYSCLK_PSADIV_512 CLK_PSADIV_512_gc |
Prescale CLKper4 by 512. More... | |
Prescaler B and C Setting (relative to CLKper4) | |
#define | SYSCLK_PSBCDIV_1_1 CLK_PSBCDIV_1_1_gc |
Do not prescale. More... | |
#define | SYSCLK_PSBCDIV_1_2 CLK_PSBCDIV_1_2_gc |
Prescale CLKper and CLKcpu by 2. More... | |
#define | SYSCLK_PSBCDIV_4_1 CLK_PSBCDIV_4_1_gc |
Prescale CLKper2, CLKper and CLKcpu by 4. More... | |
#define | SYSCLK_PSBCDIV_2_2 CLK_PSBCDIV_2_2_gc |
Prescale CLKper2 by 2, CLKper and CLKcpu by 4. More... | |
System Clock Port Numbers | |
enum | sysclk_port_id { SYSCLK_PORT_GEN, SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, SYSCLK_PORT_F } |
Clocks not associated with any port | |
| |
#define | SYSCLK_DMA PR_DMA_bm |
DMA Controller. More... | |
#define | SYSCLK_EDMA PR_EDMA_bm |
EDMA Controller. More... | |
#define | SYSCLK_EVSYS PR_EVSYS_bm |
Event System. More... | |
#define | SYSCLK_RTC PR_RTC_bm |
Real-Time Counter. More... | |
#define | SYSCLK_EBI PR_EBI_bm |
Ext Bus Interface. More... | |
#define | SYSCLK_AES PR_AES_bm |
AES Module. More... | |
#define | SYSCLK_USB PR_USB_bm |
USB Module. More... | |
#define | SYSCLK_XCL PR_XCL_bm |
USB Module. More... | |
Clocks on PORTA and PORTB | |
| |
#define | SYSCLK_AC PR_AC_bm |
Analog Comparator. More... | |
#define | SYSCLK_ADC PR_ADC_bm |
A/D Converter. More... | |
#define | SYSCLK_DAC PR_DAC_bm |
D/A Converter. More... | |
Clocks on PORTC, PORTD, PORTE and PORTF | |
| |
#define | SYSCLK_TC0 PR_TC0_bm |
Timer/Counter 0. More... | |
#define | SYSCLK_TC1 PR_TC1_bm |
Timer/Counter 1. More... | |
#define | SYSCLK_TC4 PR_TC4_bm |
Timer/Counter 0. More... | |
#define | SYSCLK_TC5 PR_TC5_bm |
Timer/Counter 1. More... | |
#define | SYSCLK_HIRES PR_HIRES_bm |
Hi-Res Extension. More... | |
#define | SYSCLK_SPI PR_SPI_bm |
SPI controller. More... | |
#define | SYSCLK_USART0 PR_USART0_bm |
USART 0. More... | |
#define | SYSCLK_USART1 PR_USART1_bm |
USART 1. More... | |
#define | SYSCLK_TWI PR_TWI_bm |
TWI controller. More... | |
RTC clock source identifiers | |
#define | SYSCLK_RTCSRC_ULP CLK_RTCSRC_ULP_gc |
1kHz from internal ULP oscillator. More... | |
#define | SYSCLK_RTCSRC_TOSC CLK_RTCSRC_TOSC_gc |
1.024kHz from 32.768kHz crystal oscillator TOSC More... | |
#define | SYSCLK_RTCSRC_RCOSC CLK_RTCSRC_RCOSC_gc |
1.024kHz from 32.768kHz internal RC oscillator More... | |
#define | SYSCLK_RTCSRC_TOSC32 CLK_RTCSRC_TOSC32_gc |
32.768kHz from crystal oscillator TOSC More... | |
#define | SYSCLK_RTCSRC_RCOSC32 CLK_RTCSRC_RCOSC32_gc |
32.768kHz from internal RC oscillator More... | |
#define | SYSCLK_RTCSRC_EXTCLK CLK_RTCSRC_EXTCLK_gc |
External clock on TOSC1. More... | |
Querying the system clock and its derived clocks | |
static uint32_t | sysclk_get_main_hz (void) |
Return the current rate in Hz of the main system clock. More... | |
static uint32_t | sysclk_get_per4_hz (void) |
Return the current rate in Hz of clk_PER4. More... | |
static uint32_t | sysclk_get_per2_hz (void) |
Return the current rate in Hz of clk_PER2. More... | |
static uint32_t | sysclk_get_per_hz (void) |
Return the current rate in Hz of clk_PER. More... | |
static uint32_t | sysclk_get_cpu_hz (void) |
Return the current rate in Hz of the CPU clock. More... | |
static uint32_t | sysclk_get_peripheral_bus_hz (const volatile void *module) |
Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral. More... | |
Enabling and disabling synchronous clocks | |
void | sysclk_enable_module (enum sysclk_port_id port, uint8_t id) |
Enable the clock to peripheral id on port port. More... | |
void | sysclk_disable_module (enum sysclk_port_id port, uint8_t id) |
Disable the clock to peripheral id on port port. More... | |
static void | sysclk_enable_peripheral_clock (const volatile void *module) |
Enable a peripheral's clock from its base address. More... | |
static void | sysclk_disable_peripheral_clock (const volatile void *module) |
Disable a peripheral's clock from its base address. More... | |
static bool | sysclk_module_is_enabled (enum sysclk_port_id port, uint8_t id) |
Check if the synchronous clock is enabled for a module. More... | |
System Clock Source and Prescaler configuration | |
static void | sysclk_set_prescalers (uint8_t psadiv, uint8_t psbcdiv) |
Set system clock prescaler configuration. More... | |
static void | sysclk_set_source (uint8_t src) |
Change the source of the main system clock. More... | |
static void | sysclk_lock (void) |
Lock the system clock configuration. More... | |
RTC clock source control | |
static void | sysclk_rtcsrc_enable (uint8_t id) |
Enable RTC clock with specified clock source. More... | |
static void | sysclk_rtcsrc_disable (void) |
Disable RTC clock. More... | |
System Clock Initialization | |
void | sysclk_init (void) |
Initialize the synchronous clock system. More... | |
#define SYSCLK_AC PR_AC_bm |
Analog Comparator.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_ADC PR_ADC_bm |
A/D Converter.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_AES PR_AES_bm |
AES Module.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_DAC PR_DAC_bm |
D/A Converter.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_DMA PR_DMA_bm |
DMA Controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_EBI PR_EBI_bm |
Ext Bus Interface.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_EDMA PR_EDMA_bm |
EDMA Controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_EVSYS PR_EVSYS_bm |
Event System.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_HIRES PR_HIRES_bm |
Hi-Res Extension.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_PSADIV_1 CLK_PSADIV_1_gc |
Do not prescale.
Referenced by sysclk_init().
#define SYSCLK_PSADIV_128 CLK_PSADIV_128_gc |
Prescale CLKper4 by 128.
#define SYSCLK_PSADIV_16 CLK_PSADIV_16_gc |
Prescale CLKper4 by 16.
#define SYSCLK_PSADIV_2 CLK_PSADIV_2_gc |
Prescale CLKper4 by 2.
#define SYSCLK_PSADIV_256 CLK_PSADIV_256_gc |
Prescale CLKper4 by 256.
#define SYSCLK_PSADIV_32 CLK_PSADIV_32_gc |
Prescale CLKper4 by 32.
#define SYSCLK_PSADIV_4 CLK_PSADIV_4_gc |
Prescale CLKper4 by 4.
#define SYSCLK_PSADIV_512 CLK_PSADIV_512_gc |
Prescale CLKper4 by 512.
Referenced by sysclk_get_per4_hz().
#define SYSCLK_PSADIV_64 CLK_PSADIV_64_gc |
Prescale CLKper4 by 64.
#define SYSCLK_PSADIV_8 CLK_PSADIV_8_gc |
Prescale CLKper4 by 8.
#define SYSCLK_PSBCDIV_1_1 CLK_PSBCDIV_1_1_gc |
Do not prescale.
Referenced by sysclk_get_per2_hz(), and sysclk_init().
#define SYSCLK_PSBCDIV_1_2 CLK_PSBCDIV_1_2_gc |
Prescale CLKper and CLKcpu by 2.
Referenced by sysclk_get_per2_hz().
#define SYSCLK_PSBCDIV_2_2 CLK_PSBCDIV_2_2_gc |
Prescale CLKper2 by 2, CLKper and CLKcpu by 4.
Referenced by sysclk_get_per2_hz().
#define SYSCLK_PSBCDIV_4_1 CLK_PSBCDIV_4_1_gc |
Prescale CLKper2, CLKper and CLKcpu by 4.
Referenced by sysclk_get_per2_hz().
#define SYSCLK_RTC PR_RTC_bm |
Real-Time Counter.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_RTCSRC_EXTCLK CLK_RTCSRC_EXTCLK_gc |
External clock on TOSC1.
Referenced by sysclk_rtcsrc_enable().
#define SYSCLK_RTCSRC_RCOSC CLK_RTCSRC_RCOSC_gc |
1.024kHz from 32.768kHz internal RC oscillator
Referenced by sysclk_rtcsrc_enable().
#define SYSCLK_RTCSRC_RCOSC32 CLK_RTCSRC_RCOSC32_gc |
32.768kHz from internal RC oscillator
Referenced by sysclk_rtcsrc_enable().
#define SYSCLK_RTCSRC_TOSC CLK_RTCSRC_TOSC_gc |
1.024kHz from 32.768kHz crystal oscillator TOSC
Referenced by sysclk_rtcsrc_enable().
#define SYSCLK_RTCSRC_TOSC32 CLK_RTCSRC_TOSC32_gc |
32.768kHz from crystal oscillator TOSC
Referenced by sysclk_rtcsrc_enable().
#define SYSCLK_RTCSRC_ULP CLK_RTCSRC_ULP_gc |
1kHz from internal ULP oscillator.
Low precision
#define SYSCLK_SPI PR_SPI_bm |
SPI controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_SRC_PLL CLK_SCLKSEL_PLL_gc |
Phase-Locked Loop.
Referenced by sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SRC_RC2MHZ CLK_SCLKSEL_RC2M_gc |
Internal 2 MHz RC oscillator.
Referenced by sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SRC_RC32KHZ CLK_SCLKSEL_RC32K_gc |
Internal 32 KHz RC oscillator.
Referenced by sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SRC_RC32MHZ CLK_SCLKSEL_RC32M_gc |
Internal 32 MHz RC oscillator.
Referenced by sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_SRC_XOSC CLK_SCLKSEL_XOSC_gc |
External oscillator.
Referenced by sysclk_get_main_hz(), and sysclk_init().
#define SYSCLK_TC0 PR_TC0_bm |
Timer/Counter 0.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_TC1 PR_TC1_bm |
Timer/Counter 1.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_TC4 PR_TC4_bm |
Timer/Counter 0.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_TC5 PR_TC5_bm |
Timer/Counter 1.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_TWI PR_TWI_bm |
TWI controller.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USART0 PR_USART0_bm |
USART 0.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USART1 PR_USART1_bm |
USART 1.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
#define SYSCLK_USB PR_USB_bm |
USB Module.
#define SYSCLK_XCL PR_XCL_bm |
USB Module.
Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().
enum sysclk_port_id |
void sysclk_disable_module | ( | enum sysclk_port_id | port, |
uint8_t | id | ||
) |
Disable the clock to peripheral id on port port.
port | ID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions). |
id | The ID (bitmask) of the peripheral module to be disabled. |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by sysclk_disable_peripheral_clock().
|
inlinestatic |
Disable a peripheral's clock from its base address.
Disables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be disabled also.
module | Pointer to the module's base address. |
References Assert, SYSCLK_AC, SYSCLK_ADC, SYSCLK_AES, SYSCLK_DAC, sysclk_disable_module(), SYSCLK_DMA, SYSCLK_EBI, SYSCLK_EDMA, SYSCLK_EVSYS, SYSCLK_HIRES, SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, SYSCLK_PORT_F, SYSCLK_PORT_GEN, SYSCLK_RTC, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TC4, SYSCLK_TC5, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, and SYSCLK_XCL.
void sysclk_enable_module | ( | enum sysclk_port_id | port, |
uint8_t | id | ||
) |
Enable the clock to peripheral id on port port.
port | ID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions). |
id | The ID (bitmask) of the peripheral module to be enabled. |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by spi_master_init(), and sysclk_enable_peripheral_clock().
|
inlinestatic |
Enable a peripheral's clock from its base address.
Enables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be enabled also.
module | Pointer to the module's base address. |
References Assert, SYSCLK_AC, SYSCLK_ADC, SYSCLK_AES, SYSCLK_DAC, SYSCLK_DMA, SYSCLK_EBI, SYSCLK_EDMA, sysclk_enable_module(), SYSCLK_EVSYS, SYSCLK_HIRES, SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, SYSCLK_PORT_F, SYSCLK_PORT_GEN, SYSCLK_RTC, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TC4, SYSCLK_TC5, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, and SYSCLK_XCL.
|
inlinestatic |
Return the current rate in Hz of the CPU clock.
References sysclk_get_per_hz().
Referenced by spi_master_setup_device().
|
inlinestatic |
Return the current rate in Hz of the main system clock.
References BOARD_XOSC_HZ, CONFIG_OSC_RC32_CAL, CONFIG_SYSCLK_SOURCE, pll_get_default_rate, SYSCLK_SRC_PLL, SYSCLK_SRC_RC2MHZ, SYSCLK_SRC_RC32KHZ, SYSCLK_SRC_RC32MHZ, and SYSCLK_SRC_XOSC.
Referenced by sysclk_get_per4_hz().
|
inlinestatic |
Return the current rate in Hz of clk_PER2.
This clock can run up to two times faster than the CPU clock.
References CONFIG_SYSCLK_PSBCDIV, sysclk_get_per4_hz(), SYSCLK_PSBCDIV_1_1, SYSCLK_PSBCDIV_1_2, SYSCLK_PSBCDIV_2_2, and SYSCLK_PSBCDIV_4_1.
Referenced by sysclk_get_per_hz(), and sysclk_get_peripheral_bus_hz().
|
inlinestatic |
Return the current rate in Hz of clk_PER4.
This clock can run up to four times faster than the CPU clock.
References CONFIG_SYSCLK_PSADIV, sysclk_get_main_hz(), and SYSCLK_PSADIV_512.
Referenced by sysclk_get_per2_hz(), and sysclk_get_peripheral_bus_hz().
|
inlinestatic |
Return the current rate in Hz of clk_PER.
This clock always runs at the same rate as the CPU clock unless the divider is set.
References CONFIG_SYSCLK_PSBCDIV, and sysclk_get_per2_hz().
Referenced by sysclk_get_cpu_hz(), and sysclk_get_peripheral_bus_hz().
|
inlinestatic |
Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral.
module | Pointer to the module's base address. |
References Assert, sysclk_get_per2_hz(), sysclk_get_per4_hz(), and sysclk_get_per_hz().
void sysclk_init | ( | void | ) |
Initialize the synchronous clock system.
This function will initialize the system clock and its source. This includes:
Since all non-essential peripheral clocks are initially disabled, it is the responsibility of the peripheral driver to re-enable any clocks that are needed for normal operation.
References Assert, ccp_write_io(), CONFIG_OSC_AUTOCAL_RC32MHZ_REF_OSC, CONFIG_OSC_RC32_CAL, CONFIG_SYSCLK_PSADIV, CONFIG_SYSCLK_PSBCDIV, CONFIG_SYSCLK_SOURCE, LSB, MSB, nvm_get_production_signature_row_offset, nvm_read_production_signature_row(), osc_disable(), osc_enable(), osc_enable_autocalibration(), OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_RC8MHZ, OSC_ID_USBSOF, OSC_ID_XOSC, osc_user_calibration(), osc_wait_ready(), pll_enable_config_defaults(), PLL_SRC_RC2MHZ, SYSCLK_PORT_F, SYSCLK_PSADIV_1, SYSCLK_PSBCDIV_1_1, sysclk_rtcsrc_enable(), sysclk_set_prescalers(), SYSCLK_SRC_PLL, SYSCLK_SRC_RC2MHZ, SYSCLK_SRC_RC32KHZ, SYSCLK_SRC_RC32MHZ, SYSCLK_SRC_XOSC, and UNUSED.
Referenced by main().
|
inlinestatic |
Lock the system clock configuration.
This function will lock the current system clock source and prescaler configuration, preventing any further changes.
References ccp_write_io().
|
inlinestatic |
Check if the synchronous clock is enabled for a module.
port | ID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions). |
id | The ID (bitmask) of the peripheral module to check (one of the SYSCLK_* module definitions). |
true | If the clock for module id on port is enabled. |
false | If the clock for module id on port is disabled. |
|
inlinestatic |
Disable RTC clock.
|
inlinestatic |
Enable RTC clock with specified clock source.
id | RTC clock source ID. Select from SYSCLK_RTCSRC_ULP, SYSCLK_RTCSRC_RCOSC, SYSCLK_RTCSRC_TOSC, SYSCLK_RTCSRC_RCOSC32, SYSCLK_RTCSRC_TOSC32 or SYSCLK_RTCSRC_EXTCLK |
References Assert, osc_enable(), OSC_ID_RC32KHZ, OSC_ID_XOSC, osc_wait_ready(), SYSCLK_RTCSRC_EXTCLK, SYSCLK_RTCSRC_RCOSC, SYSCLK_RTCSRC_RCOSC32, SYSCLK_RTCSRC_TOSC, and SYSCLK_RTCSRC_TOSC32.
Referenced by sysclk_init().
|
inlinestatic |
Set system clock prescaler configuration.
This function will change the system clock prescaler configuration to match the parameters.
psadiv | The prescaler A setting (one of the SYSCLK_PSADIV_* definitions). This determines the clkPER4 frequency. |
psbcdiv | The prescaler B and C settings (one of the SYSCLK_PSBCDIV_* definitions). These determine the clkPER2, clkPER and clkCPU frequencies. |
References ccp_write_io().
Referenced by sysclk_init().
|
inlinestatic |
Change the source of the main system clock.
src | The new system clock source. Must be one of the constants from the System Clock Sources section. |
References ccp_write_io().