Microchip® Advanced Software Framework

ui.h File Reference

Common User Interface for MSC application.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void ui_init (void)
 Initializes the user interface. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
Callback to show the MSC read and write access
void ui_start_read (void)
 
void ui_stop_read (void)
 
void ui_start_write (void)
 
void ui_stop_write (void)
 

void ui_init ( void  )

Initializes the user interface.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, LED3_GPIO, LED_Off, and LED_On.

Referenced by main().

void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED0_GPIO, LED1_GPIO, LED2_GPIO, LED3_GPIO, and LED_Off.

Referenced by main(), and main_suspend_action().

void ui_process ( uint16_t  framenumber)

This process is called each 1ms It is called only if the USB interface is enabled.

Parameters
framenumberCurrent frame number

References LED1_GPIO, LED_Off, and LED_On.

Referenced by main_sof_action().

void ui_start_read ( void  )

References LED2_GPIO, and LED_On.

void ui_start_write ( void  )

References LED3_GPIO, and LED_On.

void ui_stop_read ( void  )

References LED2_GPIO, and LED_Off.

void ui_stop_write ( void  )

References LED3_GPIO, and LED_Off.

void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0_GPIO, and LED_On.

Referenced by main_resume_action().