Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
ASF USB Device MSC

Human interface on STK600:

Introduction

This example shows how to implement a USB Device Mass Storage on Atmel MCU with USB module.

Startup

The example uses all memories available on the board and connects these to USB Device Mass Storage stack. After loading firmware, connect the board (EVKxx,Xplain,...) to the USB Host. When connected to a USB host system this application allows to display all available memories as a removable disks in the Unix/Mac/Windows operating systems.

Note
This example uses the native MSC driver on Unix/Mac/Windows OS, except for Win98.
  • Led 0 is on when USB line is in IDLE mode, and off in SUSPEND mode
  • Led 1 blinks when USB host has checked and enabled MSC interface
  • Led 2 is on during read operation
  • Led 3 is on during write operation

Setup for STK600:

  • LEDS connector is connected to PORTA
  • DataFlash should be connected:
    • PC4 to /CS pin on DataFlash connector
    • PC7 to SCK pin on DataFlash connector
    • PC6 to SO pin on DataFlash connector
    • PC5 to SI pin on DataFlash connector
  • SWITCHES are connected to PORTB
  • Warning! The AREF0 jumper must be removed because AREF0 connected on PORTA0 overrides led 0.
  • Warning! The AREF1 jumper must be removed because AREF1 connected on PORTB0 overrides switch 0.

About example

The example uses the following module groups:

  • Basic modules: Startup, board, clock, interrupt, power management
  • USB Device stack and MSC modules:
    services/usb/
    services/usb/udc/
    services/usb/class/msc/
  • Specific implementation:
    • main.c,
      initializes clock
      initializes interrupt
      manages UI
    • specific implementation for each target "./examples/product_board/":
      • conf_foo.h configuration of each module
      • ui.c implement of user's interface (leds)

1 The memory data transfers are done outside USB interrupt routine. This is done in the MSC process ("udi_msc_process_trans()") called by main loop.