Declaration of main function used by MSC unit test.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_msc_read_finish (void) |
Allows to check that a memory read access works. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vbus_action (bool b_high) |
Called when Vbus line state change. More... | |
void | memories_initialization (void) |
Initialize the memories used by examples. More... | |
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
References main_b_msc_enumerated.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
References main_b_msc_enumerated.
void main_msc_read_finish | ( | void | ) |
Allows to check that a memory read access works.
References main_b_msc_read.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References main_b_suspend_event.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_sof_event.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References main_b_resume_event.
void main_vbus_action | ( | bool | b_high | ) |
void memories_initialization | ( | void | ) |
Initialize the memories used by examples.
References at45dbx_init().
Referenced by run_usb_msc_test().