License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick start guide for the | NAND Flash module |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Direct Memory Access Controller Driver | |
Examples for Direct Memory Access Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3A/3U/3X/4E DMA Controller (DMAC) Driver |
 Quick Start Guide for the DMAC driver | This is the quick start guide for the SAM3A/3U/3X/4E DMA Controller (DMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 SAM Direct Memory Access Controller - Example Memory to Memory Transfer | |
Document Revision History | |
Quick Start Guide for the System Clock Management service (SAM3A) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick start guide for USB device Mass Storage module (UDI MSC) | This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 MSC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
"SAM3X-EK - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM3X-EK - Board informations" | This page lists several definition related to the board description |
"SAM3X-EK - PIO definitions" | This pages lists all the pio definitions |
"SAM3X-EK - USB device" | |
"SAM3X-EK - External components" | This page lists the definitions related to external on-board components located in the board.h file for the SAM3X-EK |
"SAM3X-EK - Memories" | This page lists definitions related to internal & external on-board memories |
Todo List | |
Deprecated List | |