Common abstraction layer for memory interfaces.
It provides interfaces between: Memory and USB, Memory and RAM, Memory and Memory. Common API for XMEGA and UC3.
Macros | |
#define | SECTOR_SIZE 512 |
Enumerations | |
enum | Ctrl_status { CTRL_GOOD = PASS, CTRL_FAIL = FAIL, CTRL_NO_PRESENT = FAIL + 1, CTRL_BUSY = FAIL + 2 } |
Status returned by CTRL_ACCESS interfaces. More... | |
LUN IDs | |
#define | LUN_ID_0 (0) |
First static LUN. More... | |
#define | LUN_ID_1 (LUN_ID_0 + LUN_0) |
#define | LUN_ID_2 (LUN_ID_1 + LUN_1) |
#define | LUN_ID_3 (LUN_ID_2 + LUN_2) |
#define | LUN_ID_4 (LUN_ID_3 + LUN_3) |
#define | LUN_ID_5 (LUN_ID_4 + LUN_4) |
#define | LUN_ID_6 (LUN_ID_5 + LUN_5) |
#define | LUN_ID_7 (LUN_ID_6 + LUN_6) |
#define | MAX_LUN (LUN_ID_7 + LUN_7) |
Number of static LUNs. More... | |
#define | LUN_ID_USB (MAX_LUN) |
First dynamic LUN (USB host mass storage). More... | |
Control Interface | |
U8 | get_nb_lun (void) |
Returns the number of LUNs. More... | |
U8 | get_cur_lun (void) |
Returns the current LUN. More... | |
Ctrl_status | mem_test_unit_ready (U8 lun) |
Tests the memory state and initializes the memory if required. More... | |
Ctrl_status | mem_read_capacity (U8 lun, U32 *u32_nb_sector) |
Returns the address of the last valid sector (512 bytes) in the memory. More... | |
U8 | mem_sector_size (U8 lun) |
Returns the size of the physical sector. More... | |
bool | mem_unload (U8 lun, bool unload) |
Unload/load the medium. More... | |
bool | mem_wr_protect (U8 lun) |
Returns the write-protection state of the memory. More... | |
bool | mem_removal (U8 lun) |
Tells whether the memory is removable. More... | |
const char * | mem_name (U8 lun) |
Returns a pointer to the LUN name. More... | |
MEM <-> USB Interface | |
Ctrl_status | memory_2_usb (U8 lun, U32 addr, U16 nb_sector) |
Transfers data from the memory to USB. More... | |
Ctrl_status | usb_2_memory (U8 lun, U32 addr, U16 nb_sector) |
Transfers data from USB to the memory. More... | |
#define LUN_ID_0 (0) |
First static LUN.
Referenced by get_cur_lun().
#define LUN_ID_USB (MAX_LUN) |
First dynamic LUN (USB host mass storage).
Referenced by mem_read_capacity(), mem_sector_size(), mem_test_unit_ready(), mem_unload(), and mem_wr_protect().
Number of static LUNs.
Referenced by get_nb_lun(), mem_name(), mem_read_capacity(), mem_removal(), mem_sector_size(), mem_test_unit_ready(), mem_unload(), mem_wr_protect(), memory_2_usb(), and usb_2_memory().
#define SECTOR_SIZE 512 |
Referenced by nand_flash_read_capacity(), nand_flash_usb_read_10(), and nand_flash_usb_write_10().
enum Ctrl_status |
U8 get_cur_lun | ( | void | ) |
U8 get_nb_lun | ( | void | ) |
Returns the number of LUNs.
References Ctrl_access_lock, Ctrl_access_unlock, Lun_usb_get_lun, and MAX_LUN.
const char* mem_name | ( | U8 | lun | ) |
Returns a pointer to the LUN name.
lun | Logical Unit Number. |
References ENABLE, lun_desc, LUN_USB, LUN_USB_NAME, MAX_LUN, name, and UNUSED.
Referenced by udi_msc_spc_inquiry().
Ctrl_status mem_read_capacity | ( | U8 | lun, |
U32 * | u32_nb_sector | ||
) |
Returns the address of the last valid sector (512 bytes) in the memory.
lun | Logical Unit Number. |
u32_nb_sector | Pointer to the address of the last valid sector. |
References Ctrl_access_lock, Ctrl_access_unlock, CTRL_FAIL, lun_desc, LUN_ID_USB, Lun_usb_read_capacity, MAX_LUN, and read_capacity.
Referenced by udi_msc_sbc_read_capacity().
Tells whether the memory is removable.
lun | Logical Unit Number. |
true
if the memory is removable, else false
. References Ctrl_access_lock, Ctrl_access_unlock, lun_desc, Lun_usb_removal, MAX_LUN, removal, and UNUSED.
Referenced by udi_msc_spc_inquiry().
Returns the size of the physical sector.
lun | Logical Unit Number. |
References Ctrl_access_lock, Ctrl_access_unlock, ENABLE, LUN_ID_USB, LUN_USB, Lun_usb_read_sector_size, and MAX_LUN.
Ctrl_status mem_test_unit_ready | ( | U8 | lun | ) |
Tests the memory state and initializes the memory if required.
The TEST UNIT READY SCSI primary command allows an application client to poll a LUN until it is ready without having to allocate memory for returned data.
This command may be used to check the media status of LUNs with removable media.
lun | Logical Unit Number. |
References Ctrl_access_lock, Ctrl_access_unlock, CTRL_FAIL, lun_desc, LUN_ID_USB, Lun_usb_test_unit_ready, MAX_LUN, and test_unit_ready.
Referenced by udi_msc_spc_testunitready_global().
Unload/load the medium.
lun | Logical Unit Number. |
unload | true to unload the medium, false to load the medium. |
true
if unload/load success, else false
. References Ctrl_access_lock, Ctrl_access_unlock, ENABLE, lun_desc, LUN_ID_USB, LUN_USB, MAX_LUN, unload, and UNUSED.
Referenced by udi_msc_sbc_start_stop().
Returns the write-protection state of the memory.
lun | Logical Unit Number. |
true
if the memory is write-protected, else false
.References Ctrl_access_lock, Ctrl_access_unlock, lun_desc, LUN_ID_USB, Lun_usb_wr_protect, MAX_LUN, and wr_protect.
Referenced by udi_msc_sbc_trans(), and udi_msc_spc_mode_sense().
Ctrl_status memory_2_usb | ( | U8 | lun, |
U32 | addr, | ||
U16 | nb_sector | ||
) |
Transfers data from the memory to USB.
lun | Logical Unit Number. |
addr | Address of first memory sector to read. |
nb_sector | Number of sectors to transfer. |
References Ctrl_access_lock, Ctrl_access_unlock, CTRL_FAIL, lun_desc, MAX_LUN, memory_start_read_action, memory_stop_read_action, and usb_read_10.
Referenced by udi_msc_process_trans().
Ctrl_status usb_2_memory | ( | U8 | lun, |
U32 | addr, | ||
U16 | nb_sector | ||
) |
Transfers data from USB to the memory.
lun | Logical Unit Number. |
addr | Address of first memory sector to write. |
nb_sector | Number of sectors to transfer. |
References Ctrl_access_lock, Ctrl_access_unlock, CTRL_FAIL, lun_desc, MAX_LUN, memory_start_write_action, memory_stop_write_action, and usb_write_10.
Referenced by udi_msc_process_trans().