License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick start guide for the | NAND Flash module |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the System Clock Management service (SAM4S) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Advanced use case - Peripheral Bus Clock Management (SAM4S) | |
Extra Information for Peripheral DMA Controller | |
Examples for Peripheral DMA Controller | This is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver |
![|](ftv2vertline.png) Quick Start Guide for PDC - Basic | This is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver |
![|](ftv2vertline.png) Peripheral DMA Controller Example | |
Document Revision History | |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
![|](ftv2vertline.png) Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
![|](ftv2vertline.png) Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![|](ftv2vertline.png) USART receive character and echo back | In this use case, the USART module is configured for: |
![|](ftv2vertline.png) USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick start guide for USB device Mass Storage module (UDI MSC) | This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
![|](ftv2vertline.png) MSC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
![|](ftv2vertline.png) Change USB speed | In this use case, the USB device is used with different USB speeds |
![|](ftv2vertline.png) Use USB strings | In this use case, the usual USB strings is added in the USB device |
![|](ftv2vertline.png) Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
![|](ftv2vertline.png) Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
![|](ftv2vertline.png) USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
"SAM4S-EK - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM4S-EK - Board informations" | This page lists several definition related to the board description |
"SAM4S-EK - USB device" | |
"SAM4S-EK - External components" | This page lists the definitions related to external on-board components located in the board.h file for the SAM4S-EK |
"SAM4S-EK - Memories" | This page lists definitions related to internal & external on-board memories |
Todo List | |
Deprecated List | |