Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
ASF USB host mass storage

Human interface on EVK1100 :

Introduction

This example shows how to implement a USB host mass storage on Atmel MCU with USB module.

Startup

After loading firmware, connect the board (EVKxx,Xplain,...) to a U-Disk (FAT/FAT32 are supported). This example creates a file "uhi_msc_test.txt" on all present U-disks.

  • PWR led is on when power present
  • Led 0 is on when USB OTG cable is plugged
  • Led 1 is on when Vbus is present
  • Led 2 is on when a device is connected
  • Led 3 blinks when the device is enumerated and USB in idle mode
    • The blink is slow (1s) with low speed device
    • The blink is normal (0.5s) with full speed device
    • The blink is fast (0.25s) with high speed device
  • Led 4 green is on when a read access is on going
  • Led 4 red is on when a write access is on going
  • Led 5 green is on when a LUN test is success
  • Led 5 red is on when a LUN test is unsuccessful
  • Switch PB0 allows to enter the device in suspend mode
  • Only Push joystick button can be used to wakeup USB device in suspend mode

Note: On board the LED labels are incremented of one. E.g. Led0 in software corresponding at Led1 label on board.

About example

The example uses the following module groups:

  • Basic modules: Startup, board, clock, interrupt, power management
  • USB host stack and MSC modules:
    services/usb/
    services/usb/uhc/
    services/usb/class/msc/host/
  • Specific implementation:
    • main.c,
      initializes clock
      initializes interrupt
      manages UI
    • specific implementation for each target "./examples/product_board/":
      • conf_foo.h configuration of each module
      • ui.c implement of user's interface (buttons, leds)