Microchip® Advanced Software Framework

usb_phdc_meta_data_desc_t Struct Reference

PHDC Meta-Data Descriptor Note: The optional meta-data field (0 to 253B) can follow this struct.

#include <usb_protocol_phdc.h>

Data Fields

uint8_t bDescriptorType
 PHDC descriptor type. More...
 
uint8_t bLength
 Size of this descriptor in bytes. More...
 

uint8_t usb_phdc_meta_data_desc_t::bDescriptorType

PHDC descriptor type.

uint8_t usb_phdc_meta_data_desc_t::bLength

Size of this descriptor in bytes.