PHDC QoS Descriptor.
#include <usb_protocol_phdc.h>
Data Fields | |
uint8_t | bDescriptorType |
PHDC descriptor type. More... | |
uint8_t | bLength |
Size of this descriptor in bytes. More... | |
uint8_t | bmLatencyReliability |
If bQoSEncodingVersion = 01h,. More... | |
uint8_t | bQoSEncodingVersion |
01h = version 1 QoS information encoding More... | |
uint8_t usb_phdc_qos_desc_t::bDescriptorType |
PHDC descriptor type.
uint8_t usb_phdc_qos_desc_t::bLength |
Size of this descriptor in bytes.
uint8_t usb_phdc_qos_desc_t::bmLatencyReliability |
If bQoSEncodingVersion = 01h,.
then this bitmap refers to the latency/reliability bin for the QoS data
uint8_t usb_phdc_qos_desc_t::bQoSEncodingVersion |
01h = version 1 QoS information encoding