Main functions.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
int | main (void) |
Main function. Execution starts here. More... | |
void | main_phdc_disable (void) |
Called by PHDC interface Callback running when USB Host disable PHDC interface. More... | |
bool | main_phdc_enable (void) |
Called by PHDC interface Callback running when USB Host enable PHDC interface. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
Variables | |
static volatile bool | main_b_phdc_enable = false |
int main | ( | void | ) |
Main function. Execution starts here.
References board_init(), cpu_irq_enable, ieee11073_skeleton_process(), irq_initialize_vectors, main_b_phdc_enable, sleepmgr_enter_sleep(), sleepmgr_init(), system_init(), udc_start(), ui_association(), ui_init(), and ui_powerdown().
void main_phdc_disable | ( | void | ) |
Called by PHDC interface Callback running when USB Host disable PHDC interface.
References ieee11073_skeleton_disable(), and main_b_phdc_enable.
bool main_phdc_enable | ( | void | ) |
Called by PHDC interface Callback running when USB Host enable PHDC interface.
true | if phdc startup is ok |
References ieee11073_skeleton_enable(), and main_b_phdc_enable.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
References main_b_phdc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
References ui_powerdown().
Referenced by main(), main_phdc_disable(), main_phdc_enable(), and main_sof_action().