Microchip® Advanced Software Framework

conf_usb_host.h File Reference

USB host configuration file.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "uhi_vendor.h"
#include "ui.h"
#include "main.h"

Macros

#define USB_HOST_UHI   UHI_VENDOR
 USB Host Configuration. More...
 
#define USB_HOST_POWER_MAX   500
 Maximum current allowed on Vbus (mA) More...
 
#define USB_HOST_HS_SUPPORT
 Authorize the USB HUB support. More...
 
#define UHC_MODE_CHANGE(b_host_mode)   ui_usb_mode_change(b_host_mode)
 USB Host callbacks. More...
 
#define UHC_VBUS_CHANGE(b_present)   ui_usb_vbus_change(b_present)
 To notify that the Vbus level has changed Available only in USB hardware with Vbus monitoring. More...
 
#define UHC_VBUS_ERROR()   ui_usb_vbus_error()
 To notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring. More...
 
#define UHC_CONNECTION_EVENT(dev, b_present)   ui_usb_connection_event(dev,b_present)
 To notify that a device has been connected or disconnected. More...
 
#define UHC_SOF_EVENT()   main_usb_sof_event()
 Called when a USB device or the host have wake up the USB line. More...
 
#define UHC_ENUM_EVENT(dev, b_status)   ui_usb_enum_event(dev,b_status)
 Called when a USB device configuration must be chosen. More...
 
#define UHI_VENDOR_CHANGE(dev, b_plug)   main_usb_vendor_change(dev, b_plug)
 USB Interface Configuration. More...
 
#define UHI_VENDOR_VID_PID_LIST   {USB_VID_ATMEL, USB_PID_ATMEL_ASF_VENDOR_CLASS}
 

#define UHC_CONNECTION_EVENT (   dev,
  b_present 
)    ui_usb_connection_event(dev,b_present)

To notify that a device has been connected or disconnected.

Referenced by uhc_connection_tree().

#define UHC_ENUM_EVENT (   dev,
  b_status 
)    ui_usb_enum_event(dev,b_status)

Called when a USB device configuration must be chosen.

Thus, the application can choose either a configuration number for this device or a configuration number 0 to reject it. If callback not defined the configuration 1 is chosen. Called when a USB device enumeration is completed.

Referenced by uhc_enumeration_error(), uhc_enumeration_step13(), uhc_enumeration_step14(), uhc_enumeration_step15(), uhc_enumeration_step17_lpm(), and uhc_enumeration_step18_lpm().

#define UHC_MODE_CHANGE (   b_host_mode)    ui_usb_mode_change(b_host_mode)

USB Host callbacks.

To notify that the USB mode are switched automatically. This is possible only when ID pin is available.

Referenced by usb_dual_enable().

#define UHC_SOF_EVENT ( )    main_usb_sof_event()

Called when a USB device or the host have wake up the USB line.

Called for each received SOF each 1 ms Note: Available in High and Full speed mode

Referenced by _uhd_sof_interrupt().

#define UHC_VBUS_CHANGE (   b_present)    ui_usb_vbus_change(b_present)

To notify that the Vbus level has changed Available only in USB hardware with Vbus monitoring.

#define UHC_VBUS_ERROR ( )    ui_usb_vbus_error()

To notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring.

#define UHI_VENDOR_CHANGE (   dev,
  b_plug 
)    main_usb_vendor_change(dev, b_plug)

USB Interface Configuration.

Configuration of Vendor interface

Referenced by uhi_vendor_enable(), and uhi_vendor_uninstall().

#define UHI_VENDOR_VID_PID_LIST   {USB_VID_ATMEL, USB_PID_ATMEL_ASF_VENDOR_CLASS}

Referenced by uhi_vendor_install().

#define USB_HOST_HS_SUPPORT

Authorize the USB HUB support.

Authorize the USB host to run in High Speed

#define USB_HOST_POWER_MAX   500

Maximum current allowed on Vbus (mA)

Referenced by uhc_enumeration_step13().

#define USB_HOST_UHI   UHI_VENDOR

USB Host Configuration.

Array of UHI APIs Define the list of UHI supported by USB host.