Microchip® Advanced Software Framework

usb_cdc_union_desc_t Struct Reference

CDC Union Functional Descriptor.

#include <usb_protocol_cdc.h>

Data Fields

uint8_t bDescriptorSubtype
 
uint8_t bDescriptorType
 
uint8_t bFunctionLength
 
uint8_t bMasterInterface
 
uint8_t bSlaveInterface0
 

uint8_t usb_cdc_union_desc_t::bDescriptorSubtype
uint8_t usb_cdc_union_desc_t::bDescriptorType
uint8_t usb_cdc_union_desc_t::bFunctionLength
uint8_t usb_cdc_union_desc_t::bMasterInterface
uint8_t usb_cdc_union_desc_t::bSlaveInterface0