Microchip® Advanced Software Framework

virtual_mem.h File Reference

Management of the virtual memory.

This file manages the virtual memory.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include "conf_access.h"
#include "ctrl_access.h"

Macros

#define VMEM_SECTOR_SIZE   512
 

Functions

Ctrl_status virtual_read_capacity (uint32_t *u32_nb_sector)
 This function returns the address of the last valid sector. More...
 
bool virtual_removal (void)
 This function informs about the memory type. More...
 
Ctrl_status virtual_test_unit_ready (void)
 This function tests memory state, and starts memory initialization. More...
 
bool virtual_unload (bool unload)
 This function unloads/loads the memory. More...
 
Ctrl_status virtual_usb_read_10 (uint32_t addr, uint16_t nb_sector)
 This function transfers the memory data to the USB MSC interface. More...
 
Ctrl_status virtual_usb_write_10 (uint32_t addr, uint16_t nb_sector)
 This function transfers the USB MSC data to the memory. More...
 
bool virtual_wr_protect (void)
 This function returns the write-protected mode. More...
 

#define VMEM_SECTOR_SIZE   512

Referenced by virtual_usb_trans().