USB host driver for Mass Storage Class interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | uhi_msc_lun_t |
Logical Unit Number (LUN) structure information. More... | |
Macros | |
Interface with USB Host Core (UHC) | |
Definition and functions required by UHC. | |
#define | UHI_MSC |
Global definition which contains standard UHI API for UHC. More... | |
Typedefs | |
typedef void(* | uhi_msc_scsi_callback_t )(bool) |
Callback type used by uhi_msc_scsi() functions. More... | |
Enumerations | |
enum | lun_status_t { LUN_GOOD = 0, LUN_FAIL = 1, LUN_NOT_PRESENT = 2, LUN_BUSY = 3 } |
Status of LUN. More... | |
Functions | |
Functions Required by UHC | |
uhc_enum_status_t | uhi_msc_install (uhc_device_t *dev) |
Install interface. More... | |
void | uhi_msc_enable (uhc_device_t *dev) |
Enable the interface. More... | |
void | uhi_msc_uninstall (uhc_device_t *dev) |
Uninstall the interface (if installed). More... | |
UHI for Mass Storage Class | |
Common APIs used by high level application to use this USB host class. | |
bool | uhi_msc_is_available (void) |
Tests if the interface UHI Mass Storage is available. More... | |
uint8_t | uhi_msc_get_lun (void) |
Gives the number of LUN available. More... | |
uhi_msc_lun_t * | uhi_msc_get_lun_desc (uint8_t lun) |
Gives information about a LUN. More... | |
bool | uhi_msc_scsi_test_unit_ready (uint8_t lun, uhi_msc_scsi_callback_t callback) |
Checks and update the status of the LUN. More... | |
bool | uhi_msc_scsi_read_10 (uint8_t lun, uint32_t addr, uint8_t *ram, uint8_t nb_sector, uhi_msc_scsi_callback_t callback) |
Reads a LUN data section to RAM buffer. More... | |
bool | uhi_msc_scsi_write_10 (uint8_t lun, uint32_t addr, const uint8_t *ram, uint8_t nb_sector, uhi_msc_scsi_callback_t callback) |
Writes a RAM buffer in a LUN data section. More... | |
USB Host Mass Storage Interface for Control Access Module | |
Layer added on UHI MSC interface to allow the usage of control access module. The control access module provides a common access at all memories and it is used by the File Systems available in ASF. | |
uint8_t | uhi_msc_mem_get_lun (void) |
Gives the number of available LUN. More... | |
Ctrl_status | uhi_msc_mem_test_unit_ready (uint8_t lun) |
Checks and update the status of the LUN. More... | |
Ctrl_status | uhi_msc_mem_read_capacity (uint8_t lun, uint32_t *u32_nb_sector) |
Returns the capacity of the LUN. More... | |
uint8_t | uhi_msc_mem_read_sector_size (uint8_t lun) |
Returns the sector size of the LUN. More... | |
bool | uhi_msc_mem_wr_protect (uint8_t lun) |
Checks if the LUN is write protected. More... | |
bool | uhi_msc_mem_removal (void) |
Checks if the device is removed. More... | |
Ctrl_status | uhi_msc_mem_read_10_ram (uint32_t addr, void *ram) |
Reads 512 bytes from the current LUN. More... | |
Ctrl_status | uhi_msc_mem_write_10_ram (uint32_t addr, const void *ram) |
Writes 512 bytes to the current LUN. More... | |