This example will create a simple touch-enabled GUI on the display of the mXT143E Xplained, using the Widget Toolkit.
The widget library API can be found here, while the graphics service API can be found here. The maXTouch API can be found here.
This example has been tested with the mXT143E Xplained on the following kits:
On startup the example application will create a three icon button widgets, three soft button widgets and a text label. When an icon in the icon button group is touched, the label widget will be updated to reflect the selected icon. The soft buttons can be used to select and activate an icon button widget, simulating icon button navigation without the use of direct pointer or touch input on the icon widgets themselves.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.