Graphical Widget toolkit.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Typedefs | |
typedef bool(* | wtk_frame_handler_t )(struct wtk_frame *frame, win_command_t command_data) |
Frame command event handler callback. More... | |
Functions | |
struct win_window * | wtk_frame_as_child (struct wtk_frame *frame) |
This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting. More... | |
struct win_window * | wtk_frame_as_parent (struct wtk_frame *frame) |
This function returns a reference to the window that should be used as a parent for child widgets and windows. More... | |
struct wtk_frame * | wtk_frame_create (struct win_window *parent, struct win_area const *area, char const *caption, bool allow_resize, wtk_frame_handler_t frame_handler, void *custom_data) |
This function creates a new frame widget. More... | |
void * | wtk_frame_get_custom_data (struct wtk_frame const *frame) |
This function returns the custom data from the frame's attributes. More... | |