Microchip® Advanced Software Framework

Todo List
Global app_widget_launch (void)

Add code to set up button here.

Add code to set up basic frame here.

Global app_widget_launch (void)

Add code to set up button here.

Add code to set up basic frame here.

Group External oscillator
Need to measure the actual startup time on the hardware.
Group External oscillator
Need to measure the actual startup time on the hardware.
Global font_data_type
Add support for fonts in regular ram
Global pll_wait_for_lock (unsigned int pll_id)
Use a timeout to avoid waiting forever and hanging the system
Global sub_frame_draw_handler (struct win_window *win, struct win_clip_region const *clip)
Add code here to draw text on screen using the gfx_draw_string() function.
Global sysclk_get_main_hz (void)
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.
Global widget_frame_command_handler (struct wtk_basic_frame *frame, win_command_t command_data)
Add code here to handle button press.