Purpose
This example demonstrates basic functions of SD/MMC stack. It will read and write an SD/MMC card over MCI or SPI interface. It is a development base for a specific SD/MMC application which does not require a file system.
Description
The example executes the following sequences:
- For each card slot available on board:
- Wait for a card insertion
- Initialize an SD/MMC card.
- If the inserted card is an SD or MMC card, test read/write access.
- Write data into the card
- Read data from the card
- Verify the written data.
The example outputs the information through the standard output (stdio). To know the output used on the board, look in the conf_example.h file and connect a terminal to the correct stdio port.
While using Xplained Pro evaluation kits, please attach I/O1 Xplained Pro extension board to EXT1.
Usage
- Build the program and download it into the board.
- On the computer, open and configure a terminal application. Refer to conf_example.h file.
- Start the application.
- In the terminal window, the following text should appear:
* -- SD/MMC Card Example --
* -- Compiled: xxx xx xxxx xx:xx:xx --
* Please plug an SD/MMC card in slot 1.
* !!Warning, the data contained will be lost!!
*
- If the inserted card is a SD or MMC card, the following text should appear: A card has been connected. Card information: xxxx xxxx MB Write pattern... XXXXKBps [OK] Read... XXXXKBps [OK] Read and check pattern... [OK] Test finished, please unplugged card.