Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Implementation of SD/MMC/SDIO Stack

Data Structures

struct  sd_mmc_card
 SD/MMC card information structure. More...
 

Macros

#define driver   sd_mmc_spi
 
#define driver_adtc_start   ATPASTE2(driver, _adtc_start)
 
#define driver_adtc_stop   ATPASTE2(driver, _send_cmd)
 
#define driver_deselect_device   ATPASTE2(driver, _deselect_device)
 
#define driver_get_bus_width   ATPASTE2(driver, _get_bus_width)
 
#define driver_get_response   ATPASTE2(driver, _get_response)
 
#define driver_get_response_128   ATPASTE2(driver, _get_response_128)
 
#define driver_init   ATPASTE2(driver, _init)
 
#define driver_is_high_speed_capable   ATPASTE2(driver, _is_high_speed_capable)
 
#define driver_read_word   ATPASTE2(driver, _read_word)
 
#define driver_select_device   ATPASTE2(driver, _select_device)
 
#define driver_send_clock   ATPASTE2(driver, _send_clock)
 
#define driver_send_cmd   ATPASTE2(driver, _send_cmd)
 
#define driver_start_read_blocks   ATPASTE2(driver, _start_read_blocks)
 
#define driver_start_write_blocks   ATPASTE2(driver, _start_write_blocks)
 
#define driver_wait_end_of_read_blocks   ATPASTE2(driver, _wait_end_of_read_blocks)
 
#define driver_wait_end_of_write_blocks   ATPASTE2(driver, _wait_end_of_write_blocks)
 
#define driver_write_word   ATPASTE2(driver, _write_word)
 
#define IS_SDIO()   false
 
#define sd_mmc_debug(...)
 
#define SD_MMC_HSMCI_MEM_CNT   0
 
#define sd_mmc_is_mci()   (!sd_mmc_is_spi())
 
#define sd_mmc_is_spi()   true
 
#define SD_MMC_MCI_MEM_CNT   0
 
#define SD_MMC_MEM_CNT   SD_MMC_SPI_MEM_CNT
 
#define SD_MMC_VOLTAGE_SUPPORT
 This SD MMC stack supports only the high voltage. More...
 

Enumerations

enum  card_state {
  SD_MMC_CARD_STATE_READY = 0,
  SD_MMC_CARD_STATE_DEBOUNCE = 1,
  SD_MMC_CARD_STATE_INIT = 2,
  SD_MMC_CARD_STATE_UNUSABLE = 3,
  SD_MMC_CARD_STATE_NO_CARD = 4
}
 SD/MMC card states. More...
 

Functions

sd_mmc_err_t sd_mmc_check (uint8_t slot)
 Performs a card checks. More...
 
uint32_t sd_mmc_get_capacity (uint8_t slot)
 Get the memory capacity. More...
 
card_type_t sd_mmc_get_type (uint8_t slot)
 Get the card type. More...
 
card_version_t sd_mmc_get_version (uint8_t slot)
 Get the card version. More...
 
void sd_mmc_init (void)
 Initialize the SD/MMC stack and low level driver required. More...
 
sd_mmc_err_t sd_mmc_init_read_blocks (uint8_t slot, uint32_t start, uint16_t nb_block)
 Initialize the read blocks of data from the card. More...
 
sd_mmc_err_t sd_mmc_init_write_blocks (uint8_t slot, uint32_t start, uint16_t nb_block)
 Initialize the write blocks of data. More...
 
bool sd_mmc_is_write_protected (uint8_t slot)
 Get the card write protection status. More...
 
uint8_t sd_mmc_nb_slot (void)
 Return the number of slot available. More...
 
sd_mmc_err_t sd_mmc_start_read_blocks (void *dest, uint16_t nb_block)
 Start the read blocks of data from the card. More...
 
sd_mmc_err_t sd_mmc_start_write_blocks (const void *src, uint16_t nb_block)
 Start the write blocks of data. More...
 
sd_mmc_err_t sd_mmc_wait_end_of_read_blocks (bool abort)
 Wait the end of read blocks of data from the card. More...
 
sd_mmc_err_t sd_mmc_wait_end_of_write_blocks (bool abort)
 Wait the end of write blocks of data. More...
 

Variables

const uint32_t mmc_trans_multipliers [16]
 MMC transfer multiplier factor codes (1/10) list. More...
 
static struct sd_mmc_cardsd_mmc_card
 Pointer on current slot configurated. More...
 
static struct sd_mmc_card sd_mmc_cards [SD_MMC_MEM_CNT]
 SD/MMC card list Note: Initialize card detect pin fields if present. More...
 
static uint16_t sd_mmc_nb_block_remaining = 0
 Number of block remaining to read or write on the current transfer. More...
 
static uint16_t sd_mmc_nb_block_to_tranfer = 0
 Number of block to read or write on the current transfer. More...
 
static uint8_t sd_mmc_slot_sel
 Index of current slot configurated. More...
 
const uint32_t sd_mmc_trans_units [7]
 SD/MMC transfer rate unit codes (10K) list. More...
 
const uint32_t sd_trans_multipliers [16]
 SD transfer multiplier factor codes (1/10) list. More...
 

MMC, SD and SDIO commands process

static bool mmc_spi_op_cond (void)
 Sends operation condition command and read OCR (SPI only) More...
 
static bool mmc_mci_op_cond (void)
 Sends operation condition command and read OCR (MCI only) More...
 
static bool sd_spi_op_cond (uint8_t v2)
 Ask to all cards to send their operations conditions (SPI only). More...
 
static bool sd_mci_op_cond (uint8_t v2)
 Ask to all cards to send their operations conditions (MCI only). More...
 
static bool sdio_op_cond (void)
 
static bool sdio_get_max_speed (void)
 
static bool sdio_cmd52_set_bus_width (void)
 
static bool sdio_cmd52_set_high_speed (void)
 
static bool sd_cm6_set_high_speed (void)
 CMD6 for SD - Switch card in high speed mode. More...
 
static bool mmc_cmd6_set_bus_width (uint8_t bus_width)
 CMD6 for MMC - Switches the bus width mode. More...
 
static bool mmc_cmd6_set_high_speed (void)
 CMD6 for MMC - Switches in high speed mode. More...
 
static bool sd_cmd8 (uint8_t *v2)
 CMD8 for SD card - Send Interface Condition Command. More...
 
static bool mmc_cmd8 (uint8_t *b_authorize_high_speed)
 CMD8 - The card sends its EXT_CSD register as a block of data. More...
 
static bool sd_mmc_cmd9_spi (void)
 CMD9: Addressed card sends its card-specific data (CSD) on the CMD line spi. More...
 
static bool sd_mmc_cmd9_mci (void)
 CMD9: Addressed card sends its card-specific data (CSD) on the CMD line mci. More...
 
static void mmc_decode_csd (void)
 Decodes MMC CSD register. More...
 
static void sd_decode_csd (void)
 Decodes SD CSD register. More...
 
static bool sd_mmc_cmd13 (void)
 CMD13 - Addressed card sends its status register. More...
 
static bool sd_acmd6 (void)
 ACMD6 - Define the data bus width to 4 bits bus. More...
 
static bool sd_acmd51 (void)
 ACMD51 - Read the SD Configuration Register. More...
 

Internal function to process the initialization and install

static sd_mmc_err_t sd_mmc_select_slot (uint8_t slot)
 Select a card slot and initialize the associated driver. More...
 
static void sd_mmc_configure_slot (void)
 Configures the driver with the selected card configuration. More...
 
static void sd_mmc_deselect_slot (void)
 Deselect the current card slot. More...
 
static bool sd_mmc_spi_card_init (void)
 Initialize the SD card in SPI mode. More...
 
static bool sd_mmc_mci_card_init (void)
 Initialize the SD card in MCI mode. More...
 
static bool sd_mmc_spi_install_mmc (void)
 Initialize the MMC card in SPI mode. More...
 
static bool sd_mmc_mci_install_mmc (void)
 Initialize the MMC card in MCI mode. More...
 

Internal functions to manage a large timeout after a card insertion

#define SD_MMC_DEBOUNCE_TIMEOUT   1000
 

#define driver   sd_mmc_spi
#define driver_adtc_stop   ATPASTE2(driver, _send_cmd)
#define driver_deselect_device   ATPASTE2(driver, _deselect_device)

Referenced by sd_mmc_deselect_slot().

#define driver_get_bus_width   ATPASTE2(driver, _get_bus_width)
#define driver_get_response_128   ATPASTE2(driver, _get_response_128)

Referenced by sd_mmc_cmd9_mci().

#define driver_init   ATPASTE2(driver, _init)

Referenced by sd_mmc_init().

#define driver_is_high_speed_capable   ATPASTE2(driver, _is_high_speed_capable)
#define driver_read_word   ATPASTE2(driver, _read_word)

Referenced by mmc_cmd8().

#define driver_select_device   ATPASTE2(driver, _select_device)

Referenced by sd_mmc_configure_slot().

#define driver_send_clock   ATPASTE2(driver, _send_clock)
#define driver_start_read_blocks   ATPASTE2(driver, _start_read_blocks)
#define driver_start_write_blocks   ATPASTE2(driver, _start_write_blocks)
#define driver_wait_end_of_read_blocks   ATPASTE2(driver, _wait_end_of_read_blocks)
#define driver_wait_end_of_write_blocks   ATPASTE2(driver, _wait_end_of_write_blocks)
#define driver_write_word   ATPASTE2(driver, _write_word)
#define IS_SDIO ( )    false
#define SD_MMC_DEBOUNCE_TIMEOUT   1000
#define SD_MMC_HSMCI_MEM_CNT   0
#define sd_mmc_is_spi ( )    true

Referenced by sd_mmc_check(), and sd_mmc_cmd13().

#define SD_MMC_MCI_MEM_CNT   0
#define SD_MMC_VOLTAGE_SUPPORT
Value:
#define OCR_VDD_30_31
Definition: sd_mmc_protocol.h:740
#define OCR_VDD_32_33
Definition: sd_mmc_protocol.h:742
#define OCR_VDD_28_29
Definition: sd_mmc_protocol.h:738
#define OCR_VDD_29_30
Definition: sd_mmc_protocol.h:739
#define OCR_VDD_27_28
Definition: sd_mmc_protocol.h:737
#define OCR_VDD_31_32
Definition: sd_mmc_protocol.h:741

This SD MMC stack supports only the high voltage.

Referenced by mmc_mci_op_cond(), and sd_mci_op_cond().

enum card_state

SD/MMC card states.

Enumerator
SD_MMC_CARD_STATE_READY 

Ready to use.

SD_MMC_CARD_STATE_DEBOUNCE 

Debounce on going.

SD_MMC_CARD_STATE_INIT 

Initialization on going.

SD_MMC_CARD_STATE_UNUSABLE 

Unusable card.

SD_MMC_CARD_STATE_NO_CARD 

No SD/MMC card inserted.

static bool mmc_cmd6_set_bus_width ( uint8_t  bus_width)
static

CMD6 for MMC - Switches the bus width mode.

Note
CMD6 is valid under the "trans" state.
sd_mmc_card->bus_width is updated.
Parameters
bus_widthBus width to set
Returns
true if success, otherwise false

References sd_mmc_card::bus_width, CARD_STATUS_SWITCH_ERROR, driver_get_response, driver_send_cmd, MMC_CMD6_ACCESS_SET_BITS, MMC_CMD6_INDEX_BUS_WIDTH, MMC_CMD6_SWITCH, MMC_CMD6_VALUE_BUS_WIDTH_1BIT, MMC_CMD6_VALUE_BUS_WIDTH_4BIT, MMC_CMD6_VALUE_BUS_WIDTH_8BIT, and sd_mmc_debug.

Referenced by sd_mmc_mci_install_mmc().

static bool mmc_cmd6_set_high_speed ( void  )
static

CMD6 for MMC - Switches in high speed mode.

Note
CMD6 is valid under the "trans" state.
sd_mmc_card->high_speed is updated.
sd_mmc_card->clock is updated.
Returns
true if success, otherwise false

References CARD_STATUS_SWITCH_ERROR, sd_mmc_card::clock, driver_get_response, driver_send_cmd, sd_mmc_card::high_speed, MMC_CMD6_ACCESS_WRITE_BYTE, MMC_CMD6_INDEX_HS_TIMING, MMC_CMD6_SWITCH, MMC_CMD6_VALUE_HS_TIMING_ENABLE, and sd_mmc_debug.

Referenced by sd_mmc_mci_install_mmc().

static bool mmc_cmd8 ( uint8_t *  b_authorize_high_speed)
static

CMD8 - The card sends its EXT_CSD register as a block of data.

Parameters
b_authorize_high_speedPointer to update with the high speed support information
Returns
true if success, otherwise false

References sd_mmc_card::capacity, sd_mmc_card::csd, driver_adtc_start, driver_read_word, EXT_CSD_BSIZE, EXT_CSD_CARD_TYPE_INDEX, EXT_CSD_SEC_COUNT_INDEX, MMC_CMD8_SEND_EXT_CSD, MMC_CSD_C_SIZE, and MMC_CTYPE_52MHZ.

Referenced by sd_mmc_mci_install_mmc(), and sd_mmc_spi_install_mmc().

static bool mmc_mci_op_cond ( void  )
static

Sends operation condition command and read OCR (MCI only)

  • CMD1 sends operation condition command
  • CMD1 reads OCR
Returns
true if success, otherwise false

References CARD_TYPE_HC, driver_get_response, driver_send_cmd, MMC_MCI_CMD1_SEND_OP_COND, OCR_ACCESS_MODE_MASK, OCR_ACCESS_MODE_SECTOR, OCR_POWER_UP_BUSY, sd_mmc_debug, SD_MMC_VOLTAGE_SUPPORT, and sd_mmc_card::type.

Referenced by sd_mmc_mci_install_mmc().

static bool mmc_spi_op_cond ( void  )
static

Sends operation condition command and read OCR (SPI only)

  • CMD1 sends operation condition command
  • CMD58 reads OCR
Returns
true if success, otherwise false

References CARD_TYPE_HC, driver_get_response, driver_send_cmd, MMC_SPI_CMD1_SEND_OP_COND, OCR_ACCESS_MODE_MASK, OCR_ACCESS_MODE_SECTOR, R1_SPI_IDLE, sd_mmc_debug, SDMMC_SPI_CMD58_READ_OCR, and sd_mmc_card::type.

Referenced by sd_mmc_spi_install_mmc().

static bool sd_acmd51 ( void  )
static

ACMD51 - Read the SD Configuration Register.

Note
SD Card Configuration Register (SCR) provides information on the SD Memory Card's special features that were configured into the given card. The size of SCR register is 64 bits.
Returns
true if success, otherwise false

References CARD_VER_SD_1_0, CARD_VER_SD_1_10, CARD_VER_SD_2_0, CARD_VER_SD_3_0, driver_adtc_start, driver_send_cmd, driver_start_read_blocks, driver_wait_end_of_read_blocks, sd_mmc_card::rca, SD_ACMD51_SEND_SCR, SD_SCR_REG_BSIZE, SD_SCR_SD_SPEC, SD_SCR_SD_SPEC3, SD_SCR_SD_SPEC_1_0_01, SD_SCR_SD_SPEC_1_10, SD_SCR_SD_SPEC_2_00, SD_SCR_SD_SPEC_3_00, SDMMC_CMD55_APP_CMD, and sd_mmc_card::version.

Referenced by sd_mmc_mci_card_init(), and sd_mmc_spi_card_init().

static bool sd_acmd6 ( void  )
static

ACMD6 - Define the data bus width to 4 bits bus.

Returns
true if success, otherwise false

References sd_mmc_card::bus_width, driver_send_cmd, sd_mmc_card::rca, SD_ACMD6_SET_BUS_WIDTH, sd_mmc_debug, and SDMMC_CMD55_APP_CMD.

Referenced by sd_mmc_mci_card_init().

static bool sd_cmd8 ( uint8_t *  v2)
static

CMD8 for SD card - Send Interface Condition Command.

Note
Send SD Memory Card interface condition, which includes host supply voltage information and asks the card whether card supports voltage. Should be performed at initialization time to detect the card type.
Parameters
v2Pointer to v2 flag to update
Returns
true if success, otherwise false with a update of sd_mmc_err.

References driver_get_response, driver_send_cmd, SD_CMD8_HIGH_VOLTAGE, SD_CMD8_MASK_PATTERN, SD_CMD8_MASK_VOLTAGE, SD_CMD8_PATTERN, SD_CMD8_SEND_IF_COND, and sd_mmc_debug.

Referenced by sd_mmc_mci_card_init(), and sd_mmc_spi_card_init().

static bool sd_mci_op_cond ( uint8_t  v2)
static

Ask to all cards to send their operations conditions (MCI only).

  • ACMD41 sends operation condition command.
  • ACMD41 reads OCR
Parameters
v2Shall be 1 if it is a SD card V2
Returns
true if success, otherwise false

References CARD_TYPE_HC, driver_get_response, driver_send_cmd, OCR_CCS, OCR_POWER_UP_BUSY, SD_ACMD41_HCS, SD_MCI_ACMD41_SD_SEND_OP_COND, sd_mmc_debug, SD_MMC_VOLTAGE_SUPPORT, SDMMC_CMD55_APP_CMD, and sd_mmc_card::type.

Referenced by sd_mmc_mci_card_init().

sd_mmc_err_t sd_mmc_check ( uint8_t  slot)

Performs a card checks.

Parameters
slotCard slot to use
Return values
SD_MMC_OKCard ready
SD_MMC_INIT_ONGOINGInitialization on going
SD_MMC_ERR_NO_CARDCard not present in slot
Othervalue for error cases, see sd_mmc_err_t

References SD_MMC_CARD_STATE_READY, SD_MMC_CARD_STATE_UNUSABLE, sd_mmc_debug, sd_mmc_deselect_slot(), SD_MMC_ERR_UNUSABLE, SD_MMC_INIT_ONGOING, sd_mmc_is_spi, sd_mmc_mci_card_init(), sd_mmc_select_slot(), sd_mmc_spi_card_init(), and sd_mmc_card::state.

Referenced by main(), and sd_mmc_test_unit_ready().

static bool sd_mmc_cmd13 ( void  )
static

CMD13 - Addressed card sends its status register.

This function waits the clear of the busy flag

Returns
true if success, otherwise false

References CARD_STATUS_READY_FOR_DATA, driver_get_response, driver_send_cmd, sd_mmc_card::rca, sd_mmc_debug, sd_mmc_is_spi, SDMMC_MCI_CMD13_SEND_STATUS, and SDMMC_SPI_CMD13_SEND_STATUS.

Referenced by sd_mmc_init_read_blocks(), sd_mmc_spi_card_init(), and sd_mmc_spi_install_mmc().

static bool sd_mmc_cmd9_mci ( void  )
static

CMD9: Addressed card sends its card-specific data (CSD) on the CMD line mci.

Returns
true if success, otherwise false

References sd_mmc_card::csd, driver_get_response_128, driver_send_cmd, sd_mmc_card::rca, and SDMMC_MCI_CMD9_SEND_CSD.

Referenced by sd_mmc_mci_card_init(), and sd_mmc_mci_install_mmc().

static bool sd_mmc_cmd9_spi ( void  )
static

CMD9: Addressed card sends its card-specific data (CSD) on the CMD line spi.

Returns
true if success, otherwise false

References sd_mmc_card::csd, CSD_REG_BSIZE, driver_adtc_start, driver_start_read_blocks, driver_wait_end_of_read_blocks, sd_mmc_card::rca, and SDMMC_SPI_CMD9_SEND_CSD.

Referenced by sd_mmc_spi_card_init(), and sd_mmc_spi_install_mmc().

static void sd_mmc_configure_slot ( void  )
static
uint32_t sd_mmc_get_capacity ( uint8_t  slot)

Get the memory capacity.

Parameters
slotCard slot
Returns
Capacity (unit KB)

References sd_mmc_card::capacity, sd_mmc_deselect_slot(), SD_MMC_OK, and sd_mmc_select_slot().

Referenced by sd_mmc_read_capacity().

card_type_t sd_mmc_get_type ( uint8_t  slot)

Get the card type.

Parameters
slotCard slot
Returns
Card type (card_type_t)

References CARD_TYPE_UNKNOWN, sd_mmc_deselect_slot(), SD_MMC_OK, sd_mmc_select_slot(), and sd_mmc_card::type.

Referenced by sd_mmc_test_unit_ready().

card_version_t sd_mmc_get_version ( uint8_t  slot)

Get the card version.

Parameters
slotCard slot
Returns
Card version (card_version_t)

References CARD_VER_UNKNOWN, sd_mmc_deselect_slot(), SD_MMC_OK, sd_mmc_select_slot(), and sd_mmc_card::version.

void sd_mmc_init ( void  )

Initialize the SD/MMC stack and low level driver required.

Enable the PMC clock for the card detect pins

Enable the PMC clock for the card write protection pins

References driver_init, MREPEAT, SD_MMC_CARD_STATE_NO_CARD, sd_mmc_cards, SD_MMC_MEM_CNT, sd_mmc_slot_sel, and sd_mmc_card::state.

Referenced by main().

sd_mmc_err_t sd_mmc_init_read_blocks ( uint8_t  slot,
uint32_t  start,
uint16_t  nb_block 
)

Initialize the read blocks of data from the card.

Parameters
slotCard slot to use
startStart block number to to read.
nb_blockTotal number of blocks to be read.
Returns
return SD_MMC_OK if success, otherwise return an error code (sd_mmc_err_t).

References CARD_STATUS_ERR_RD_WR, CARD_TYPE_HC, driver_adtc_start, driver_get_response, SD_MMC_BLOCK_SIZE, sd_mmc_cmd13(), sd_mmc_debug, sd_mmc_deselect_slot(), SD_MMC_ERR_COMM, sd_mmc_is_mci, sd_mmc_nb_block_remaining, sd_mmc_nb_block_to_tranfer, SD_MMC_OK, sd_mmc_select_slot(), SDMMC_CMD17_READ_SINGLE_BLOCK, SDMMC_CMD18_READ_MULTIPLE_BLOCK, SDMMC_CMD_GET_INDEX, and sd_mmc_card::type.

Referenced by sd_mmc_mem_2_ram().

sd_mmc_err_t sd_mmc_init_write_blocks ( uint8_t  slot,
uint32_t  start,
uint16_t  nb_block 
)

Initialize the write blocks of data.

Parameters
slotCard slot to use
startStart block number to be written.
nb_blockTotal number of blocks to be written.
Returns
return SD_MMC_OK if success, otherwise return an error code (sd_mmc_err_t).

References CARD_STATUS_ERR_RD_WR, CARD_TYPE_HC, driver_adtc_start, driver_get_response, SD_MMC_BLOCK_SIZE, sd_mmc_debug, sd_mmc_deselect_slot(), SD_MMC_ERR_COMM, SD_MMC_ERR_WP, sd_mmc_is_mci, sd_mmc_is_write_protected(), sd_mmc_nb_block_remaining, sd_mmc_nb_block_to_tranfer, SD_MMC_OK, sd_mmc_select_slot(), SDMMC_CMD24_WRITE_BLOCK, SDMMC_CMD25_WRITE_MULTIPLE_BLOCK, SDMMC_CMD_GET_INDEX, and sd_mmc_card::type.

Referenced by sd_mmc_ram_2_mem().

bool sd_mmc_is_write_protected ( uint8_t  slot)

Get the card write protection status.

Parameters
slotCard slot
Returns
true, if write portected

References port_pin_get_input_level(), sd_mmc_cards, and UNUSED.

Referenced by sd_mmc_init_write_blocks(), and sd_mmc_wr_protect().

static bool sd_mmc_mci_card_init ( void  )
static
static bool sd_mmc_mci_install_mmc ( void  )
static

Initialize the MMC card in MCI mode.

Note
This function runs the initialization procedure and the identification process, then it sets the SD/MMC card in transfer state. At last, it will automaticly enable maximum bus width and transfer speed.
Returns
true if success, otherwise false

References CARD_VER_MMC_4, driver_get_bus_width, driver_is_high_speed_capable, driver_send_cmd, MMC_CMD3_SET_RELATIVE_ADDR, mmc_cmd6_set_bus_width(), mmc_cmd6_set_high_speed(), mmc_cmd8(), mmc_decode_csd(), mmc_mci_op_cond(), sd_mmc_card::rca, SD_MMC_BLOCK_SIZE, sd_mmc_cmd9_mci(), sd_mmc_configure_slot(), sd_mmc_slot_sel, SDMMC_CMD16_SET_BLOCKLEN, SDMMC_CMD2_ALL_SEND_CID, SDMMC_CMD7_SELECT_CARD_CMD, SDMMC_MCI_CMD0_GO_IDLE_STATE, and sd_mmc_card::version.

Referenced by sd_mmc_mci_card_init().

uint8_t sd_mmc_nb_slot ( void  )

Return the number of slot available.

Returns
Number of card slot available

References SD_MMC_MEM_CNT.

static sd_mmc_err_t sd_mmc_select_slot ( uint8_t  slot)
static

Select a card slot and initialize the associated driver.

Parameters
slotCard slot number
Return values
SD_MMC_ERR_SLOTWrong slot number
SD_MMC_ERR_NO_CARDNo card present on slot
SD_MMC_ERR_UNUSABLEUnusable card
SD_MMC_INIT_ONGOINGCard initialization requested
SD_MMC_OKCard present

Card Detect pins

References Assert, sd_mmc_card::bus_width, sd_mmc_card::cd_gpio, sd_mmc_card::clock, sd_mmc_card::high_speed, port_pin_get_input_level(), SD_MMC_0_CD_DETECT_VALUE, SD_MMC_CARD_STATE_DEBOUNCE, SD_MMC_CARD_STATE_INIT, SD_MMC_CARD_STATE_NO_CARD, SD_MMC_CARD_STATE_UNUSABLE, sd_mmc_cards, sd_mmc_configure_slot(), SD_MMC_ERR_NO_CARD, SD_MMC_ERR_SLOT, SD_MMC_ERR_UNUSABLE, SD_MMC_INIT_ONGOING, SD_MMC_MEM_CNT, sd_mmc_nb_block_remaining, SD_MMC_OK, sd_mmc_slot_sel, SDMMC_CLOCK_INIT, and sd_mmc_card::state.

Referenced by sd_mmc_check(), sd_mmc_get_capacity(), sd_mmc_get_type(), sd_mmc_get_version(), sd_mmc_init_read_blocks(), and sd_mmc_init_write_blocks().

static bool sd_mmc_spi_card_init ( void  )
static

Initialize the SD card in SPI mode.

Note
This function runs the initialization procedure and the identification process, then it sets the SD/MMC card in transfer state. At last, it will automaticly enable maximum bus width and transfer speed.
Returns
true if success, otherwise false

References CARD_TYPE_HC, CARD_TYPE_MMC, CARD_TYPE_SD, CARD_VER_UNKNOWN, driver_send_clock, driver_send_cmd, IS_SDIO, sd_mmc_card::rca, sd_acmd51(), sd_cmd8(), sd_decode_csd(), SD_MMC_BLOCK_SIZE, sd_mmc_cmd13(), sd_mmc_cmd9_spi(), sd_mmc_configure_slot(), sd_mmc_debug, sd_mmc_spi_install_mmc(), sd_spi_op_cond(), sdio_get_max_speed(), sdio_op_cond(), SDMMC_CMD16_SET_BLOCKLEN, SDMMC_SPI_CMD0_GO_IDLE_STATE, SDMMC_SPI_CMD59_CRC_ON_OFF, sd_mmc_card::type, and sd_mmc_card::version.

Referenced by sd_mmc_check().

static bool sd_mmc_spi_install_mmc ( void  )
static

Initialize the MMC card in SPI mode.

Note
This function runs the initialization procedure and the identification process, then it sets the SD/MMC card in transfer state. At last, it will automaticly enable maximum bus width and transfer speed.
Returns
true if success, otherwise false

References CARD_VER_MMC_4, driver_send_cmd, mmc_cmd8(), mmc_decode_csd(), mmc_spi_op_cond(), SD_MMC_BLOCK_SIZE, sd_mmc_cmd13(), sd_mmc_cmd9_spi(), sd_mmc_configure_slot(), SDMMC_CMD16_SET_BLOCKLEN, SDMMC_SPI_CMD0_GO_IDLE_STATE, SDMMC_SPI_CMD59_CRC_ON_OFF, and sd_mmc_card::version.

Referenced by sd_mmc_spi_card_init().

sd_mmc_err_t sd_mmc_start_read_blocks ( void *  dest,
uint16_t  nb_block 
)

Start the read blocks of data from the card.

Parameters
destPointer to read buffer.
nb_blockNumber of blocks to be read.
Returns
return SD_MMC_OK if started, otherwise return an error code (sd_mmc_err_t).

References Assert, driver_start_read_blocks, SD_MMC_ERR_COMM, sd_mmc_nb_block_remaining, and SD_MMC_OK.

Referenced by sd_mmc_mem_2_ram().

sd_mmc_err_t sd_mmc_start_write_blocks ( const void *  src,
uint16_t  nb_block 
)

Start the write blocks of data.

Parameters
srcPointer to write buffer.
nb_blockNumber of blocks to be written.
Returns
return SD_MMC_OK if started, otherwise return an error code (sd_mmc_err_t).

References Assert, driver_start_write_blocks, SD_MMC_ERR_COMM, sd_mmc_nb_block_remaining, and SD_MMC_OK.

Referenced by sd_mmc_ram_2_mem().

sd_mmc_err_t sd_mmc_wait_end_of_read_blocks ( bool  abort)

Wait the end of read blocks of data from the card.

Parameters
abortAbort reading process initialized by sd_mmc_init_read_blocks() after the reading issued by sd_mmc_start_read_blocks() is done
Returns
return SD_MMC_OK if success, otherwise return an error code (sd_mmc_err_t).

References driver_adtc_stop, driver_wait_end_of_read_blocks, sd_mmc_deselect_slot(), SD_MMC_ERR_COMM, sd_mmc_nb_block_remaining, sd_mmc_nb_block_to_tranfer, SD_MMC_OK, and SDMMC_CMD12_STOP_TRANSMISSION.

Referenced by sd_mmc_mem_2_ram().

sd_mmc_err_t sd_mmc_wait_end_of_write_blocks ( bool  abort)

Wait the end of write blocks of data.

Parameters
abortAbort writing process initialized by sd_mmc_init_write_blocks() after the writing issued by sd_mmc_start_write_blocks() is done
Returns
return SD_MMC_OK if success, otherwise return an error code (sd_mmc_err_t).

References driver_adtc_stop, driver_wait_end_of_write_blocks, sd_mmc_deselect_slot(), SD_MMC_ERR_COMM, sd_mmc_is_mci, sd_mmc_nb_block_remaining, sd_mmc_nb_block_to_tranfer, SD_MMC_OK, and SDMMC_CMD12_STOP_TRANSMISSION.

Referenced by sd_mmc_ram_2_mem().

static bool sd_spi_op_cond ( uint8_t  v2)
static

Ask to all cards to send their operations conditions (SPI only).

  • ACMD41 sends operation condition command.
  • CMD58 reads OCR
Parameters
v2Shall be 1 if it is a SD card V2
Returns
true if success, otherwise false

References CARD_TYPE_HC, driver_get_response, driver_send_cmd, OCR_CCS, R1_SPI_IDLE, SD_ACMD41_HCS, sd_mmc_debug, SD_SPI_ACMD41_SD_SEND_OP_COND, SDMMC_CMD55_APP_CMD, SDMMC_SPI_CMD58_READ_OCR, and sd_mmc_card::type.

Referenced by sd_mmc_spi_card_init().

static bool sdio_cmd52_set_bus_width ( void  )
static

Referenced by sd_mmc_mci_card_init().

static bool sdio_cmd52_set_high_speed ( void  )
static

Referenced by sd_mmc_mci_card_init().

static bool sdio_get_max_speed ( void  )
static
static bool sdio_op_cond ( void  )
static

const uint32_t mmc_trans_multipliers[16]
Initial value:
= {
0, 10, 12, 13, 15, 20, 26, 30, 35, 40, 45, 52, 55, 60, 70, 80
}

MMC transfer multiplier factor codes (1/10) list.

Referenced by mmc_decode_csd().

struct sd_mmc_card* sd_mmc_card
static

Pointer on current slot configurated.

struct sd_mmc_card sd_mmc_cards[SD_MMC_MEM_CNT]
static
Initial value:
= {
#define SD_MMC_CD(slot, unused)
}

SD/MMC card list Note: Initialize card detect pin fields if present.

Referenced by sd_mmc_init(), sd_mmc_is_write_protected(), and sd_mmc_select_slot().

uint16_t sd_mmc_nb_block_remaining = 0
static
uint16_t sd_mmc_nb_block_to_tranfer = 0
static

Number of block to read or write on the current transfer.

Referenced by sd_mmc_init_read_blocks(), sd_mmc_init_write_blocks(), sd_mmc_wait_end_of_read_blocks(), and sd_mmc_wait_end_of_write_blocks().

uint8_t sd_mmc_slot_sel
static
const uint32_t sd_mmc_trans_units[7]
Initial value:
= {
10, 100, 1000, 10000, 0, 0, 0
}

SD/MMC transfer rate unit codes (10K) list.

Referenced by mmc_decode_csd(), and sd_decode_csd().

const uint32_t sd_trans_multipliers[16]
Initial value:
= {
0, 10, 12, 13, 15, 20, 25, 30, 35, 40, 45, 50, 55, 60, 70, 80
}

SD transfer multiplier factor codes (1/10) list.

Referenced by sd_decode_csd().