This example demonstrates how to set up correct clock settings for the megaAVR devices. The goal of this example is to use the libc delay functions.
The example application set up the correct clock setting to use the libc delay functions. The only thing this application will do is to demonstrate how to call the libc delay functions. There are no output in form of leds. To verify operation of this example it is recommended to use debugging and break on different lines.
This software was written for the GNU GCC for AVR.
Other compilers may or may not work.
For further information, visit Microchip.