#include <stddef.h>
#include <ctype.h>
#include <stdbool.h>
#include <stdio.h>
#include <string.h>
#include <avr/io.h>
#include <avr/interrupt.h>
#include <util/delay.h>
#include <avr/pgmspace.h>
#include <asf.h>
#include <conf_usart.h>
Data Structures | |
struct | RING |
Ring Buffer Structure. More... | |
Macros | |
#define | BAUD_PRESCALE (((F_CPU / (USART_BAUDRATE * 16UL))) - 1) |
#define | DOT_TIME_IN_MS (DOT_TIME_IN_TICKS * 10.0) |
#define | DOT_TIME_IN_TICKS (25) |
#define | min(a, b) |
#define | MORSE_RX_BUF_SIZE (32) |
#define | REMORSE_CLK_HZ (100) |
#define | REMORSE_RESTART (400) |
#define | REMORSE_TIMEOUT (1000) |
Typedefs | |
typedef RING * | RING_ID |
Functions | |
static int | bsp_morse_getchar (FILE *stream) |
Decode morse code input from button. More... | |
static int | bsp_morse_putchar (char c, FILE *stream) |
Flash out morse code for character on led. More... | |
static int | bsp_tty_getchar (FILE *stream) |
Fetch a character from uart receiver. More... | |
static int | bsp_tty_putchar (char c, FILE *stream) |
Push a character out uart transmitter. More... | |
ISR (TIMER1_COMPA_vect) | |
Interrupt Service Routines. More... | |
int | main (void) |
Entry point for morse code example. More... | |
static void | morse_fmtchar (char rc) |
Print out character as ASCII morse code (. More... | |
static char | morse_parse (uint8_t pattern, int len) |
Parse morse code pattern into ASCII character. More... | |
static void | morse_poll (void) |
Poll button for debounced conversion to Morse code. More... | |
static void | remorse_instructions (void) |
Print out remorse instructions. More... | |
static int | rng_buf_get (RING_ID rng_id, char *buffer, int maxbytes) |
| |
static int | rng_buf_put (RING_ID rng_id, char *buffer, int nbytes) |
| |
static void | rng_flush (RING_ID ring_id) |
make a ring buffer empty More... | |
static int | rng_free_bytes (RING_ID ring_id) |
| |
static RING_ID | rng_init (RING *p_ring, int nbytes, char *buffer) |
Ring Utility Functions. More... | |
static bool | rng_is_empty (RING_ID ring_id) |
| |
static bool | rng_is_full (RING_ID ring_id) |
| |
void | rng_move_ahead (RING_ID ring_id, int n) |
| |
static int | rng_nBytes (RING_ID ring_id) |
rng_nBytes - determine the number of bytes in a ring buffer More... | |
void | rng_put_ahead (RING_ID ring_id, char byte, int offset) |
| |
Variables | |
const uint8_t | morse_ascii_tbl [][2] |
static char | morse_rx_buf [MORSE_RX_BUF_SIZE+1] |
static RING | morse_rx_ring |
static RING_ID | morse_rx_ring_id |
static volatile bool | remorse_restart |
static volatile uint32_t | remorse_tick_cnt |
static volatile uint32_t | remorse_wd_cnt |
static FILE | tty_console = FDEV_SETUP_STREAM(bsp_tty_putchar, bsp_tty_getchar, _FDEV_SETUP_RW) |
static FILE | tty_morse = FDEV_SETUP_STREAM(bsp_morse_putchar, bsp_morse_getchar, _FDEV_SETUP_RW) |
static bool | user_input = false |
#define BAUD_PRESCALE (((F_CPU / (USART_BAUDRATE * 16UL))) - 1) |
#define DOT_TIME_IN_MS (DOT_TIME_IN_TICKS * 10.0) |
Referenced by bsp_morse_putchar().
#define DOT_TIME_IN_TICKS (25) |
Referenced by morse_poll().
#define min | ( | a, | |
b | |||
) |
Referenced by rng_buf_get(), and rng_buf_put().
#define MORSE_RX_BUF_SIZE (32) |
Referenced by main().
#define REMORSE_CLK_HZ (100) |
#define REMORSE_RESTART (400) |
Referenced by morse_poll().
#define REMORSE_TIMEOUT (1000) |
Referenced by ISR().
|
static |
Decode morse code input from button.
If we have any decoded morse code we return it or _FDEV_ERR if none.
References rng_buf_get().
|
static |
Flash out morse code for character on led.
Polling version of character write. We spin here until character can be placed in transmit register.
References DOT_TIME_IN_MS, LED0, LED_Off, LED_On, and morse_ascii_tbl.
|
static |
Fetch a character from uart receiver.
Polling version of a character read. We spin here until receive buffer has something to read.
References USART0, usart_get(), usart_rx_is_complete(), and user_input.
|
static |
Push a character out uart transmitter.
Polling version of character write. We spin here until character can be placed in transmit register.
References USART0, usart_data_register_is_empty(), and usart_put().
ISR | ( | TIMER1_COMPA_vect | ) |
Interrupt Service Routines.
Remorse clock interrupt routine
This routine is called at interrupt level on each clock interrupt.
References morse_poll(), remorse_restart, remorse_tick_cnt, REMORSE_TIMEOUT, and remorse_wd_cnt.
int main | ( | void | ) |
Entry point for morse code example.
References usart_rs232_options::baudrate, board_init(), CONF_BAUDRATE, CONF_CHARLENGTH, CONF_PARITY, CONF_STOPBITS, LED0, LED_Off, morse_fmtchar(), morse_rx_buf, MORSE_RX_BUF_SIZE, remorse_instructions(), remorse_restart, remorse_wd_cnt, rng_init(), tty_console, tty_morse, USART0, and usart_init_rs232().
|
static |
Print out character as ASCII morse code (.
and -)
References morse_ascii_tbl.
Referenced by main(), and remorse_instructions().
|
static |
Parse morse code pattern into ASCII character.
[in] | pattern | morse code pattern to match |
[in] | len | morse code patter length |
References morse_ascii_tbl.
Referenced by morse_poll().
|
static |
Poll button for debounced conversion to Morse code.
References DOT_TIME_IN_TICKS, GPIO_PUSH_BUTTON_0, ioport_get_pin_level(), LED0, LED_Off, LED_On, morse_parse(), REMORSE_RESTART, remorse_restart, remorse_tick_cnt, rng_buf_put(), rng_flush(), and user_input.
Referenced by ISR().
|
static |
Print out remorse instructions.
References morse_fmtchar(), tty_morse, and user_input.
Referenced by main().
|
static |
This routine copies bytes from the ring buffer <rng_id> into <buffer>. It copies as many bytes as are available in the ring, up to <maxbytes>. The bytes copied will be removed from the ring.
param[in] ring_id ring buffer to get data from param[in] buffer pointer to buffer to receive data param[in] maxbytes maximum number of bytes to get
References RING::buf, RING::buf_size, min, RING::p_from_buf, and RING::p_to_buf.
Referenced by bsp_morse_getchar().
|
static |
This routine puts bytes from <buffer> into ring buffer <ring_id>. The specified number of bytes will be put into the ring, up to the number of bytes available in the ring.
[in] | rng_id | ring buffer to put data into |
[in] | buffer | buffer to get data from |
[in] | nbytes | number of bytes to try to put |
References RING::buf, RING::buf_size, min, RING::p_from_buf, and RING::p_to_buf.
Referenced by morse_poll().
|
static |
make a ring buffer empty
This routine initializes a specified ring buffer to be empty. Any data currently in the buffer will be lost.
[in] | ring_id | ring buffer to initialize |
References RING::p_from_buf, and RING::p_to_buf.
Referenced by morse_poll(), and rng_init().
|
static |
This routine determines the number of bytes currently unused in a specified ring buffer.
[in] | rng_id | ring buffer to examine |
References RING::buf_size, RING::p_from_buf, and RING::p_to_buf.
Ring Utility Functions.
initialize an empty ring buffer
This routine initializes a ring buffer of size "nbytes". The buffer must be one byte larger than nBytes since the algorithm always leaves at least one empty byte in the buffer.
[in] | p_ring | pointer to a RING struct |
[in] | nbytes | number of bytes in ring buffer |
[in] | buffer | pointer to RING buffer of size nBytes + 1 |
References RING::buf, RING::buf_size, and rng_flush().
Referenced by main().
|
static |
This routine determines if a specified ring buffer is empty.
[in] | rng_id | ring buffer to test |
References RING::p_from_buf, and RING::p_to_buf.
|
static |
This routine determines if a specified ring buffer is completely full.
[in] | rng_id | ring buffer to test |
References RING::buf_size, RING::p_from_buf, and RING::p_to_buf.
void rng_move_ahead | ( | RING_ID | ring_id, |
int | n | ||
) |
This routine advances the ring buffer input pointer by <n> bytes. This makes <n> bytes available in the ring buffer, after having been written ahead in the ring buffer with rng_put_ahead().
[in] | ring_id | ring buffer to be advanced |
[in] | n | number of bytes ahead to move input pointer |
References RING::buf_size, and RING::p_to_buf.
|
static |
rng_nBytes - determine the number of bytes in a ring buffer
This routine determines the number of bytes currently in a specified ring buffer.
[in] | rng_id | ring buffer to be enumerated |
References RING::buf_size, RING::p_from_buf, and RING::p_to_buf.
void rng_put_ahead | ( | RING_ID | ring_id, |
char | byte, | ||
int | offset | ||
) |
This routine writes a byte into the ring, but does not move the ring buffer pointers. Thus the byte will not yet be available to rng_buf_get() calls. The byte is written <offset> bytes ahead of the next input location in the ring. Thus, an offset of 0 puts the byte in the same position as would RNG_ELEM_PUT would put a byte, except that the input pointer is not updated.
Bytes written ahead in the ring buffer with this routine can be made available all at once by subsequently moving the ring buffer pointers with the routine rng_move_ahead().
Before calling nng_put_ahead(), the caller must verify that at least <offset> + 1 bytes are available in the ring buffer.
[in] | ring_id | ring buffer to put byte in |
[in] | byte | byte to be put in ring |
[in] | offset | offset beyond next input byte where to put byte |
References RING::buf, RING::buf_size, and RING::p_to_buf.
const uint8_t morse_ascii_tbl[][2] |
Referenced by bsp_morse_putchar(), morse_fmtchar(), and morse_parse().
|
static |
Referenced by main().
|
static |
|
static |
|
static |
Referenced by ISR(), main(), and morse_poll().
|
static |
Referenced by ISR(), and morse_poll().
|
static |
Referenced by main().
|
static |
Referenced by main(), and remorse_instructions().
|
static |
Referenced by bsp_tty_getchar(), morse_poll(), and remorse_instructions().