STK board header file.
This file contains definitions and services related to the features of the STK600 board.
To use this board, define BOARD= STK600_MEGA.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | GPIO_PUSH_BUTTON_ON_BOARD IOPORT_CREATE_PIN(PORTE, 5) |
#define | LED_GREEN_GPIO IOPORT_CREATE_PIN(PORTE, 2) |
#define | LED_RED_GPIO IOPORT_CREATE_PIN(PORTE, 4) |
#define | LED_YELLOW_GPIO IOPORT_CREATE_PIN(PORTE, 3) |
GPIO Connections of LEDs | |
LEDS connector is connected to PORTB
| |
#define | LED0_GPIO IOPORT_CREATE_PIN(PORTB, 0) |
#define | LED1_GPIO IOPORT_CREATE_PIN(PORTB, 1) |
#define | LED2_GPIO IOPORT_CREATE_PIN(PORTB, 2) |
#define | LED3_GPIO IOPORT_CREATE_PIN(PORTB, 3) |
#define | LED4_GPIO IOPORT_CREATE_PIN(PORTB, 4) |
#define | LED5_GPIO IOPORT_CREATE_PIN(PORTB, 5) |
#define | LED6_GPIO IOPORT_CREATE_PIN(PORTB, 6) |
#define | LED7_GPIO IOPORT_CREATE_PIN(PORTB, 7) |
#define | LED0 LED0_GPIO |
#define | LED1 LED1_GPIO |
#define | LED2 LED2_GPIO |
#define | LED3 LED3_GPIO |
#define | LED4 LED4_GPIO |
#define | LED5 LED5_GPIO |
#define | LED6 LED6_GPIO |
#define | LED7 LED7_GPIO |
GPIO Connections of Push Buttons. To use these defines, connect the | |
STK600 PORTD connector to the SWITCHES connector. | |
#define | GPIO_PUSH_BUTTON_0 IOPORT_CREATE_PIN(PORTD, 0) |
#define | GPIO_PUSH_BUTTON_1 IOPORT_CREATE_PIN(PORTD, 1) |
#define | GPIO_PUSH_BUTTON_2 IOPORT_CREATE_PIN(PORTD, 2) |
#define | GPIO_PUSH_BUTTON_3 IOPORT_CREATE_PIN(PORTD, 3) |
#define | GPIO_PUSH_BUTTON_4 IOPORT_CREATE_PIN(PORTD, 4) |
#define | GPIO_PUSH_BUTTON_5 IOPORT_CREATE_PIN(PORTD, 5) |
#define | GPIO_PUSH_BUTTON_6 IOPORT_CREATE_PIN(PORTD, 6) |
#define | GPIO_PUSH_BUTTON_7 IOPORT_CREATE_PIN(PORTD, 7) |
External oscillator | |
#define | BOARD_EXTERNAL_CLK 32000000UL |
SPI Connections of the AT45DBX Data Flash Memory. To use these defines, | |
connect :
| |
#define | AT45DBX_SPI &SPCR |
#define | AT45DBX_CS IOPORT_CREATE_PIN(PORTB,0) |
#define | AT45DBX_MASTER_SS IOPORT_CREATE_PIN(PORTB,0) |
#define | AT45DBX_MASTER_SCK IOPORT_CREATE_PIN(PORTB,1) |
#define | AT45DBX_MASTER_MOSI IOPORT_CREATE_PIN(PORTB,2) |
#define | AT45DBX_MASTER_MISO IOPORT_CREATE_PIN(PORTB,3) |
#define AT45DBX_CS IOPORT_CREATE_PIN(PORTB,0) |
Referenced by board_init().
#define AT45DBX_MASTER_MISO IOPORT_CREATE_PIN(PORTB,3) |
Referenced by board_init().
#define AT45DBX_MASTER_MOSI IOPORT_CREATE_PIN(PORTB,2) |
Referenced by board_init().
#define AT45DBX_MASTER_SCK IOPORT_CREATE_PIN(PORTB,1) |
Referenced by board_init().
#define AT45DBX_MASTER_SS IOPORT_CREATE_PIN(PORTB,0) |
#define AT45DBX_SPI &SPCR |
#define BOARD_EXTERNAL_CLK 32000000UL |
#define GPIO_PUSH_BUTTON_0 IOPORT_CREATE_PIN(PORTD, 0) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_1 IOPORT_CREATE_PIN(PORTD, 1) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_2 IOPORT_CREATE_PIN(PORTD, 2) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_3 IOPORT_CREATE_PIN(PORTD, 3) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_4 IOPORT_CREATE_PIN(PORTD, 4) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_5 IOPORT_CREATE_PIN(PORTD, 5) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_6 IOPORT_CREATE_PIN(PORTD, 6) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_7 IOPORT_CREATE_PIN(PORTD, 7) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_ON_BOARD IOPORT_CREATE_PIN(PORTE, 5) |
Referenced by board_init().
#define LED0 LED0_GPIO |
#define LED0_GPIO IOPORT_CREATE_PIN(PORTB, 0) |
Referenced by board_init().
#define LED1 LED1_GPIO |
#define LED1_GPIO IOPORT_CREATE_PIN(PORTB, 1) |
Referenced by board_init().
#define LED2 LED2_GPIO |
#define LED2_GPIO IOPORT_CREATE_PIN(PORTB, 2) |
Referenced by board_init().
#define LED3 LED3_GPIO |
#define LED3_GPIO IOPORT_CREATE_PIN(PORTB, 3) |
Referenced by board_init().
#define LED4 LED4_GPIO |
#define LED4_GPIO IOPORT_CREATE_PIN(PORTB, 4) |
Referenced by board_init().
#define LED5 LED5_GPIO |
#define LED5_GPIO IOPORT_CREATE_PIN(PORTB, 5) |
Referenced by board_init().
#define LED6 LED6_GPIO |
#define LED6_GPIO IOPORT_CREATE_PIN(PORTB, 6) |
Referenced by board_init().
#define LED7 LED7_GPIO |
#define LED7_GPIO IOPORT_CREATE_PIN(PORTB, 7) |
Referenced by board_init().
#define LED_GREEN_GPIO IOPORT_CREATE_PIN(PORTE, 2) |
Referenced by board_init().
#define LED_RED_GPIO IOPORT_CREATE_PIN(PORTE, 4) |
Referenced by board_init().
#define LED_YELLOW_GPIO IOPORT_CREATE_PIN(PORTE, 3) |
Referenced by board_init().