Microchip® Advanced Software Framework

•All Files Functions Typedefs Enumerations Enumerator Macros Groups
megaAVR ADC Driver

This driver provides an interface for the megaAVR ADC module.

It consists of inline functions that can be used to configure the ADC module and blocking ADC read functions for both 8- and 10-bit results.

Interface

To initialize the ADC you can use the adc_init() function. This sets the ADC prescaler and enables the ADC module. These operations can also be done separately using the adc_set_prescaler() and adc_enable() functions.

To do a blocking ADC read there are two different functions, one for 8-bit and one for 10-bit results:

Usage

First include the header file:

#include "adc.h"

Then initialize and enable the ADC with the correct prescaler:

To do an 8-bit read of ADC channel 0 using 1.1V internal reference:

The syntax to do a 10-bit read is the same, but it returns a 16-bit unsigned integer to fit the whole 10-bit result.

the adc_read_8bit() and adc_read_10bit() functions do not take into account the fact that the voltage reference may be unstable after changing it. It is recommended to discard the first sample after changing voltage reference to avoid incorrect results.

Note
None of the functions are interrupt safe to avoid overhead. If you need interrupt protection you can use the following in your application code:

Macros

#define ADC_ADTS_SOURCE_MASK   (1 << ADTS2 | 1 << ADTS1 | 1 << ADTS0)
 
#define ADC_MUX_MASK   (1 << MUX3 | 1 << MUX2 | 1 << MUX1 | 1 << MUX0)
 
#define ADC_PRESCALER_MASK   (1 << ADPS2 | 1 << ADPS1 | 1 << ADPS0)
 
#define ADC_VREF_MASK   (1 << REFS1 | 1 << REFS0)
 

Enumerations

enum  adc_adjustment {
  ADC_ADJUSTMENT_RIGHT = 0,
  ADC_ADJUSTMENT_LEFT = (1 << ADLAR)
}
 
enum  adc_auto_trigger_source {
  ADC_AUTOTRIGGER_SOURCE_FREERUNNING = (0x0 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_ANALOG_COMPARATOR = (0x1 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_EIR0 = (0x2 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_TC0_COMPARE = (0x3 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_TC0_OVERFLOW = (0x4 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_TC1_COMPARE_B = (0x5 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_TC1_OVERFLOW = (0x6 << ADTS0),
  ADC_AUTOTRIGGER_SOURCE_TC1_CAPTURE = (0x7 << ADTS0)
}
 ADC Auto Trigger sources. More...
 
enum  adc_mux_setting {
  ADC_MUX_ADC0 = 0x0,
  ADC_MUX_ADC1 = 0x1,
  ADC_MUX_ADC2 = 0x2,
  ADC_MUX_ADC3 = 0x3,
  ADC_MUX_ADC4 = 0x4,
  ADC_MUX_ADC5 = 0x5,
  ADC_MUX_ADC6 = 0x6,
  ADC_MUX_ADC7 = 0x7,
  ADC_MUX_1V1 = 0x0E,
  ADC_MUX_GND = 0x0F
}
 ADC input MUX settings. More...
 
enum  adc_prescaler {
  ADC_PRESCALER_DIV2 = (0x1 << ADPS0),
  ADC_PRESCALER_DIV4 = (0x2 << ADPS0),
  ADC_PRESCALER_DIV8 = (0x3 << ADPS0),
  ADC_PRESCALER_DIV16 = (0x4 << ADPS0),
  ADC_PRESCALER_DIV32 = (0x5 << ADPS0),
  ADC_PRESCALER_DIV64 = (0x6 << ADPS0),
  ADC_PRESCALER_DIV128 = (0x7 << ADPS0)
}
 ADC prescaler settings. More...
 
enum  adc_voltage_reference {
  ADC_VREF_AREF = (0x0 << REFS0),
  ADC_VREF_AVCC = (0x1 << REFS0),
  ADC_VREF_RESERVED = (0x2 << REFS0),
  ADC_VREF_1V1 = (0x3 << REFS0)
}
 ADC voltage references. More...
 

Functions

static bool adc_conversion_is_complete (void)
 Poll ADC conversion complete interrupt flag. More...
 
static void adc_disable (void)
 
static void adc_disable_autotrigger (void)
 
static void adc_disable_interrupt (void)
 
static void adc_enable (void)
 
static void adc_enable_autotrigger (void)
 
static void adc_enable_interrupt (void)
 
static uint16_t adc_get_data_10bit (void)
 
static uint8_t adc_get_data_8bit (void)
 
static void adc_init (enum adc_prescaler prescaler)
 ADC initialization. More...
 
static uint16_t adc_read_10bit (enum adc_mux_setting input, enum adc_voltage_reference vref)
 Blocking ADC conversion with 10-bit result. More...
 
static uint8_t adc_read_8bit (enum adc_mux_setting input, enum adc_voltage_reference vref)
 Blocking ADC conversion with 8-bit result. More...
 
static void adc_set_autotrigger_source (enum adc_auto_trigger_source trg)
 Set ADC Auto Trigger source. More...
 
static void adc_set_mux (enum adc_mux_setting input)
 Select source from ADC input mux. More...
 
static void adc_set_prescaler (enum adc_prescaler prescaler)
 Set ADC clock prescaler. More...
 
static void adc_set_voltage_reference (enum adc_voltage_reference vref)
 Set the ADC voltage reference. More...
 
static void adc_start_conversion (void)
 

Optimized functions for register accesses

These functions are for cases where you do not want the overhead of masking out bitfields before updating the register value. These will only do a write to the register instead of a read-modify-write.

static void adc_set_admux (uint8_t regval)
 Set voltage reference, mux and adjustment bits in admux register. More...
 

#define ADC_ADTS_SOURCE_MASK   (1 << ADTS2 | 1 << ADTS1 | 1 << ADTS0)
#define ADC_MUX_MASK   (1 << MUX3 | 1 << MUX2 | 1 << MUX1 | 1 << MUX0)
#define ADC_PRESCALER_MASK   (1 << ADPS2 | 1 << ADPS1 | 1 << ADPS0)

Referenced by adc_set_prescaler().

#define ADC_VREF_MASK   (1 << REFS1 | 1 << REFS0)

Enumerator
ADC_ADJUSTMENT_RIGHT 
ADC_ADJUSTMENT_LEFT 

ADC Auto Trigger sources.

Available trigger sources for ADC Auto Trigger

Enumerator
ADC_AUTOTRIGGER_SOURCE_FREERUNNING 
ADC_AUTOTRIGGER_SOURCE_ANALOG_COMPARATOR 
ADC_AUTOTRIGGER_SOURCE_EIR0 
ADC_AUTOTRIGGER_SOURCE_TC0_COMPARE 
ADC_AUTOTRIGGER_SOURCE_TC0_OVERFLOW 
ADC_AUTOTRIGGER_SOURCE_TC1_COMPARE_B 
ADC_AUTOTRIGGER_SOURCE_TC1_OVERFLOW 
ADC_AUTOTRIGGER_SOURCE_TC1_CAPTURE 

ADC input MUX settings.

MUX settings for ADC input

Note
If using 10X or 200X gain only 2.56V should be used as internal voltage reference.
The doxygen documentation contains MUX settings for multiple devices. check the device datasheet or family header files to find what options are available on your device.
Enumerator
ADC_MUX_ADC0 

ADC0, single ended.

ADC_MUX_ADC1 

ADC1, single ended.

ADC_MUX_ADC2 

ADC2, single ended.

ADC_MUX_ADC3 

ADC3, single ended.

ADC_MUX_ADC4 

ADC4, single ended.

ADC_MUX_ADC5 

ADC5, single ended.

ADC_MUX_ADC6 

ADC6, single ended.

ADC_MUX_ADC7 

ADC7, single ended.

ADC_MUX_1V1 

1.1V internal bandgap voltage

ADC_MUX_GND 

GND, single ended.

ADC prescaler settings.

Available ADC prescaler settings

Enumerator
ADC_PRESCALER_DIV2 
ADC_PRESCALER_DIV4 
ADC_PRESCALER_DIV8 
ADC_PRESCALER_DIV16 
ADC_PRESCALER_DIV32 
ADC_PRESCALER_DIV64 
ADC_PRESCALER_DIV128 

ADC voltage references.

Available ADC voltage references

Enumerator
ADC_VREF_AREF 

AREF, internal Vref turned off.

ADC_VREF_AVCC 

AVCC.

ADC_VREF_RESERVED 

Reserved value, not available.

ADC_VREF_1V1 

Internal 1.1V voltage reference.

static bool adc_conversion_is_complete ( void  )
inlinestatic

Poll ADC conversion complete interrupt flag.

Returns
false if conversion not complete
static void adc_disable ( void  )
inlinestatic
static void adc_disable_autotrigger ( void  )
inlinestatic
static void adc_disable_interrupt ( void  )
inlinestatic
static void adc_enable ( void  )
inlinestatic
static void adc_enable_autotrigger ( void  )
inlinestatic
static void adc_enable_interrupt ( void  )
inlinestatic
static uint16_t adc_get_data_10bit ( void  )
inlinestatic
static uint8_t adc_get_data_8bit ( void  )
inlinestatic
static void adc_init ( enum adc_prescaler  prescaler)
inlinestatic

ADC initialization.

Set ADC prescaler and enable the ADC

Parameters
prescalerADC clock prescaler

Referenced by main().

static uint16_t adc_read_10bit ( enum adc_mux_setting  input,
enum adc_voltage_reference  vref 
)
inlinestatic

Blocking ADC conversion with 10-bit result.

An example demonstrating the minimum initialization needed to perform a conversion:

// Initialize and enable ADC
Parameters
inputADC input mux selection and voltage reference
vrefADC voltage reference
Returns
Conversion result as an unsigned 16-bit integer
Note
The first ADC conversion result after switching reference voltage source may be inaccurate, and the user is advised to discard this result. this function is not interrupt safe

References ADC_MUX_MASK.

Referenced by main().

static uint8_t adc_read_8bit ( enum adc_mux_setting  input,
enum adc_voltage_reference  vref 
)
inlinestatic

Blocking ADC conversion with 8-bit result.

An example demonstrating the minimum initialization needed to perform a conversion:

Parameters
inputADC input mux selection.
vrefADC voltage reference
Returns
Conversion result as an unsigned 8-bit integer
Note
The first ADC conversion result after switching reference voltage source may be inaccurate, and the user is advised to discard this result. this function is not interrupt safe.

References ADC_ADJUSTMENT_LEFT, and ADC_MUX_MASK.

static void adc_set_admux ( uint8_t  regval)
inlinestatic

Set voltage reference, mux and adjustment bits in admux register.

Note
This does not handle the MUX5 bit if this is available, only the MUX bits in ADMUX.

Example usage:

Parameters
regvalADC input mux selection and voltage reference
static void adc_set_autotrigger_source ( enum adc_auto_trigger_source  trg)
inlinestatic

Set ADC Auto Trigger source.

Parameters
trgADC Auto Trigger source

References ADC_ADTS_REG, and ADC_ADTS_SOURCE_MASK.

static void adc_set_mux ( enum adc_mux_setting  input)
inlinestatic

Select source from ADC input mux.

A small example demonstrating the usage:

Parameters
inputADC channel

References ADC_MUX_MASK.

static void adc_set_prescaler ( enum adc_prescaler  prescaler)
inlinestatic

Set ADC clock prescaler.

Note
The ADC clock must not exceed the maximum speed of 1MHz

A small example demonstrating the usage:

Parameters
prescalerADC clock prescaler

References ADC_PRESCALER_MASK.

static void adc_set_voltage_reference ( enum adc_voltage_reference  vref)
inlinestatic

Set the ADC voltage reference.

An example demonstrating the usage:

Parameters
vrefADC voltage reference
Note
The first ADC conversion result after switching reference voltage source may be inaccurate, and the user is advised to discard this result.

References ADC_VREF_MASK.

static void adc_start_conversion ( void  )
inlinestatic