This is the unit test for the MEGARF TWI driver.
This example has been tested with the following setup(s):
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/