Microchip® Advanced Software Framework

sysclk.c File Reference

Chip-specific system clock management functions.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <compiler.h>
#include <sysclk.h>

Functions

void sysclk_init (void)
 Function to initialize the clock and disable clock for not required modules. More...
 
void sysclk_enable_module (enum power_red_id port, uint8_t id)
 Enable the clock to peripheral id on port port. More...
 
void sysclk_disable_module (enum power_red_id port, uint8_t id)
 Disable the clock to peripheral id on port port. More...
 

void sysclk_disable_module ( enum power_red_id  port,
uint8_t  id 
)

Disable the clock to peripheral id on port port.

Parameters
portID of the port to which the module is connected (one of the power_red_id *definitions).
idThe ID (bit mask) of the peripheral module to be disabled.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_disable_peripheral_clock(), and sysclk_get_peripheral_bus_hz().

void sysclk_enable_module ( enum power_red_id  port,
uint8_t  id 
)

Enable the clock to peripheral id on port port.

Parameters
portID of the port to which the module is connected (one of the power_red_id *definitions).
idThe ID (bitmask) of the peripheral module to be enabled.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_enable_peripheral_clock(), and usart_enable_module_clock().