![]() | |
![]() | |
![]() | |
![]() | See Quickstart guide for SAM RTC driver |
![]() | The Universal Asynchronous Receiver Transmitter features a two-pin UART that can be used for communication and trace purposes and offers an ideal medium for in-situ programming solutions |
![]() | Receiver Transmitter (USART) |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | The following structures provide the USB device descriptors required for USB Device with a single interface MSC |
![]() | Service of FatFS file system |
![]() | Low level driver for FatFS |
![]() | See Quickstart guide for SAM SPI driver |
![]() | Low-level driver for the ILI93XX LCD controller |
![]() | Low-level driver for the AAT31XX LCD backlight controller |
![]() | The Embedded Flash service provides functions for internal flash operations |
![]() | The Enhanced Embedded Flash Controller ensures the interface of the Flash block with the 32-bit internal bus |
![]() | Driver for the SUPC (Supply Controller) |
![]() | See Quickstart guide for SAM ADC driver |
![]() | Driver for the WDT (Watchdog Timer) |
![]() | This is the QTouch Library for AVR and AVR32 devices that consists of one api header file(touch_api.h) and respective pre-compiled libraries |
![]() | See Quick start guide for the |
![]() | This is the common API for GPIO |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service |
![]() | Driver for the Static Memory Controller |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (SAM4S) |
![]() | Common abstraction layer for memory interfaces |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | The sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time |
![]() | See Quick start guide for the common IOPORT service |
![]() | This stack includes the USB Device Stack, USB Host Stack and common definitions |
![]() ![]() | This module includes USB Stack Device implementation |
![]() ![]() | This module defines Atmel PID and VIDs constants |
![]() ![]() | This module defines constants and data structures provided by the USB 2.0 specification |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | |
![]() | Croutine |
![]() | Croutine |
![]() | Croutine |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Queue |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Semphr |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | Task |
![]() | This service provides an interface for handling resistive touch component |
![]() ![]() | This is hardware specific configuration that configures the resistive touch service for use with the ADS7843 touch controller |
![]() | Low-level driver for the ADS7843 touch controller |
![]() | This is the common API for SPI interface |
![]() | This service provides an interface to drawing graphics on a graphical display |
![]() ![]() | Window system for organizing window elements in a graphical user interface (GUI) |
![]() ![]() | The Widget toolkit implements many common widgets for use on a graphical display using the functionality of Window system and Graphics library |
![]() ![]() | This is hardware specific configuration that configures the graphical service for use with the ILI93XX display controller display |
![]() ![]() | This is a library of generic implementations of various graphics primitives |
![]() ![]() | This modules provides functionality for outputting a font to a display |
![]() | The Membag allocator is a optimized, fragmentationless general purpose memory allocator utility module designed to replace the standard C library malloc() and free() functions in resource constrained environments |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the the Peripheral Direct Memory Access (DMA) Controller (PDC) module |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |