Getting Started Application.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | BLINK_PERIOD 1000 |
LED0 blink time, LED1 blink half this time, in ms. More... | |
#define | IRQ_PRIOR_PIO 0 |
IRQ priority for PIO (The lower the value, the greater the priority) More... | |
#define | STRING_EOL "\r" |
#define | STRING_HEADER |
Functions | |
static void | Button1_Handler (uint32_t id, uint32_t mask) |
Handler for Button 1 rising edge interrupt. More... | |
static void | Button2_Handler (uint32_t id, uint32_t mask) |
Handler for Button 2 falling edge interrupt. More... | |
static void | configure_buttons (void) |
Configure the Pushbuttons. More... | |
static void | configure_console (void) |
Configure UART console. More... | |
static void | configure_tc (void) |
Configure Timer Counter 0 to generate an interrupt every 250ms. More... | |
int | main (void) |
getting-started Application entry point. More... | |
static void | mdelay (uint32_t ul_dly_ticks) |
Wait for the given number of milliseconds (using the g_ul_ms_ticks generated by the SAM's microcontrollers's system tick). More... | |
static void | ProcessButtonEvt (uint8_t uc_button) |
Process Buttons Events. More... | |
void | SysTick_Handler (void) |
Handler for System Tick interrupt. More... | |
void | TC0_Handler (void) |
Interrupt handler for TC0 interrupt. More... | |
Variables | |
volatile bool | g_b_led0_active = true |
LED0 blinking control. More... | |
volatile uint32_t | g_ul_ms_ticks = 0 |
Global g_ul_ms_ticks in milliseconds since start of application. More... | |
#define BLINK_PERIOD 1000 |
LED0 blink time, LED1 blink half this time, in ms.
#define IRQ_PRIOR_PIO 0 |
IRQ priority for PIO (The lower the value, the greater the priority)
Referenced by configure_buttons().
#define STRING_EOL "\r" |
#define STRING_HEADER |
Referenced by main().
|
static |
Handler for Button 1 rising edge interrupt.
Handle process led1 status change.
References PIN_PUSHBUTTON_1_ID, PIN_PUSHBUTTON_1_MASK, and ProcessButtonEvt().
Referenced by configure_buttons().
|
static |
Handler for Button 2 falling edge interrupt.
Handle process led2 status change.
References PIN_PUSHBUTTON_2_ID, PIN_PUSHBUTTON_2_MASK, and ProcessButtonEvt().
Referenced by configure_buttons().
|
static |
Configure the Pushbuttons.
Configure the PIO as inputs and generate corresponding interrupt when pressed or released.
References Button1_Handler(), Button2_Handler(), IRQ_PRIOR_PIO, PIN_PUSHBUTTON_1_ATTR, PIN_PUSHBUTTON_1_ID, PIN_PUSHBUTTON_1_MASK, PIN_PUSHBUTTON_1_PIO, PIN_PUSHBUTTON_2_ATTR, PIN_PUSHBUTTON_2_ID, PIN_PUSHBUTTON_2_MASK, PIN_PUSHBUTTON_2_PIO, pio_enable_interrupt(), pio_handler_set(), pio_handler_set_priority(), pio_set_debounce_filter(), and pmc_enable_periph_clk().
Referenced by main().
|
static |
Configure UART console.
References uart_rs232_options::baudrate, CONF_UART, CONF_UART_BAUDRATE, CONF_UART_PARITY, CONSOLE_UART_ID, stdio_serial_init(), and sysclk_enable_peripheral_clock().
Referenced by main().
|
static |
Configure Timer Counter 0 to generate an interrupt every 250ms.
Configure TC for a 4Hz frequency and trigger on RC compare.
References pmc_disable_pck(), pmc_enable_pck(), pmc_enable_periph_clk(), PMC_PCK_3, pmc_switch_pck_to_sclk(), sysclk_get_cpu_hz(), tc_enable_interrupt(), tc_find_mck_divisor(), tc_init(), tc_start(), and tc_write_rc().
Referenced by main().
int main | ( | void | ) |
getting-started Application entry point.
[main_step_sys_init]
[main_step_sys_init]
[main_step_console_init]
[main_step_console_init]
[main_step_systick_init]
[main_step_systick_init]
[main_step_tc_init]
[main_step_tc_init]
[main_step_btn_init]
[main_step_btn_init]
[main_step_loop]
[main_step_loop]
References board_init(), configure_buttons(), configure_console(), configure_tc(), g_b_led0_active, GPIO_PUSH_BUTTON_2, GPIO_PUSH_BUTTON_2_FLAGS, IOPORT_DIR_INPUT, ioport_set_pin_dir(), ioport_set_pin_mode(), ioport_set_pin_sense_mode(), ioport_toggle_pin_level(), LED0_GPIO, LED_0_NAME, LED_1_NAME, mdelay(), PUSHBUTTON_1_NAME, PUSHBUTTON_2_NAME, STRING_HEADER, sysclk_get_cpu_hz(), and sysclk_init().
|
static |
Wait for the given number of milliseconds (using the g_ul_ms_ticks generated by the SAM's microcontrollers's system tick).
ul_dly_ticks | Delay to wait for, in milliseconds. |
References g_ul_ms_ticks.
Referenced by main().
|
static |
Process Buttons Events.
Change active states of LEDs when corresponding button events happened.
References g_b_led0_active, IOPORT_PIN_LEVEL_HIGH, IOPORT_PIN_LEVEL_LOW, ioport_set_pin_level(), LED0_GPIO, LED1_GPIO, tc_start(), and tc_stop().
Referenced by Button1_Handler(), and Button2_Handler().
void SysTick_Handler | ( | void | ) |
Handler for System Tick interrupt.
Process System Tick Event Increments the g_ul_ms_ticks counter.
References g_ul_ms_ticks.
void TC0_Handler | ( | void | ) |
Interrupt handler for TC0 interrupt.
Toggles the state of LED#2.
References ioport_toggle_pin_level(), LED1_GPIO, tc_get_status(), and UNUSED.
LED0 blinking control.
Referenced by main(), and ProcessButtonEvt().
volatile uint32_t g_ul_ms_ticks = 0 |
Global g_ul_ms_ticks in milliseconds since start of application.
Referenced by mdelay(), and SysTick_Handler().