Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
System Clock Management

See Quick Start Guide for the System Clock Management service (SAM4L).

The sysclk API covers the system clock and all clocks derived from it. The system clock is a chip-internal clock on which all synchronous clocks, i.e. CPU and bus/peripheral clocks, are based. The system clock is typically generated from one of a variety of sources, which may include crystal and RC oscillators as well as PLLs. The clocks derived from the system clock are sometimes also known as synchronous clocks, since they always run synchronously with respect to each other, as opposed to generic clocks which may run from different oscillators or PLLs.

Most applications should simply call sysclk_init() to initialize everything related to the system clock and its source (oscillator, PLL or DFLL), and leave it at that. More advanced applications, and platform-specific drivers, may require additional services from the clock system, some of which may be platform-specific.

Platform Dependencies

The sysclk API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.

The following functions are available on all platforms with the same parameters and functionality. These functions may be called freely by portable applications, drivers and services:

The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behavior. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:

All other functions should be considered platform-specific. Enabling/disabling clocks to specific peripherals as well as determining the speed of these clocks should be done by calling functions provided by the driver for that peripheral.

Modules

 System Clock internals
 

Macros

#define CONFIG_HCACHE_ENABLE   1
 
#define CONFIG_SYSCLK_CPU_DIV   0
 Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\). More...
 
#define CONFIG_SYSCLK_INIT_CPUMASK
 Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_HSBMASK
 Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBAMASK
 Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBBMASK
 Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBCMASK
 Configuration symbol for the PBC clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_INIT_PBDMASK
 Configuration symbol for the PBD clocks enabled at power-on after the sysclock module has been initialized. More...
 
#define CONFIG_SYSCLK_PBA_DIV   0
 Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\). More...
 
#define CONFIG_SYSCLK_PBB_DIV   0
 Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\). More...
 
#define CONFIG_SYSCLK_PBC_DIV   0
 Configuration symbol for dividing the PBC clock frequency by \(2^{CONFIG\_SYSCLK\_PBC\_DIV}\). More...
 
#define CONFIG_SYSCLK_PBD_DIV   0
 Configuration symbol for dividing the PBD clock frequency by \(2^{CONFIG\_SYSCLK\_PBD\_DIV}\). More...
 
#define CONFIG_SYSCLK_SOURCE   SYSCLK_SRC_RCSYS
 
#define CONFIG_USBCLK_DIV
 Configuration symbol for the USB generic clock divider setting. More...
 
#define CONFIG_USBCLK_SOURCE
 Configuration symbol for the USB generic clock source. More...
 
#define USBCLK_STARTUP_TIMEOUT   (OSC0_STARTUP_TIMEOUT*(1000000/OSC_RCSYS_NOMINAL_HZ))
 Number of us to wait for USB clock to start. More...
 

Functions

void sysclk_disable_usb (void)
 Disable the USB generic clock. More...
 
void sysclk_enable_usb (void)
 Enable the USB generic clock. More...
 
void sysclk_priv_disable_module (uint32_t bus_id, uint32_t module_index)
 Disable a maskable module clock. More...
 
void sysclk_priv_enable_module (uint32_t bus_id, uint32_t module_index)
 Enable a maskable module clock. More...
 

System clock source

#define SYSCLK_SRC_RCSYS   0
 System RC oscillator. More...
 
#define SYSCLK_SRC_OSC0   1
 Oscillator 0. More...
 
#define SYSCLK_SRC_PLL0   2
 Phase Locked Loop 0. More...
 
#define SYSCLK_SRC_DFLL   3
 Digital Frequency Locked Loop. More...
 
#define SYSCLK_SRC_RC80M   4
 80 MHz RC oscillator More...
 
#define SYSCLK_SRC_RCFAST   5
 4-8-12 MHz RC oscillator More...
 
#define SYSCLK_SRC_RC1M   6
 1 MHz RC oscillator More...
 

USB Clock Sources

#define USBCLK_SRC_OSC0   GENCLK_SRC_OSC0
 Use OSC0. More...
 
#define USBCLK_SRC_PLL0   GENCLK_SRC_PLL0
 Use PLL0. More...
 
#define USBCLK_SRC_DFLL   GENCLK_SRC_DFLL
 Use DFLL. More...
 
#define USBCLK_SRC_GCLKIN0   GENCLK_SRC_GCLKIN0
 Use GCLKIN0. More...
 

Bus index of maskable module clocks

#define PM_CLK_GRP_CPU   0
 
#define PM_CLK_GRP_HSB   1
 
#define PM_CLK_GRP_PBA   2
 
#define PM_CLK_GRP_PBB   3
 
#define PM_CLK_GRP_PBC   4
 
#define PM_CLK_GRP_PBD   5
 

Clocks derived from the CPU clock

#define SYSCLK_OCD   0
 On-Chip Debug system. More...
 

Clocks derived from the HSB clock

#define SYSCLK_PDCA_HSB   0
 PDCA memory interface. More...
 
#define SYSCLK_HFLASHC_DATA   1
 Flash data interface. More...
 
#define SYSCLK_HRAMC1_DATA   2
 HRAMC data interface. More...
 
#define SYSCLK_USBC_DATA   3
 USBC DMA and FIFO interface. More...
 
#define SYSCLK_CRCCU_DATA   4
 CRCCU data interface. More...
 
#define SYSCLK_PBA_BRIDGE   5
 HSB<->PBA bridge. More...
 
#define SYSCLK_PBB_BRIDGE   6
 HSB<->PBB bridge. More...
 
#define SYSCLK_PBC_BRIDGE   7
 HSB<->PBC bridge. More...
 
#define SYSCLK_PBD_BRIDGE   8
 HSB<->PBD bridge. More...
 
#define SYSCLK_AESA_HSB   9
 Advanced Encryption Standard. More...
 

Clocks derived from the PBA clock

#define SYSCLK_IISC   0
 IISC Controller. More...
 
#define SYSCLK_SPI   1
 SPI Controller. More...
 
#define SYSCLK_TC0   2
 Timer/Counter 0. More...
 
#define SYSCLK_TC1   3
 Timer/Counter 1. More...
 
#define SYSCLK_TWIM0   4
 TWI Master 0. More...
 
#define SYSCLK_TWIS0   5
 TWI Slave 0. More...
 
#define SYSCLK_TWIM1   6
 TWI Master 1. More...
 
#define SYSCLK_TWIS1   7
 TWI Slave 1. More...
 
#define SYSCLK_USART0   8
 USART 0. More...
 
#define SYSCLK_USART1   9
 USART 1. More...
 
#define SYSCLK_USART2   10
 USART 2. More...
 
#define SYSCLK_USART3   11
 USART 3. More...
 
#define SYSCLK_ADCIFE   12
 A/D Converter. More...
 
#define SYSCLK_DACC   13
 D/A Converter. More...
 
#define SYSCLK_ACIFC   14
 Analog Comparator. More...
 
#define SYSCLK_GLOC   15
 Glue Logic Controller. More...
 
#define SYSCLK_ABDACB   16
 ABDACB Controller. More...
 
#define SYSCLK_TRNG   17
 TRNG Controller. More...
 
#define SYSCLK_PARC   18
 PARC Controller. More...
 
#define SYSCLK_CATB   19
 Capacitive Touch. More...
 
#define SYSCLK_TWIM2   21
 TWI Master 2. More...
 
#define SYSCLK_TWIM3   22
 TWI Master 3. More...
 
#define SYSCLK_LCDCA   23
 LCD Controller. More...
 

Clocks derived from the PBB clock

#define SYSCLK_HFLASHC_REGS   0
 Flash Controller registers. More...
 
#define SYSCLK_HRAMC1_REGS   1
 HRAMC Controller registers. More...
 
#define SYSCLK_HMATRIX   2
 HSB Matrix configuration. More...
 
#define SYSCLK_PDCA_PB   3
 PDCA peripheral bus interface. More...
 
#define SYSCLK_CRCCU_REGS   4
 CRCCU registers. More...
 
#define SYSCLK_USBC_REGS   5
 USBC registers. More...
 
#define SYSCLK_PEVC   6
 PEVC Controller. More...
 

Clocks derived from the PBC clock

#define SYSCLK_PM   0
 PM configuration. More...
 
#define SYSCLK_CHIPID   1
 CHIPID Controller. More...
 
#define SYSCLK_SCIF   2
 System Control Interface. More...
 
#define SYSCLK_FREQM   3
 Frequency Meter. More...
 
#define SYSCLK_GPIO   4
 General-Purpose I/O. More...
 

Clocks derived from the PBD clock

#define SYSCLK_BPM   0
 BPM configuration. More...
 
#define SYSCLK_BSCIF   1
 BSCIF configuration. More...
 
#define SYSCLK_AST   2
 Asynchronous Timer. More...
 
#define SYSCLK_WDT   3
 Watchdog Timer. More...
 
#define SYSCLK_EIC   4
 External Interrupt Controller. More...
 
#define SYSCLK_PICOUART   5
 PICOUART. More...
 

Divided clock mask derived from the PBA clock

#define PBA_DIVMASK_TIMER_CLOCK2   (1u << 0)
 TIMER_CLOCK2 mask. More...
 
#define PBA_DIVMASK_TIMER_CLOCK3   (1u << 2)
 TIMER_CLOCK3 mask. More...
 
#define PBA_DIVMASK_CLK_USART   (1u << 2)
 CLK_USART/DIV mask. More...
 
#define PBA_DIVMASK_TIMER_CLOCK4   (1u << 4)
 TIMER_CLOCK4 mask. More...
 
#define PBA_DIVMASK_TIMER_CLOCK5   (1u << 6)
 TIMER_CLOCK5 mask. More...
 
#define PBA_DIVMASK_Msk   (0x7Fu << 0)
 Bitfield mask. More...
 

Querying the system clock and its derived clocks

The following functions may be used to query the current frequency of the system clock and the CPU and bus clocks derived from it.

sysclk_get_main_hz() and sysclk_get_cpu_hz() can be assumed to be available on all platforms, although some platforms may define additional accessors for various chip-internal bus clocks. These are usually not intended to be queried directly by generic code.

uint32_t sysclk_get_peripheral_bus_hz (const volatile void *module)
 Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral. More...
 
static uint32_t sysclk_get_main_hz (void)
 Return the current rate in Hz of the main system clock. More...
 
static uint32_t sysclk_get_cpu_hz (void)
 Return the current rate in Hz of the CPU clock. More...
 
static uint32_t sysclk_get_hsb_hz (void)
 Return the current rate in Hz of the High-Speed Bus clock. More...
 
static uint32_t sysclk_get_pba_hz (void)
 Return the current rate in Hz of the Peripheral Bus A clock. More...
 
static uint32_t sysclk_get_pbb_hz (void)
 Return the current rate in Hz of the Peripheral Bus B clock. More...
 
static uint32_t sysclk_get_pbc_hz (void)
 Return the current rate in Hz of the Peripheral Bus C clock. More...
 
static uint32_t sysclk_get_pbd_hz (void)
 Return the current rate in Hz of the Peripheral Bus D clock. More...
 

Enabling and disabling synchronous clocks

void sysclk_enable_pba_module (uint32_t module_index)
 Enable a module clock derived from the PBA clock. More...
 
void sysclk_disable_pba_module (uint32_t module_index)
 Disable a module clock derived from the PBA clock. More...
 
void sysclk_enable_pbb_module (uint32_t module_index)
 Enable a module clock derived from the PBB clock. More...
 
void sysclk_disable_pbb_module (uint32_t module_index)
 Disable a module clock derived from the PBB clock. More...
 
void sysclk_enable_peripheral_clock (const volatile void *module)
 Enable a peripheral's clock from its base address. More...
 
void sysclk_disable_peripheral_clock (const volatile void *module)
 Disable a peripheral's clock from its base address. More...
 
static void sysclk_enable_cpu_module (uint32_t module_index)
 Enable a module clock derived from the CPU clock. More...
 
static void sysclk_disable_cpu_module (uint32_t module_index)
 Disable a module clock derived from the CPU clock. More...
 
static void sysclk_enable_hsb_module (uint32_t module_index)
 Enable a module clock derived from the HSB clock. More...
 
static void sysclk_disable_hsb_module (uint32_t module_index)
 Disable a module clock derived from the HSB clock. More...
 
static void sysclk_enable_pbc_module (uint32_t module_index)
 Enable a module clock derived from the PBC clock. More...
 
static void sysclk_disable_pbc_module (uint32_t module_index)
 Disable a module clock derived from the PBC clock. More...
 
static void sysclk_enable_pbd_module (uint32_t module_index)
 Enable a module clock derived from the PBD clock. More...
 
static void sysclk_disable_pbd_module (uint32_t module_index)
 Disable a module clock derived from the PBD clock. More...
 
static void sysclk_enable_pba_divmask (uint32_t mask)
 Enable divided clock mask derived from the PBA clock. More...
 
static void sysclk_disable_pba_divmask (uint32_t mask)
 Disable divided clock mask derived from the PBA clock. More...
 

System Clock Source and Prescaler configuration

void sysclk_set_prescalers (uint32_t cpu_shift, uint32_t pba_shift, uint32_t pbb_shift, uint32_t pbc_shift, uint32_t pbd_shift)
 Set system clock prescaler configuration. More...
 
void sysclk_set_source (uint32_t src)
 Change the source of the main system clock. More...
 

System Clock Initialization

void sysclk_init (void)
 Initialize the synchronous clock system. More...
 

#define CONFIG_HCACHE_ENABLE   1
#define CONFIG_SYSCLK_CPU_DIV   0

Configuration symbol for dividing the CPU clock frequency by \(2^{CONFIG\_SYSCLK\_CPU\_DIV}\).

If this symbol is not defined, the CPU clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_cpu_hz(), and sysclk_get_hsb_hz().

#define CONFIG_SYSCLK_INIT_CPUMASK

Configuration symbol for the CPU clocks enabled at power-on after the sysclock module has been initialized.

By default, all CPU clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all CPU clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_HSBMASK

Configuration symbol for the HSB clocks enabled at power-on after the sysclock module has been initialized.

By default, all HSB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all HSB clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBAMASK

Configuration symbol for the PBA clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBA clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBA clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBBMASK

Configuration symbol for the PBB clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBB clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBB clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBCMASK

Configuration symbol for the PBC clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBC clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBC clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_INIT_PBDMASK

Configuration symbol for the PBD clocks enabled at power-on after the sysclock module has been initialized.

By default, all PBD clocks are left enabled, however to save power these can be automatically disabled by defining this value to a mask of SYSCLOCK_xxx settings.

If this symbol is not defined, then all PBD clocks are left enabled.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_init().

#define CONFIG_SYSCLK_PBA_DIV   0

Configuration symbol for dividing the PBA clock frequency by \(2^{CONFIG\_SYSCLK\_PBA\_DIV}\).

If this symbol is not defined, the PBA clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pba_hz().

#define CONFIG_SYSCLK_PBB_DIV   0

Configuration symbol for dividing the PBB clock frequency by \(2^{CONFIG\_SYSCLK\_PBB\_DIV}\).

If this symbol is not defined, the PBB clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pbb_hz().

#define CONFIG_SYSCLK_PBC_DIV   0

Configuration symbol for dividing the PBC clock frequency by \(2^{CONFIG\_SYSCLK\_PBC\_DIV}\).

If this symbol is not defined, the PBC clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pbc_hz().

#define CONFIG_SYSCLK_PBD_DIV   0

Configuration symbol for dividing the PBD clock frequency by \(2^{CONFIG\_SYSCLK\_PBD\_DIV}\).

If this symbol is not defined, the PBD clock frequency is not divided.

This symbol may be defined in conf_clock.h.

Referenced by sysclk_get_pbd_hz().

#define CONFIG_SYSCLK_SOURCE   SYSCLK_SRC_RCSYS

Referenced by sysclk_get_main_hz().

#define CONFIG_USBCLK_DIV

Configuration symbol for the USB generic clock divider setting.

Sets the clock division for the USB generic clock. If a USB clock source is selected with CONFIG_USBCLK_SOURCE, this configuration symbol must also be defined.

Define this as any value that does not exceed GENCLK_DIV_MAX, and which will give a 48 MHz clock frequency from the selected source.

#define CONFIG_USBCLK_SOURCE

Configuration symbol for the USB generic clock source.

Sets the clock source to use for the USB. The source must also be properly configured.

Define this to one of the USBCLK_SRC_xxx settings. Leave it undefined if USB is not required.

#define PBA_DIVMASK_CLK_USART   (1u << 2)

CLK_USART/DIV mask.

Referenced by sysclk_enable_peripheral_clock().

#define PBA_DIVMASK_Msk   (0x7Fu << 0)

Bitfield mask.

Referenced by sysclk_disable_peripheral_clock().

#define PBA_DIVMASK_TIMER_CLOCK2   (1u << 0)

TIMER_CLOCK2 mask.

Referenced by sysclk_enable_peripheral_clock().

#define PBA_DIVMASK_TIMER_CLOCK3   (1u << 2)

TIMER_CLOCK3 mask.

Referenced by sysclk_enable_peripheral_clock().

#define PBA_DIVMASK_TIMER_CLOCK4   (1u << 4)

TIMER_CLOCK4 mask.

Referenced by sysclk_enable_peripheral_clock().

#define PBA_DIVMASK_TIMER_CLOCK5   (1u << 6)

TIMER_CLOCK5 mask.

Referenced by sysclk_enable_peripheral_clock().

#define PM_CLK_GRP_CPU   0
#define PM_CLK_GRP_HSB   1
#define PM_CLK_GRP_PBA   2
#define PM_CLK_GRP_PBB   3
#define PM_CLK_GRP_PBC   4
#define PM_CLK_GRP_PBD   5
#define SYSCLK_ABDACB   16
#define SYSCLK_ACIFC   14
#define SYSCLK_ADCIFE   12
#define SYSCLK_AESA_HSB   9

Advanced Encryption Standard.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_AST   2
#define SYSCLK_BPM   0
#define SYSCLK_BSCIF   1

BSCIF configuration.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_CATB   19
#define SYSCLK_CHIPID   1
#define SYSCLK_CRCCU_DATA   4

CRCCU data interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_CRCCU_REGS   4
#define SYSCLK_DACC   13
#define SYSCLK_EIC   4

External Interrupt Controller.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_FREQM   3
#define SYSCLK_GLOC   15

Glue Logic Controller.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_GPIO   4

General-Purpose I/O.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_HFLASHC_DATA   1

Flash data interface.

Referenced by sysclk_enable_peripheral_clock().

#define SYSCLK_HFLASHC_REGS   0

Flash Controller registers.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_HMATRIX   2

HSB Matrix configuration.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_HRAMC1_DATA   2

HRAMC data interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_HRAMC1_REGS   1

HRAMC Controller registers.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_IISC   0
#define SYSCLK_LCDCA   23
#define SYSCLK_OCD   0

On-Chip Debug system.

#define SYSCLK_PARC   18
#define SYSCLK_PBA_BRIDGE   5

HSB<->PBA bridge.

Referenced by sysclk_disable_pba_module(), and sysclk_enable_pba_module().

#define SYSCLK_PBB_BRIDGE   6

HSB<->PBB bridge.

Referenced by sysclk_disable_pbb_module(), and sysclk_enable_pbb_module().

#define SYSCLK_PBC_BRIDGE   7

HSB<->PBC bridge.

#define SYSCLK_PBD_BRIDGE   8

HSB<->PBD bridge.

#define SYSCLK_PDCA_HSB   0

PDCA memory interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_PDCA_PB   3

PDCA peripheral bus interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_PEVC   6
#define SYSCLK_PICOUART   5
#define SYSCLK_PM   0
#define SYSCLK_SCIF   2

System Control Interface.

Referenced by sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

#define SYSCLK_SPI   1
#define SYSCLK_SRC_DFLL   3

Digital Frequency Locked Loop.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_OSC0   1

Oscillator 0.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_PLL0   2

Phase Locked Loop 0.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RC1M   6

1 MHz RC oscillator

Referenced by sysclk_get_main_hz(), sysclk_init(), and sysclk_set_source().

#define SYSCLK_SRC_RC80M   4

80 MHz RC oscillator

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RCFAST   5

4-8-12 MHz RC oscillator

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RCSYS   0

System RC oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_TC0   2
#define SYSCLK_TC1   3
#define SYSCLK_TRNG   17
#define SYSCLK_TWIM0   4
#define SYSCLK_TWIM1   6
#define SYSCLK_TWIM2   21
#define SYSCLK_TWIM3   22
#define SYSCLK_TWIS0   5
#define SYSCLK_TWIS1   7
#define SYSCLK_USART0   8
#define SYSCLK_USART1   9
#define SYSCLK_USART2   10
#define SYSCLK_USART3   11
#define SYSCLK_USBC_DATA   3
#define SYSCLK_USBC_REGS   5
#define SYSCLK_WDT   3
#define USBCLK_SRC_DFLL   GENCLK_SRC_DFLL

Use DFLL.

#define USBCLK_SRC_GCLKIN0   GENCLK_SRC_GCLKIN0

Use GCLKIN0.

#define USBCLK_SRC_OSC0   GENCLK_SRC_OSC0

Use OSC0.

#define USBCLK_SRC_PLL0   GENCLK_SRC_PLL0

Use PLL0.

#define USBCLK_STARTUP_TIMEOUT   (OSC0_STARTUP_TIMEOUT*(1000000/OSC_RCSYS_NOMINAL_HZ))

Number of us to wait for USB clock to start.

static void sysclk_disable_cpu_module ( uint32_t  module_index)
inlinestatic

Disable a module clock derived from the CPU clock.

Parameters
module_indexIndex of the module clock in the CPUMASK register

References PM_CLK_GRP_CPU, and sysclk_priv_disable_module().

static void sysclk_disable_hsb_module ( uint32_t  module_index)
inlinestatic

Disable a module clock derived from the HSB clock.

Parameters
module_indexIndex of the module clock in the HSBMASK register

References PM_CLK_GRP_HSB, and sysclk_priv_disable_module().

Referenced by sysclk_disable_pba_module(), sysclk_disable_pbb_module(), and sysclk_disable_peripheral_clock().

static void sysclk_disable_pba_divmask ( uint32_t  mask)
inlinestatic

Disable divided clock mask derived from the PBA clock.

Parameters
maskmask of the divided clock in the PBADIVMASK register

Referenced by sysclk_disable_peripheral_clock().

void sysclk_disable_pba_module ( uint32_t  module_index)

Disable a module clock derived from the PBA clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References cpu_irq_restore(), cpu_irq_save(), PM_CLK_GRP_PBA, sysclk_disable_hsb_module(), SYSCLK_PBA_BRIDGE, and sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

void sysclk_disable_pbb_module ( uint32_t  module_index)

Disable a module clock derived from the PBB clock.

Parameters
module_indexIndex of the module clock in the PBBMASK register

References cpu_irq_restore(), cpu_irq_save(), PM_CLK_GRP_PBB, sysclk_disable_hsb_module(), SYSCLK_PBB_BRIDGE, and sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

static void sysclk_disable_pbc_module ( uint32_t  module_index)
inlinestatic

Disable a module clock derived from the PBC clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References PM_CLK_GRP_PBC, and sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

static void sysclk_disable_pbd_module ( uint32_t  module_index)
inlinestatic

Disable a module clock derived from the PBD clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References PM_CLK_GRP_PBD, and sysclk_priv_disable_module().

Referenced by sysclk_disable_peripheral_clock().

void sysclk_disable_usb ( void  )

Disable the USB generic clock.

References genclk_disable().

Referenced by otg_dual_disable().

static void sysclk_enable_cpu_module ( uint32_t  module_index)
inlinestatic

Enable a module clock derived from the CPU clock.

Parameters
module_indexIndex of the module clock in the CPUMASK register

References PM_CLK_GRP_CPU, and sysclk_priv_enable_module().

static void sysclk_enable_hsb_module ( uint32_t  module_index)
inlinestatic

Enable a module clock derived from the HSB clock.

Parameters
module_indexIndex of the module clock in the HSBMASK register

References PM_CLK_GRP_HSB, and sysclk_priv_enable_module().

Referenced by sysclk_enable_pba_module(), sysclk_enable_pbb_module(), sysclk_enable_peripheral_clock(), and sysclk_enable_usb().

static void sysclk_enable_pba_divmask ( uint32_t  mask)
inlinestatic

Enable divided clock mask derived from the PBA clock.

Parameters
maskmask of the divided clock in the PBADIVMASK register

Referenced by sysclk_enable_peripheral_clock().

void sysclk_enable_pba_module ( uint32_t  module_index)

Enable a module clock derived from the PBA clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References cpu_irq_restore(), cpu_irq_save(), PM_CLK_GRP_PBA, sysclk_enable_hsb_module(), SYSCLK_PBA_BRIDGE, and sysclk_priv_enable_module().

Referenced by sysclk_enable_peripheral_clock().

void sysclk_enable_pbb_module ( uint32_t  module_index)

Enable a module clock derived from the PBB clock.

Parameters
module_indexIndex of the module clock in the PBBMASK register

References cpu_irq_restore(), cpu_irq_save(), PM_CLK_GRP_PBB, sysclk_enable_hsb_module(), SYSCLK_PBB_BRIDGE, and sysclk_priv_enable_module().

Referenced by sysclk_enable_peripheral_clock(), and sysclk_enable_usb().

static void sysclk_enable_pbc_module ( uint32_t  module_index)
inlinestatic

Enable a module clock derived from the PBC clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References PM_CLK_GRP_PBC, and sysclk_priv_enable_module().

Referenced by sysclk_enable_peripheral_clock().

static void sysclk_enable_pbd_module ( uint32_t  module_index)
inlinestatic

Enable a module clock derived from the PBD clock.

Parameters
module_indexIndex of the module clock in the PBAMASK register

References PM_CLK_GRP_PBD, and sysclk_priv_enable_module().

Referenced by sysclk_enable_peripheral_clock().

void sysclk_enable_peripheral_clock ( const volatile void *  module)
void sysclk_enable_usb ( void  )

Enable the USB generic clock.

Precondition
The USB generic clock must be configured to 48MHz. CONFIG_USBCLK_SOURCE and CONFIG_USBCLK_DIV must be defined with proper configuration. The selected clock source must also be configured.

References CONFIG_USBCLK_DIV, CONFIG_USBCLK_SOURCE, genclk_enable_config(), sysclk_enable_hsb_module(), sysclk_enable_pbb_module(), SYSCLK_USBC_DATA, and SYSCLK_USBC_REGS.

Referenced by otg_dual_enable().

static uint32_t sysclk_get_cpu_hz ( void  )
inlinestatic

Return the current rate in Hz of the CPU clock.

Todo:
This function assumes that the CPU always runs at the system clock frequency. We want to support at least two more scenarios: Fixed CPU/bus clock dividers (config symbols) and dynamic CPU/bus clock dividers (which may change at run time). Ditto for all the bus clocks.
Returns
Frequency of the CPU clock, in Hz.

References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().

Referenced by sysclk_init(), and wdt_set_ctrl().

static uint32_t sysclk_get_hsb_hz ( void  )
inlinestatic

Return the current rate in Hz of the High-Speed Bus clock.

Returns
Frequency of the High Speed Peripheral Bus clock, in Hz.

References CONFIG_SYSCLK_CPU_DIV, and sysclk_get_main_hz().

static uint32_t sysclk_get_main_hz ( void  )
inlinestatic

Return the current rate in Hz of the main system clock.

Todo:
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.

References BOARD_OSC0_HZ, CONFIG_RCFAST_FRANGE, CONFIG_SYSCLK_SOURCE, dfll_get_default_rate, OSC_RC1M_NOMINAL_HZ, OSC_RC80M_NOMINAL_HZ, OSC_RCFAST12M_NOMINAL_HZ, OSC_RCFAST4M_NOMINAL_HZ, OSC_RCFAST8M_NOMINAL_HZ, OSC_RCSYS_NOMINAL_HZ, pll_get_default_rate, SYSCLK_SRC_DFLL, SYSCLK_SRC_OSC0, SYSCLK_SRC_PLL0, SYSCLK_SRC_RC1M, SYSCLK_SRC_RC80M, SYSCLK_SRC_RCFAST, and SYSCLK_SRC_RCSYS.

Referenced by sysclk_get_cpu_hz(), sysclk_get_hsb_hz(), sysclk_get_pba_hz(), sysclk_get_pbb_hz(), sysclk_get_pbc_hz(), and sysclk_get_pbd_hz().

static uint32_t sysclk_get_pba_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus A clock.

Returns
Frequency of the Peripheral Bus A clock, in Hz.

References CONFIG_SYSCLK_PBA_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_pbb_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus B clock.

Returns
Frequency of the Peripheral Bus B clock, in Hz.

References CONFIG_SYSCLK_PBB_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_pbc_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus C clock.

Returns
Frequency of the Peripheral Bus C clock, in Hz.

References CONFIG_SYSCLK_PBC_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_pbd_hz ( void  )
inlinestatic

Return the current rate in Hz of the Peripheral Bus D clock.

Returns
Frequency of the Peripheral Bus D clock, in Hz.

References CONFIG_SYSCLK_PBD_DIV, and sysclk_get_main_hz().

Referenced by sysclk_get_peripheral_bus_hz().

uint32_t sysclk_get_peripheral_bus_hz ( const volatile void *  module)

Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral.

Parameters
modulePointer to the module's base address.
Returns
Frequency of the bus attached to the specified peripheral, in Hz.

References Assert, sysclk_get_pba_hz(), sysclk_get_pbb_hz(), sysclk_get_pbc_hz(), and sysclk_get_pbd_hz().

Referenced by console_init().

void sysclk_init ( void  )

Initialize the synchronous clock system.

This function will initialize the system clock and its source. This includes:

  • Mask all synchronous clocks except for any clocks which are essential for normal operation (for example internal memory clocks).
  • Set up the system clock prescalers as specified by the application's configuration file.
  • Enable the clock source specified by the application's configuration file (oscillator or PLL) and wait for it to become stable.
  • Set the main system clock source to the clock specified by the application's configuration file.

Since all non-essential peripheral clocks are initially disabled, it is the responsibility of the peripheral driver to re-enable any clocks that are needed for normal operation.

References Assert, bpm_configure_power_scaling(), bpm_enable_fast_wakeup(), bpm_get_status(), BPM_PS_0, BPM_PS_1, BPM_PS_2, BPM_PSCM_CPU_NOT_HALT, CONFIG_SYSCLK_CPU_DIV, CONFIG_SYSCLK_INIT_CPUMASK, CONFIG_SYSCLK_INIT_HSBMASK, CONFIG_SYSCLK_INIT_PBAMASK, CONFIG_SYSCLK_INIT_PBBMASK, CONFIG_SYSCLK_INIT_PBCMASK, CONFIG_SYSCLK_INIT_PBDMASK, CONFIG_SYSCLK_PBA_DIV, CONFIG_SYSCLK_PBB_DIV, CONFIG_SYSCLK_PBC_DIV, CONFIG_SYSCLK_PBD_DIV, CONFIG_SYSCLK_SOURCE, cpu_irq_restore(), cpu_irq_save(), dfll_enable_config_defaults(), FLASH_FREQ_PS1_FWS_0_MAX_FREQ, FLASH_FREQ_PS1_FWS_1_MAX_FREQ, flash_set_bus_freq, osc_enable(), OSC_ID_OSC0, OSC_ID_RC1M, OSC_ID_RC80M, OSC_ID_RCFAST, osc_wait_ready(), pll_enable_config_defaults(), sysclk_enable_peripheral_clock(), sysclk_get_cpu_hz(), SYSCLK_INIT_MINIMAL_CPUMASK, SYSCLK_INIT_MINIMAL_HSBMASK, SYSCLK_INIT_MINIMAL_PBAMASK, SYSCLK_INIT_MINIMAL_PBBMASK, SYSCLK_INIT_MINIMAL_PBCMASK, SYSCLK_INIT_MINIMAL_PBDMASK, sysclk_set_prescalers(), sysclk_set_source(), SYSCLK_SRC_DFLL, SYSCLK_SRC_OSC0, SYSCLK_SRC_PLL0, SYSCLK_SRC_RC1M, SYSCLK_SRC_RC80M, SYSCLK_SRC_RCFAST, and SYSCLK_SRC_RCSYS.

Referenced by bootloader_system_init().

void sysclk_priv_disable_module ( uint32_t  bus_id,
uint32_t  module_index 
)

Disable a maskable module clock.

Parameters
bus_idBus index, given by the PM_CLK_GRP_xxx definitions.
module_indexIndex of the module to be disabled. This is the bit number in the corresponding xxxMASK register.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_disable_cpu_module(), sysclk_disable_hsb_module(), sysclk_disable_pba_module(), sysclk_disable_pbb_module(), sysclk_disable_pbc_module(), and sysclk_disable_pbd_module().

void sysclk_priv_enable_module ( uint32_t  bus_id,
uint32_t  module_index 
)

Enable a maskable module clock.

Parameters
bus_idBus index, given by the PM_CLK_GRP_xxx definitions.
module_indexIndex of the module to be enabled. This is the bit number in the corresponding xxxMASK register.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_enable_cpu_module(), sysclk_enable_hsb_module(), sysclk_enable_pba_module(), sysclk_enable_pbb_module(), sysclk_enable_pbc_module(), and sysclk_enable_pbd_module().

void sysclk_set_prescalers ( uint32_t  cpu_shift,
uint32_t  pba_shift,
uint32_t  pbb_shift,
uint32_t  pbc_shift,
uint32_t  pbd_shift 
)

Set system clock prescaler configuration.

This function will change the system clock prescaler configuration to match the parameters.

Note
The parameters to this function are device-specific.
Parameters
cpu_shiftThe CPU clock will be divided by \(2^{cpu\_shift}\)
pba_shiftThe PBA clock will be divided by \(2^{pba\_shift}\)
pbb_shiftThe PBB clock will be divided by \(2^{pbb\_shift}\)
pbc_shiftThe PBC clock will be divided by \(2^{pbc\_shift}\)
pbd_shiftThe PBD clock will be divided by \(2^{pbd\_shift}\)

References Assert, cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_init().

void sysclk_set_source ( uint32_t  src)

Change the source of the main system clock.

Parameters
srcThe new system clock source. Must be one of the constants from the System Clock Sources section.

References Assert, cpu_irq_restore(), cpu_irq_save(), and SYSCLK_SRC_RC1M.

Referenced by sysclk_init().