The QTouch LED demo will help new users get familiar with Atmel's SAM family of microcontrollers. This basic application shows how to initialize the QTouch library and flash the LEDs by setting the timer counter frequency through the QTouch slider.
This package can be used with SAM4S-Xplained evaluation kits.
The demonstration program makes two LEDs on the board blink at a specific rate. This rate is generated by using Time tick timer. The frequency of the Time tick can be adjusted by the QTouch slider.