Microchip® Advanced Software Framework

sam_spi/spi_master.h File Reference

SPI master common service for SAM.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "sysclk.h"
#include "status_codes.h"
#include "spi.h"
#include "conf_spi_master.h"

Data Structures

struct  spi_device
 Polled SPI device definition. More...
 

Macros

#define SPI_CPHA   (1 << 0)
 Default Configuration of SPI Master Delay BCS. More...
 
#define SPI_CPOL   (1 << 1)
 Clock polarity. More...
 
#define SPI_MODE_0   0
 SPI mode 0. More...
 
#define SPI_MODE_1   (SPI_CPHA)
 SPI mode 1. More...
 
#define SPI_MODE_2   (SPI_CPOL)
 SPI mode 2. More...
 
#define SPI_MODE_3   (SPI_CPOL | SPI_CPHA)
 SPI mode 3. More...
 
#define SPI_TYPE_DEFS
 

Typedefs

typedef uint32_t board_spi_select_id_t
 Board SPI Select Id Definition. More...
 
typedef uint8_t spi_flags_t
 SPI Flags Definition. More...
 

Functions

void spi_deselect_device (Spi *p_spi, struct spi_device *device)
 Deselect the given device on the SPI bus. More...
 
void spi_master_init (Spi *p_spi)
 Initialize the SPI in master mode. More...
 
void spi_master_setup_device (Spi *p_spi, struct spi_device *device, spi_flags_t flags, uint32_t baud_rate, board_spi_select_id_t sel_id)
 Set up an SPI device. More...
 
status_code_t spi_read_packet (Spi *p_spi, uint8_t *data, size_t len)
 Receive a sequence of bytes from an SPI device. More...
 
static void spi_read_single (Spi *p_spi, uint8_t *data)
 Receive one byte from an SPI device. More...
 
void spi_select_device (Spi *p_spi, struct spi_device *device)
 Select the given device on the SPI bus. More...
 
status_code_t spi_transceive_packet (Spi *p_spi, uint8_t *tx_data, uint8_t *rx_data, size_t len)
 Send and receive a sequence of bytes from an SPI device. More...
 
status_code_t spi_write_packet (Spi *p_spi, const uint8_t *data, size_t len)
 Send a sequence of bytes to an SPI device. More...
 
static void spi_write_single (Spi *p_spi, uint8_t data)
 Write one byte to an SPI device. More...
 

#define SPI_CPHA   (1 << 0)

Default Configuration of SPI Master Delay BCS.

Default Configuration of SPI Master Bits per Transfer Definition Default Configuration of SPI Master Delay BCT Default Configuration of SPI Master Delay BS Default Configuration of SPI Master Dummy Field Clock phase.

#define SPI_CPOL   (1 << 1)

Clock polarity.

#define SPI_MODE_0   0

SPI mode 0.

Referenced by usart_init_spi_master(), and usart_init_spi_slave().

#define SPI_MODE_1   (SPI_CPHA)

SPI mode 1.

Referenced by usart_init_spi_master(), and usart_init_spi_slave().

#define SPI_MODE_2   (SPI_CPOL)

SPI mode 2.

Referenced by usart_init_spi_master(), and usart_init_spi_slave().

#define SPI_MODE_3   (SPI_CPOL | SPI_CPHA)
#define SPI_TYPE_DEFS

typedef uint32_t board_spi_select_id_t

Board SPI Select Id Definition.

typedef uint8_t spi_flags_t

SPI Flags Definition.

void spi_deselect_device ( Spi *  p_spi,
struct spi_device device 
)

Deselect the given device on the SPI bus.

Call board chip deselect.

Parameters
p_spiBase address of the SPI instance.
deviceSPI device.
Precondition
SPI device must be selected with spi_select_device() first.

References NONE_CHIP_SELECT_ID, spi_is_tx_empty(), spi_set_lastxfer(), spi_set_peripheral_chip_select_value(), and UNUSED.

void spi_master_setup_device ( Spi *  p_spi,
struct spi_device device,
spi_flags_t  flags,
uint32_t  baud_rate,
board_spi_select_id_t  sel_id 
)

Set up an SPI device.

The returned device descriptor structure must be passed to the driver whenever that device should be used as current slave device.

Parameters
p_spiBase address of the SPI instance.
devicePointer to SPI device struct that should be initialized.
flagsSPI configuration flags. Common flags for all implementations are the SPI modes SPI_MODE_0 ... SPI_MODE_3.
baud_rateBaud rate for communication with slave device in Hz.
sel_idBoard specific select id.

References Assert, CONFIG_SPI_MASTER_BITS_PER_TRANSFER, CONFIG_SPI_MASTER_DELAY_BCT, CONFIG_SPI_MASTER_DELAY_BS, spi_device::id, spi_calc_baudrate_div(), spi_configure_cs_behavior(), SPI_CS_KEEP_LOW, spi_set_baudrate_div(), spi_set_bits_per_transfer(), spi_set_clock_phase(), spi_set_clock_polarity(), spi_set_transfer_delay(), sysclk_get_peripheral_hz(), and UNUSED.

Referenced by ili9488_init().

status_code_t spi_read_packet ( Spi *  p_spi,
uint8_t *  data,
size_t  len 
)

Receive a sequence of bytes from an SPI device.

All bytes sent out on SPI bus are sent as value 0xff.

Parameters
p_spiBase address of the SPI instance.
dataData buffer to read.
lenLength of data to be read.
Precondition
SPI device must be selected with spi_select_device() first.

All bytes sent out on SPI bus are sent as value 0.

Parameters
p_spiBase address of the SPI instance.
dataData buffer to read.
lenLength of data to be read.
Precondition
SPI device must be selected with spi_select_device() first.

References CONFIG_SPI_MASTER_DUMMY, ERR_TIMEOUT, spi_is_rx_ready(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.

Referenced by ili9488_copy_pixels_from_screen(), ili9488_read_chipid(), and ili9488_read_ram().

static void spi_read_single ( Spi *  p_spi,
uint8_t *  data 
)
inlinestatic

Receive one byte from an SPI device.

Parameters
p_spiBase address of the SPI instance.
dataData to read.

References spi_get().

Referenced by spi_read_packet(), and spi_transceive_packet().

void spi_select_device ( Spi *  p_spi,
struct spi_device device 
)

Select the given device on the SPI bus.

Set device specific setting and call board chip select.

Parameters
p_spiBase address of the SPI instance.
deviceSPI device.

References spi_device::id, MAX_NUM_WITH_DECODER, MAX_NUM_WITHOUT_DECODER, spi_get_peripheral_select_decode_setting(), and spi_set_peripheral_chip_select_value().

Referenced by ili9488_init().

status_code_t spi_transceive_packet ( Spi *  p_spi,
uint8_t *  tx_data,
uint8_t *  rx_data,
size_t  len 
)

Send and receive a sequence of bytes from an SPI device.

Parameters
p_spiBase address of the SPI instance.
tx_dataData buffer to send.
rx_dataData buffer to read.
lenLength of data to be read.
Precondition
SPI device must be selected with spi_select_device() first.

References ERR_TIMEOUT, spi_is_rx_ready(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.

status_code_t spi_write_packet ( Spi *  p_spi,
const uint8_t *  data,
size_t  len 
)

Send a sequence of bytes to an SPI device.

Received bytes on the SPI bus are discarded.

Parameters
p_spiBase address of the SPI instance.
dataData buffer to write.
lenLength of data to be written.
Precondition
SPI device must be selected with spi_select_device() first.

References ERR_TIMEOUT, spi_is_tx_ready(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.

Referenced by ili9488_write_ram_buffer(), and ili9488_write_register().

static void spi_write_single ( Spi *  p_spi,
uint8_t  data 
)
inlinestatic

Write one byte to an SPI device.

Parameters
p_spiBase address of the SPI instance.
dataData to write.

References spi_put().

Referenced by spi_read_packet(), spi_transceive_packet(), and spi_write_packet().