The Starter Kit Demo will help new users get familiar with Atmel's SAM family of microcontrollers. This demo features the IO1 and OLED1 extension boards for the SAM4 Xplained Pro.
This package can be used with SAM Xplained Pro evaluation kits.
The demonstration program can operate in 3 different modes; temperature information, light sensor information and SD card status. The user can switch between the various mode by pressing Button1. When running in mode 3 (SD card content), the user can browse the SD content using Button2 (previous) and Button3 (next). Filenames are directly printed on the OLED screen.
IO1 extension must be connected on EXT2. OLED1 extension must be connected on EXT3.