Controller Area Network (CAN) driver module for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Data Structures | |
struct | can_mb_conf_t |
Define the struct for CAN message mailbox. More... | |
Macros | |
#define | CAN_BPS_1000K 1000 |
Define the typical baudrate for CAN communication in KHz. More... | |
#define | CAN_BPS_10K 10 |
#define | CAN_BPS_125K 125 |
#define | CAN_BPS_250K 250 |
#define | CAN_BPS_25K 25 |
#define | CAN_BPS_500K 500 |
#define | CAN_BPS_50K 50 |
#define | CAN_BPS_5K 5 |
#define | CAN_BPS_800K 800 |
#define | CAN_DISABLE_ALL_INTERRUPT_MASK 0xffffffff |
Disable all interrupt mask. More... | |
#define | CAN_MAILBOX_NOT_READY 0x01 |
Receiver is empty or transmitter is busy. More... | |
#define | CAN_MAILBOX_RX_NEED_RD_AGAIN 0x04 |
Application needs to re-read the data register in Receive with Overwrite mode. More... | |
#define | CAN_MAILBOX_RX_OVER 0x02 |
Message overwriting happens or there're messages lost in different receive modes. More... | |
#define | CAN_MAILBOX_TRANSFER_OK 0 |
Define CAN mailbox transfer status code. More... | |
#define | CAN_MB_CONSUMER_MODE 4 |
#define | CAN_MB_DISABLE_MODE 0 |
Define the mailbox mode. More... | |
#define | CAN_MB_PRODUCER_MODE 5 |
#define | CAN_MB_RX_MODE 1 |
#define | CAN_MB_RX_OVER_WR_MODE 2 |
#define | CAN_MB_TX_MODE 3 |
#define | GLOBAL_MAILBOX_MASK 0x000000ff |
Define the Mailbox mask for eight mailboxes. More... | |
Functions | |
void | can_disable (Can *p_can) |
Disable CAN Controller. More... | |
void | can_disable_autobaud_listen_mode (Can *p_can) |
Disable CAN Controller autobaud/listen mode. More... | |
void | can_disable_interrupt (Can *p_can, uint32_t dw_mask) |
Disable CAN interrupt. More... | |
void | can_disable_low_power_mode (Can *p_can) |
Disable CAN Controller low power mode. More... | |
void | can_disable_overload_frame (Can *p_can) |
CAN Controller won't generate overload frame. More... | |
void | can_disable_time_triggered_mode (Can *p_can) |
Disable CAN Controller time triggered mode. More... | |
void | can_disable_timer_freeze (Can *p_can) |
Disable CAN Controller timer freeze. More... | |
void | can_disable_tx_repeat (Can *p_can) |
Disable CAN Controller transmit repeat function. More... | |
void | can_enable (Can *p_can) |
Enable CAN Controller. More... | |
void | can_enable_autobaud_listen_mode (Can *p_can) |
Enable CAN Controller autobaud/listen mode. More... | |
void | can_enable_interrupt (Can *p_can, uint32_t dw_mask) |
Enable CAN interrupt. More... | |
void | can_enable_low_power_mode (Can *p_can) |
Enable CAN Controller low power mode. More... | |
void | can_enable_overload_frame (Can *p_can) |
CAN Controller will generate an overload frame after each successful reception for mailboxes configured in Receive mode, Producer and Consumer. More... | |
void | can_enable_time_triggered_mode (Can *p_can) |
Enable CAN Controller time triggered mode. More... | |
void | can_enable_timer_freeze (Can *p_can) |
Enable CAN Controller timer freeze. More... | |
void | can_enable_tx_repeat (Can *p_can) |
Enable CAN Controller transmit repeat function. More... | |
uint32_t | can_get_internal_timer_value (Can *p_can) |
Get the 16-bit free-running internal timer count. More... | |
uint32_t | can_get_interrupt_mask (Can *p_can) |
Get CAN Interrupt Mask. More... | |
uint8_t | can_get_rx_error_cnt (Can *p_can) |
Get CAN receive error counter. More... | |
uint32_t | can_get_status (Can *p_can) |
Get CAN status. More... | |
uint32_t | can_get_timestamp_value (Can *p_can) |
Get CAN timestamp register value. More... | |
uint8_t | can_get_tx_error_cnt (Can *p_can) |
Get CAN transmit error counter. More... | |
void | can_global_send_abort_cmd (Can *p_can, uint8_t uc_mask) |
Send global abort request. More... | |
void | can_global_send_transfer_cmd (Can *p_can, uint8_t uc_mask) |
Send global transfer request. More... | |
uint32_t | can_init (Can *p_can, uint32_t ul_mck, uint32_t ul_baudrate) |
Initialize CAN controller. More... | |
uint32_t | can_mailbox_get_status (Can *p_can, uint8_t uc_index) |
Get status of the mailbox. More... | |
void | can_mailbox_init (Can *p_can, can_mb_conf_t *p_mailbox) |
Initialize the mailbox in different mode and set up related configuration. More... | |
uint32_t | can_mailbox_read (Can *p_can, can_mb_conf_t *p_mailbox) |
Read receive information for the mailbox. More... | |
void | can_mailbox_send_abort_cmd (Can *p_can, can_mb_conf_t *p_mailbox) |
Send single mailbox abort request. More... | |
void | can_mailbox_send_transfer_cmd (Can *p_can, can_mb_conf_t *p_mailbox) |
Send single mailbox transfer request. More... | |
void | can_mailbox_set_timemark (Can *p_can, uint8_t uc_index, uint16_t us_cnt) |
Configure the timemark for the mailbox. More... | |
uint32_t | can_mailbox_tx_remote_frame (Can *p_can, can_mb_conf_t *p_mailbox) |
Require to send out a remote frame. More... | |
uint32_t | can_mailbox_write (Can *p_can, can_mb_conf_t *p_mailbox) |
Prepare transmit information and write them into the mailbox. More... | |
void | can_reset_all_mailbox (Can *p_can) |
Reset the eight mailboxes. More... | |
void | can_reset_internal_timer (Can *p_can) |
Reset the internal free-running 16-bit timer. More... | |
void | can_set_rx_sync_stage (Can *p_can, uint32_t ul_stage) |
Configure CAN Controller reception synchronization stage. More... | |
void | can_set_timestamp_capture_point (Can *p_can, uint32_t ul_flag) |
Configure the timestamp capture point, at the start or the end of frame. More... | |
#define CAN_BPS_1000K 1000 |
Define the typical baudrate for CAN communication in KHz.
Referenced by main().
#define CAN_BPS_10K 10 |
#define CAN_BPS_125K 125 |
#define CAN_BPS_250K 250 |
#define CAN_BPS_25K 25 |
#define CAN_BPS_500K 500 |
#define CAN_BPS_50K 50 |
#define CAN_BPS_5K 5 |
#define CAN_BPS_800K 800 |
#define CAN_DISABLE_ALL_INTERRUPT_MASK 0xffffffff |
Disable all interrupt mask.
Referenced by main().
#define CAN_MAILBOX_NOT_READY 0x01 |
Receiver is empty or transmitter is busy.
Referenced by can_mailbox_tx_remote_frame(), and can_mailbox_write().
#define CAN_MAILBOX_RX_NEED_RD_AGAIN 0x04 |
Application needs to re-read the data register in Receive with Overwrite mode.
Referenced by can_mailbox_read().
#define CAN_MAILBOX_RX_OVER 0x02 |
Message overwriting happens or there're messages lost in different receive modes.
Referenced by can_mailbox_read().
#define CAN_MAILBOX_TRANSFER_OK 0 |
Define CAN mailbox transfer status code.
Read from or write into mailbox successfully.
Referenced by can_mailbox_read(), can_mailbox_tx_remote_frame(), and can_mailbox_write().
#define CAN_MB_CONSUMER_MODE 4 |
Referenced by test_4().
#define CAN_MB_DISABLE_MODE 0 |
Define the mailbox mode.
Referenced by can_reset_all_mailbox().
#define CAN_MB_PRODUCER_MODE 5 |
Referenced by test_4().
#define CAN_MB_RX_OVER_WR_MODE 2 |
Referenced by test_3().
#define GLOBAL_MAILBOX_MASK 0x000000ff |
Define the Mailbox mask for eight mailboxes.
Referenced by CAN1_Handler(), can_global_send_abort_cmd(), and can_global_send_transfer_cmd().