This is the documentation for the data structures, functions, variables, defines, enums, and typedefs for the C42412A LCD Glass component example. It also comes bundled with an application-example of usage.
This example demonstrates how to use the C42412A LCD Glass driver with the 32 KHz oscillator crystal.
This software is written for GNU GCC and IAR Embedded Workbench for Atmel. Other compilers may or may not work.
All SAM devices with an LCDCA connected to C42412A LCD Glass component and a USART module can be used.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/