Microchip® Advanced Software Framework

conf_ili9488.h File Reference

ILI9488 configuration.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

#include "board.h"

Macros

#define BOARD_ILI9488_ADDR   0x63000000 /* The base address, depends on which SMC chip select is used by ILI9488. */
 Configuration of the ILI9488 LCD display driver. More...
 

#define BOARD_ILI9488_ADDR   0x63000000 /* The base address, depends on which SMC chip select is used by ILI9488. */

Configuration of the ILI9488 LCD display driver.

Referenced by LCD_IR(), LCD_MULTI_RD(), LCD_MULTI_WD(), LCD_RD(), and LCD_WD().