Purpose
This example shows how to configure the MT48LC16M16A2. It will perform write and read operations to check the configuration.
Description
An accurate one-to-one comparison is processed after the complete SDRAM configuration.
Compilation Info
This software was written for the GNU GCC and IAR EWARM. Other compilers may or may not work.
Usage
- Build the program and download it into the evaluation board.
- On the computer, open and configure a terminal application (e.g., HyperTerminal on Microsoft Windows) with these settings:
- 115200 bauds
- 8 bits of data
- No parity
- 1 stop bit
- No flow control
- Start the application.
- In the terminal window, the following text should appear (values depend on the board and the chip used):
-- SDRAMC Example --
-- xxxxxx-xx
-- Compiled: xxx xx xxxx xx:xx:xx --
...